Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Laptop Webcam to USB Webcam? for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 6225 views
  • Users 0 members are here
  • usb
  • raspberry_pi
  • raspberrypi
  • raspberry_pi_camera
  • laptop
  • webcam
Related

Laptop Webcam to USB Webcam? for Raspberry Pi

e14 Contributor
e14 Contributor over 12 years ago

I have just dissembled my HP pavilion Dv7 because the motherboard gave up, and now i am looking to salvage part of it to use for my raspberry pi. I have its Webcam and was wondering if i could rewire it to work with a USB.

 

The camera is a 21QCMMA00M0 (it has 6 wires Red, Orange, Yellow, Green, Blue and a black), if anyone could tell me how to rewire it to use with a USB that would be very helpful.

 

{I just attached a few image of the wires one is the usb i am going to use and the other is the wires of the camera.}

 

|   |   |

V  V V

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • ericwertz
    0 ericwertz over 12 years ago

    Unless this device was originally implemented as a USB camera and hooked-up to USB internally, there's zero chance that you're just going to be able to wire this up as a USB webcam.  You would have been able to determine if this were the case or not when the machine was working by noting whether or not it showed up in the Device Manager somewhere under the USB tree.  If it did, then you'd stand a chance of getting it to work.

     

    The camera module's interface could, in the general case, be anything -- SPI, MIPI CSI/CSI-2, or something custom.  Given how few wires you note that it has, it's unlikely to be CSI-2 (the connector to which the Pi Cam connects).  Without knowing a lot about camera module interfacing, this project is a non-starter if your goal is simply to get a working camera on the Pi (which you buy for $25).  If your goal is to learn a lot about camera interfacing, then this project may be a worthy one.

     

    Just like you can't take an engine out of an arbitrary car and "solder it up" to another arbitrary car, this camera isn't going to just "drop in" to your Pi.  This isn't to say that it ultimately can't be gotten to work, the question is with how much effort.  It's conceivable some driver exists somewhere that can get you most of the way there, but whether or not it ultimately makes use of USB is fairly inconsequential.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • knight_rider1977
    0 knight_rider1977 over 12 years ago in reply to ericwertz

    I think our initial goal was to see how much of our dead in the water Laptops can be reused/repurposed for different projects.  I am also looking at it as an opportunity to expand my knowledge about embedded components and how they interface with different systems.  Honestly you are correct, it would be more of a viable option to just purchase the camera designed for the Pi.  I found this to be a good challenge to keep expanding my knowledge, in this case camera interfacing.  It would also be cool to reuse it for a purpose other than the Pi.  One less thing to go to the land fill image

     

    I did more digging and was finally able to read the crazy small print on the IC and found it to be a MX25L512-12G SPI chip.  I also downloaded the datasheet for the chip.  There is still another IC on the board but half of it is covered in some soft of semi transparent black coating.  I can almost read it via a magnified picture with a my phone LED light.  My next challenge reading it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • knight_rider1977
    0 knight_rider1977 over 12 years ago in reply to ericwertz

    I think our initial goal was to see how much of our dead in the water Laptops can be reused/repurposed for different projects.  I am also looking at it as an opportunity to expand my knowledge about embedded components and how they interface with different systems.  Honestly you are correct, it would be more of a viable option to just purchase the camera designed for the Pi.  I found this to be a good challenge to keep expanding my knowledge, in this case camera interfacing.  It would also be cool to reuse it for a purpose other than the Pi.  One less thing to go to the land fill image

     

    I did more digging and was finally able to read the crazy small print on the IC and found it to be a MX25L512-12G SPI chip.  I also downloaded the datasheet for the chip.  There is still another IC on the board but half of it is covered in some soft of semi transparent black coating.  I can almost read it via a magnified picture with a my phone LED light.  My next challenge reading it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago in reply to knight_rider1977

    you can even try this

     

    black = gnd

    red = +5v

    green = D-

    yellow = D+