Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum GPIO pins
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 709 subscribers
  • Views 2717 views
  • Users 0 members are here
  • wolfson
  • raspberry
  • pins
  • pi
  • gpio
  • audio_card
  • raspberry_pi
  • raspeberry_pi_accessories
Related

GPIO pins

e14 Contributor
e14 Contributor over 12 years ago

I wanted to use this for a HiFi project, but it seems to use all the GPIO pins, and I need more pins for IR reciever and a small LCD screen, is this impossible or is there a way around it?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The audio card uses i2c from Raspberry Pi, and a single GPIO output, plus the lines form the P5 header. There are lines available (i2c is multidrop anyway).

     

       1.  If the user is not skilled with a soldering iron, there is unfortunately no mechanical access to the GPIO pins once the audio card has been plugged on to the top of the Pi. Also,   

            options to ‘stack’ the board using expansion options like PiFace Rack, are not possible either, because the Raspberry Pi P5 pins are needed make the board work. P5 is not part of 

            the expansion board specification.


       2.  With soldering skills, the user could demount the pogo pin header, fit an 8-pin header to his Pi, and fit one of the opposite gender to his sound card. Short ribbon cables could then   

            be constructed to join the two boards together, breaking out the GPIO’s required to drive display and IR receiver.

     

       3.  Again, with soldering skills, the relevant GPIO’s required can be taken from the back of the Pi with very fine and short flying leads.

     

    Of course, all of the soldering options will invalidate any warranty in place for the Raspberry Pi and the Audio Card, but if you know what you are doing, should be fine. There is also a product called PiFace Control and Display that gives you the display and remote control options you might want, together with software required to drive it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The audio card uses i2c from Raspberry Pi, and a single GPIO output, plus the lines form the P5 header. There are lines available (i2c is multidrop anyway).

     

       1.  If the user is not skilled with a soldering iron, there is unfortunately no mechanical access to the GPIO pins once the audio card has been plugged on to the top of the Pi. Also,   

            options to ‘stack’ the board using expansion options like PiFace Rack, are not possible either, because the Raspberry Pi P5 pins are needed make the board work. P5 is not part of 

            the expansion board specification.


       2.  With soldering skills, the user could demount the pogo pin header, fit an 8-pin header to his Pi, and fit one of the opposite gender to his sound card. Short ribbon cables could then   

            be constructed to join the two boards together, breaking out the GPIO’s required to drive display and IR receiver.

     

       3.  Again, with soldering skills, the relevant GPIO’s required can be taken from the back of the Pi with very fine and short flying leads.

     

    Of course, all of the soldering options will invalidate any warranty in place for the Raspberry Pi and the Audio Card, but if you know what you are doing, should be fine. There is also a product called PiFace Control and Display that gives you the display and remote control options you might want, together with software required to drive it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I have some experience with a soldering iron, but not much and it was a long time ago.

     

    How difficult would it be to demount the old pin headers and fit the new ones?

     

    Thanks for the reply

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to e14 Contributor

    I did this to a PiFace Digital ... before the Pi rack was available.

    It isn't hard to do, and you don't need to use 2 13 pin strips if you only want a few pins.

    http://www.element14.com/community/roadTestReviews/1452

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I'm currently using a pifacecad with my pi. I'm willing to forego the lcd and external buttons to use the wolfson audio card, but I''m not sure I could live without the IR receiver. Will an IR receiver module work with the expansion header of the wolfson card?

     

    Thank you!