Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum What battery to use for portable RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 6 answers
  • Subscribers 706 subscribers
  • Views 6927 views
  • Users 0 members are here
  • batteries
  • help
  • pi
  • plug
  • robotics
  • portable_battery
  • raspberry_pi
  • aa
  • battery
  • raspberrypi
  • rpi
  • wireless
  • question
Related

What battery to use for portable RPi?

e14 Contributor
e14 Contributor over 11 years ago

I was planning on making an RPi robot, wireless, of course, and i was wondering what type of battery or battery pack to use (size, voltage, amperage, etc). It would also be helpful to know if i should wire it directly to a male micro usb cable to plug directly into the Pi, or with a female micro usb jack to plug another cable into. If you could give any sugestions as to how to recharge the battery pack, or simply use regular AA batteries, it would be greatly appreciated.

  • Sign in to reply
  • Cancel
  • toxxn
    0 toxxn over 11 years ago

    Lucky enough for projects like this there are a wide variety of different types of batteries one could use, Lipo, Li-ion, ni-cd, etc, or you could even go with a 5v 4x AA battery pack.

    Any hobbyist battery of 4.5-5v with at least 1000mA or higher would be my choice. They are generally small, rechargeable, decently priced, and if you need more amperage, you have that option as they come in a variety. As for size of the battery, that depends on your project and how much space you want to allocate for the battery. As mentioned however, hobbyist batteries are generally quite small and lightweight as they are used in electronics such as RC cars, boats, planes, etc.

     

    You can power the Pi directly using the provided GPIO pins on the board using one of these batteries. I wouldn't alter the battery in any way to adjust how you want to power the Pi as some of these batteries such as Lithium Ion can be very dangerous if misused. If you did not want to use the GPIO's, you could simply just get a connector that fits to the battery and solder on a micro USB.

     

    Just a a word of caution with li-ion batteries, only charge them with the correct method of charging. Otherwise you could create a recipe for disaster as Li-ion's if not charged properly, overcharged, or misused can create quite a powerful chemical reaction that may result in a fire and/or the battery to explode. I tend to stay away from lithium batteries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to toxxn

    Something I have that is long lasting for a four wheel rover is a RC Lipo Battery (11.1V/2600mAh). Works for the motors and I add a 5V/1.5A regulator bypass for the RasPi. Lasts for days and the battery charges in 2hrs. Works as well for the BeagleBone Black.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • toxxn
    0 toxxn over 11 years ago in reply to e14 Contributor

    This is also a great option. Using a Step-Down Module (Buck Converter) you could use a larger voltage battery and increase the mAh drastically.

     

    I have a KIS3R33S USB DC 7V-24V to 5V 3A Step-Down module that I used in a custom Pi power supply I made.

    I recycled an old Bose wall wart that is 12v 1800mA for my custom power supply which allows me to power a small tft lcd (Car reverse monitor) at the same time, while the step-down module allows me to step the 12v down to 5v for the Pi. 2 in 1 power supply. This also leaves me open for a larger voltage battery or a car charger using the same power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago

    You don't say how big your robot is. I think that beyond a certain size the Robot it's self will burn more juice than the Pi.

    If it's only small then a few AA rechargeable will be good enough to experiment so say 4.5-6V(4XAA) for the motors and the same again for the PI.Maybe even say 6AA's for the PI thinking about it so you can use a regulator to get a good 5V input to it.

     

    A dual supply is almost always a good idea as the motors of the robot will induce noise on the power line which may be enough to crash/restart the PI or at least have strange behaviour.

     

    Larger robots could use small SLA lead acid batteries as they give lots of current and easy to charge and generally safe enough as long as you respect them. failing that say a Lithium racing pack but they take more care to charge correctly...Nicer solution need to be careful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Problemchild

    The robot I'm planning on making will have a servo motor, a few different sensors, and 2 dc motors. I'm also using a backup display with composite output for the monitor.It probably wont be much larger than 15x20 cm (about 6x9 inches), and 15 cm tall (6 inches). I still need plan out the mechanics for it's arm/club (it's going to hit a golf ball into a hole), but it will probably be made out of plastic or aluminium, with some parts sticking out. I'd like to have the battery near the bottom or back so that the robot isn't topheavy, or tip the bot over when it hits the ball, and so that it can be accessed easily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 11 years ago in reply to e14 Contributor

    You will most likely need a couple different power options unless you want one big battery but then you will need a Buck Converter to step down the voltage for the Pi.

    Depending on the servos and DC Motors you plan to use, I would say a battery for the LCD and servo/motors, and another for the Pi.

     

    The TFT LCD you mentioned is about 12v DC 200mA.

    Depending on the Pi version, using model b for example is 5v 700mA and with anything connected to the Pi you will need more than a 700mA supply. I would recommend around 5v 1500-2000mA.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Iisn't it much more efficient to use a 5V 1.5 A voltage regulator IC with a couple of small capacitors, one on the input and one on the output, as compared to using a Buck down converter module? I don't know how much conversion loss there is in those Buck modules, but some power must be lost to heat in the DC-> AC -> DC conversion process they use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ipv1
    0 ipv1 over 11 years ago

    Ah Excellent Idea. Here is my answer:

    Option 1: Get a 2200mAh battery pack that is a good option for the RPI B+ itself. Make sure you power the motors from a different battery though since motor starts can cause problems with the regulation when drawing high currents.

     

    Option 2: With the RPI B+ you can buy the LiPo Rider Pro which can be used to charge the LiPo battery as well as supply the high currents to the RPi. Again separate batteries for the motor.

     

    Option 3: IF you can use a bigger battery, Get a 12V lead acid battery along with a LM2596 switching regulator to get 5V from the 12V battery. In this case you may use the lead acid battery for the motor as well.

     

    I use the lipo rider pro since I can charge the LiPo while it powers the RPi B+ image

    Hope that helps image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to ipv1

    For situations that require absolute safety I would go for stacking the ultra flat Prologium LCB batteries.

    http://www.prologium.com/Performance.aspx?02F0EA87FB60FF526BD81D51338B43D5

    I saw their demo in 2012 at a Battery fair in Tokyo. They showed that these batteries can be cut with a scissor or thrown in the fire and nothing dangerous happened with it.

    These batteries also bring the possibility of shaping and curving although not recommended. The flat squares can find an easy home in your robot suit or become the suit image


    The slightly thicker Pouch types are more powerful so lets try one 12V configuration, assuming we can take care of the Motor noise with a TVS Diode clamping at 15V :

     

    Using PLCB 140210 type of battery with these specs:

    Dimensions (mm): 140x210

    Weight (g): 145

    Nominal Voltage (V) 3.75

    Nominal Capacity (mAh): 4970


    Arrange 2 sets of 4 in serial, in parallel mode results in:

    VDC range (V) 12~15

    Nominal Capacity (mAh): 9940

    Total weight(g): 1160

    Recommended max discharge rate 0.2C will be about 2A.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    If you want to use the same battery source for all consumers then maybe Four-quadrant Zero-current-transition Converter-fed Dc Motor Driving as for automotive is feasible

    http://union-services.com/aevs/911-917.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>