Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum What battery to use for portable RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 6 answers
  • Subscribers 706 subscribers
  • Views 6928 views
  • Users 0 members are here
  • batteries
  • help
  • pi
  • plug
  • robotics
  • portable_battery
  • raspberry_pi
  • aa
  • battery
  • raspberrypi
  • rpi
  • wireless
  • question
Related

What battery to use for portable RPi?

e14 Contributor
e14 Contributor over 11 years ago

I was planning on making an RPi robot, wireless, of course, and i was wondering what type of battery or battery pack to use (size, voltage, amperage, etc). It would also be helpful to know if i should wire it directly to a male micro usb cable to plug directly into the Pi, or with a female micro usb jack to plug another cable into. If you could give any sugestions as to how to recharge the battery pack, or simply use regular AA batteries, it would be greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 11 years ago

    You don't say how big your robot is. I think that beyond a certain size the Robot it's self will burn more juice than the Pi.

    If it's only small then a few AA rechargeable will be good enough to experiment so say 4.5-6V(4XAA) for the motors and the same again for the PI.Maybe even say 6AA's for the PI thinking about it so you can use a regulator to get a good 5V input to it.

     

    A dual supply is almost always a good idea as the motors of the robot will induce noise on the power line which may be enough to crash/restart the PI or at least have strange behaviour.

     

    Larger robots could use small SLA lead acid batteries as they give lots of current and easy to charge and generally safe enough as long as you respect them. failing that say a Lithium racing pack but they take more care to charge correctly...Nicer solution need to be careful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Problemchild

    The robot I'm planning on making will have a servo motor, a few different sensors, and 2 dc motors. I'm also using a backup display with composite output for the monitor.It probably wont be much larger than 15x20 cm (about 6x9 inches), and 15 cm tall (6 inches). I still need plan out the mechanics for it's arm/club (it's going to hit a golf ball into a hole), but it will probably be made out of plastic or aluminium, with some parts sticking out. I'd like to have the battery near the bottom or back so that the robot isn't topheavy, or tip the bot over when it hits the ball, and so that it can be accessed easily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Problemchild

    The robot I'm planning on making will have a servo motor, a few different sensors, and 2 dc motors. I'm also using a backup display with composite output for the monitor.It probably wont be much larger than 15x20 cm (about 6x9 inches), and 15 cm tall (6 inches). I still need plan out the mechanics for it's arm/club (it's going to hit a golf ball into a hole), but it will probably be made out of plastic or aluminium, with some parts sticking out. I'd like to have the battery near the bottom or back so that the robot isn't topheavy, or tip the bot over when it hits the ball, and so that it can be accessed easily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • toxxn
    0 toxxn over 11 years ago in reply to e14 Contributor

    You will most likely need a couple different power options unless you want one big battery but then you will need a Buck Converter to step down the voltage for the Pi.

    Depending on the servos and DC Motors you plan to use, I would say a battery for the LCD and servo/motors, and another for the Pi.

     

    The TFT LCD you mentioned is about 12v DC 200mA.

    Depending on the Pi version, using model b for example is 5v 700mA and with anything connected to the Pi you will need more than a 700mA supply. I would recommend around 5v 1500-2000mA.