Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum What battery to use for portable RPi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 6 answers
  • Subscribers 706 subscribers
  • Views 6938 views
  • Users 0 members are here
  • batteries
  • help
  • pi
  • plug
  • robotics
  • portable_battery
  • raspberry_pi
  • aa
  • battery
  • raspberrypi
  • rpi
  • wireless
  • question
Related

What battery to use for portable RPi?

e14 Contributor
e14 Contributor over 11 years ago

I was planning on making an RPi robot, wireless, of course, and i was wondering what type of battery or battery pack to use (size, voltage, amperage, etc). It would also be helpful to know if i should wire it directly to a male micro usb cable to plug directly into the Pi, or with a female micro usb jack to plug another cable into. If you could give any sugestions as to how to recharge the battery pack, or simply use regular AA batteries, it would be greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • toxxn
    0 toxxn over 11 years ago

    Lucky enough for projects like this there are a wide variety of different types of batteries one could use, Lipo, Li-ion, ni-cd, etc, or you could even go with a 5v 4x AA battery pack.

    Any hobbyist battery of 4.5-5v with at least 1000mA or higher would be my choice. They are generally small, rechargeable, decently priced, and if you need more amperage, you have that option as they come in a variety. As for size of the battery, that depends on your project and how much space you want to allocate for the battery. As mentioned however, hobbyist batteries are generally quite small and lightweight as they are used in electronics such as RC cars, boats, planes, etc.

     

    You can power the Pi directly using the provided GPIO pins on the board using one of these batteries. I wouldn't alter the battery in any way to adjust how you want to power the Pi as some of these batteries such as Lithium Ion can be very dangerous if misused. If you did not want to use the GPIO's, you could simply just get a connector that fits to the battery and solder on a micro USB.

     

    Just a a word of caution with li-ion batteries, only charge them with the correct method of charging. Otherwise you could create a recipe for disaster as Li-ion's if not charged properly, overcharged, or misused can create quite a powerful chemical reaction that may result in a fire and/or the battery to explode. I tend to stay away from lithium batteries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to toxxn

    Something I have that is long lasting for a four wheel rover is a RC Lipo Battery (11.1V/2600mAh). Works for the motors and I add a 5V/1.5A regulator bypass for the RasPi. Lasts for days and the battery charges in 2hrs. Works as well for the BeagleBone Black.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • toxxn
    0 toxxn over 11 years ago in reply to e14 Contributor

    This is also a great option. Using a Step-Down Module (Buck Converter) you could use a larger voltage battery and increase the mAh drastically.

     

    I have a KIS3R33S USB DC 7V-24V to 5V 3A Step-Down module that I used in a custom Pi power supply I made.

    I recycled an old Bose wall wart that is 12v 1800mA for my custom power supply which allows me to power a small tft lcd (Car reverse monitor) at the same time, while the step-down module allows me to step the 12v down to 5v for the Pi. 2 in 1 power supply. This also leaves me open for a larger voltage battery or a car charger using the same power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Iisn't it much more efficient to use a 5V 1.5 A voltage regulator IC with a couple of small capacitors, one on the input and one on the output, as compared to using a Buck down converter module? I don't know how much conversion loss there is in those Buck modules, but some power must be lost to heat in the DC-> AC -> DC conversion process they use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shumaila
    0 shumaila over 9 years ago in reply to e14 Contributor

    can i use 11.1V 2200mah battery instead of 2600mah battery. plz reply

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago in reply to e14 Contributor

    Generally DC-DC converters are much more efficient than linear regulators. They are also usually more complex and more expensive, but the costs keep coming down. On the drawback side, they can be significantly more noisy, larger and more failure prone.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago in reply to shumaila

    Yes, as long as you use an appropriate voltage regulator/power supply to decrease the voltage to 5V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 9 years ago in reply to shumaila

    Yes, as long as you use an appropriate voltage regulator/power supply to decrease the voltage to 5V.