Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum I need simple python code to run my PI GPIO with channgel relay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 710 subscribers
  • Views 7119 views
  • Users 0 members are here
  • raspberry_pi_getting_started
Related

I need simple python code to run my PI GPIO with channgel relay

e14 Contributor
e14 Contributor over 11 years ago

I have Raspberry Pi B+ and i just bought 8 channel relay. i successfully connected but i really need a simple code to run it to trun on and off the channel relay?

would you please help me

  • Sign in to reply
  • Cancel
Parents
  • nschreiber0813
    0 nschreiber0813 over 11 years ago

    Dear: Simsim

    You should know that it is fairly simple using GPIO. As a matter of a fact I used GPIO to make an LED blink Morse code. You should know the code is simple. Try this in python.

    import RPi.GPIO as GPIO
    import time

    You should know that this basically imports GPIO and time so we can use the GPIO board and use time to control the amount of GPIO we use but it does not do anything else. Try this to turn on the board.

    GPIO.setmode(GPIO.BOARD)

    This will turn on the board try this to create an output.

    number = 37
    GPIO.setup(number,GPIO.OUT)
    GPIO.output(number,True)

    Of course there are many ways to create an output but this is the easiest for me anyways. What the the code does is turns on GPIO 26 to ouput high. to create an input do this.

    GPIO.setup(GPIO.BCM)
    number = 37
    GPIO.setup(number, GPIO.IN)
    GPIO.input(number, True)

    To create a bidrectional (or IO) I don't know. I am sorry but I can't answer that. Next you will need to look at this diagram to help you with your code. Also you should know to look for the diagram relavent to your raspberry pi.

    imageimage

     

    Good luck and bye..

    From: Noah

     

    PS in case you are wondering the pinout above is for B+ the pinout below is for A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nschreiber0813
    0 nschreiber0813 over 11 years ago

    Dear: Simsim

    You should know that it is fairly simple using GPIO. As a matter of a fact I used GPIO to make an LED blink Morse code. You should know the code is simple. Try this in python.

    import RPi.GPIO as GPIO
    import time

    You should know that this basically imports GPIO and time so we can use the GPIO board and use time to control the amount of GPIO we use but it does not do anything else. Try this to turn on the board.

    GPIO.setmode(GPIO.BOARD)

    This will turn on the board try this to create an output.

    number = 37
    GPIO.setup(number,GPIO.OUT)
    GPIO.output(number,True)

    Of course there are many ways to create an output but this is the easiest for me anyways. What the the code does is turns on GPIO 26 to ouput high. to create an input do this.

    GPIO.setup(GPIO.BCM)
    number = 37
    GPIO.setup(number, GPIO.IN)
    GPIO.input(number, True)

    To create a bidrectional (or IO) I don't know. I am sorry but I can't answer that. Next you will need to look at this diagram to help you with your code. Also you should know to look for the diagram relavent to your raspberry pi.

    imageimage

     

    Good luck and bye..

    From: Noah

     

    PS in case you are wondering the pinout above is for B+ the pinout below is for A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to nschreiber0813

    HI Noah

    I was just looking at this post as I am looking for assistance with getting a PI A+ board to run 4 Relays with multiple programs held on the SD Card on the PI board.

    As well as a web page hosted on the board to access via the wifi dongle directly via iPone or Android to run the programs at the push of a button.

    Can you possibly help or be able to point me in the right direction.

     

    Craig