Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum How to address the UART
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 704 subscribers
  • Views 3185 views
  • Users 0 members are here
  • raspberry
  • address
  • on
  • pi
  • raspberry_pi
  • uart
Related

How to address the UART

e14 Contributor
e14 Contributor over 11 years ago

I've been using the article by Peter Jan " Low level programming the Raspberry Pi in C". this was very helpful and I was able to get his program working to toggle I/O pins. My interest is to use the UART to produce control for DMX512 Lighting. It should be possible top get the required 250 KHz baud rate by setting the clock to 16Mhz. Unfortunately he doesn't give an example program for the uart.  The "data sheet" he uses seems to have a typo in the base address for the UART: 0x7e20100, which is missing one digit. I tried 0x7e201000, but that didn't work. Finding the correct address by trial and error has not been productive, (possibly due to an error in my code?). but it would be helpful to start with the correct address. Anyone know the correct address for the UART?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    https://github.com/Pieter-Jan/PJ_RPI

    Has the code you need!image

    http://www.raspberrypi.org/wp-content/uploads/2012/02/BCM2835-ARM-Peripherals.pdf

    This is the datasheet for the RPi but not the new RPi-2!image On p177 I see incorrect address, but use the names on the sheet and the include from source above and you should be fine!

     

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    I've been using that article and looked at the header file, which works with the GPIO pins but there is no reference to the uart.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    I've been using that article and looked at the header file, which works with the GPIO pins but there is no reference to the uart.