Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What is a good waterproof case for a Raspberry Pi and NoIR PiCam?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 4406 views
  • Users 0 members are here
  • raspberry
  • ir_led
  • pi
  • raspberry-pi
  • noir
  • raspberry_pi_projects
Related

What is a good waterproof case for a Raspberry Pi and NoIR PiCam?

dkelley810
dkelley810 over 11 years ago

I have built a birdhouse, with a Raspberry Pi and NoIR in it. But I am having issues with sealing it from the elements.

I had an IR Led light ring that burned out part of circuit. Not sure if it was because of elements.

Also looking to seal up the PiCam for weather.

 

Thank You for any Answers and Ideas.

 

First Version of Birdhouse. - Original location for PiCam and IR LED Ring.

image

 

 

Version 2 - Modified PiCam and IR LED ring location.

image

  • Sign in to reply
  • Cancel
Parents
  • n5xmt
    0 n5xmt over 11 years ago

    I would suggest something like a tupperware container.  seal any holes where water can get in, but you still need holes for ventilation... need to put some kind of louvers over them to keep the elements out.  if the LED ring was connected to the +5v of the Pi itself, that would be why some things fried...  looks like 36 LED's and the 5mm LED's typically require 20-30mA each.  so that makes a total power consumption of 720mA to 1080mA.  Just the Pi itself requires 1000mA.  not sure what the camera draws, but I'd recommend a separate power supply for the LED's

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • n5xmt
    0 n5xmt over 11 years ago

    I would suggest something like a tupperware container.  seal any holes where water can get in, but you still need holes for ventilation... need to put some kind of louvers over them to keep the elements out.  if the LED ring was connected to the +5v of the Pi itself, that would be why some things fried...  looks like 36 LED's and the 5mm LED's typically require 20-30mA each.  so that makes a total power consumption of 720mA to 1080mA.  Just the Pi itself requires 1000mA.  not sure what the camera draws, but I'd recommend a separate power supply for the LED's

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dkelley810
    0 dkelley810 over 11 years ago in reply to n5xmt

    Thank you for the Reply. The IR LED light ring is powered by it separate Power supply AC -12V. I have both the power for the Pi and the ring enclosed in a 20oz Pop bottle. So that is enclosed nicely.

     

    I have a ProtoCam board on order from Kickstarter - https://www.kickstarter.com/projects/955730101/protocam-raspberry-pi-a-b-camera-module-add-on-boa

     

    http://1.bp.blogspot.com/-Ud5T0awnTSU/VJ8NpF-w1nI/AAAAAAAAFmk/4EHnadZLeeU/s1600/Bplus_Main.png

     

    So my plan was to have IR LED's powered from the Pi. After thinking, I may still power it from a separate power source.

     

    My other concern is if I need to work on the Raspberry Pi + NoIR PiCAM + IR LED's, I want to be able to bring the whole module into the house. not the Whole birdhouse. Just in case a bird wants to move in. I want to disturb them, the least as possible.

     

    Thanks for the Ideas!

    Dennis Kelley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to dkelley810

    So my plan was to have IR LED's powered from the Pi

    The Pi does not have a suitable supply to handle that.

     

    I did one here using a 500w floodlight housing, which could work if you mount it above.

    I used a simple transistor to switch the IR leds.

    I'm not sure if birds can see IR, so you may just have a really bright torch shining in ther face.

     

     

    The other housing I'm experimenting with is this.

    image

    I discuss it here.  Mounting 2

     

     

    Mark