Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using a Membrane Matrix Keypad to operate a lock with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 2349 views
  • Users 0 members are here
  • raspberry
  • python
  • help
  • pi
  • gpio
  • electric_lock
  • program
  • lock
  • raspberry-pi
  • code
  • raspberrypi
  • help!
Related

Using a Membrane Matrix Keypad to operate a lock with Raspberry Pi

e14 Contributor
e14 Contributor over 11 years ago

I am very basic with the language of python but I am trying out a project which is an electronic lock.

 

But the problem is that I cant seem to work out how to make a program that asks for a four digit number password and when the correct digits are entered a pin becomes active i.e. turning on or off the lock.

 

The keypad I am using is a Membrane Matrix Keypad.

Here is the keypad schematic:


image


Can someone please help me with making this program?

All feedback will be appreciated



Also Gaven MacDonald has made a video on using this type of keypad if this helps

https://www.youtube.com/watch?v=yYnX5QodqQ4

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    Do you have the code in the video? If so, paste here and I will help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago

    You can use one of those Microchip I/O expanders to drive the keyboard such as the MCP23017 or similar that way you still have lots of I/O to drive the lock release.

    http://www.microchip.com/wwwproducts/Devices.aspx?product=MCP23017

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Yes i do have the code

     

    But this program only shows what you have pressed on the keypad

     

     

    import RPi.GPIO as GPIO

    import time

     

     

    GPIO.setmode(GPIO.BOARD)

     

     

    MATRIX = [ [1,2,3,'A'],

               [4,5,6,'B'],

               [7,8,9,'C'],

               ['*',0,'#','D'] ]

     

     

    ROW = [3,5,8,10]

    COL = [19,21,23,24]

     

     

    for j in range(4):

      GPIO.setup(COL[j], GPIO.OUT)

      GPIO.output(COL[j], 1)

     

     

    for i in range(4):

      GPIO.setup(ROW[i], GPIO.IN, pull_up_down = GPIO.PUD_UP)

     

     

    try:

      while(True):

      for j in range(4):

      GPIO.output(COL[j],0)

     

     

                            for i in range(4):

      if GPIO.input(ROW[i]) == 0:

      print MATRIX[i][j]

      time.sleep(0.2)

      while(GPIO.input(ROW[i]) == 0):

      pass

                                                         

      GPIO.output(COL[j],1)

    except KeyboardInterupt:

      GPIO.cleanup()

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Problemchild

    Thank you for you idea but I would like to control it via a single GPIO output

    i.e. electronic solenoid attached onto GPIO pin and lock opens when pin is set high

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to e14 Contributor

    Yeah using the expander you can read the keyboard drive what ever solenoid you like then have some I/O left for LEDs or whatever all from one SPI/I2C bus on the RPI. It also protects your RPI from any abuses or mis-programing at the expense of one £2 chip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Problemchild

    Ok thank you I will consider using that now and quite honestly for future projects.

     

    But that doesn't answer my original question which is that I need help with the program.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    This code will not work since the indentation is wrong. It will take me a while to correct.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Private message me it when you are done please

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • imrsjs
    0 imrsjs over 6 years ago in reply to e14 Contributor

    hi. do u have the revised code?