Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 Model B Switches/Door Contact Switches
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 1663 views
  • Users 0 members are here
  • raspberry
  • raspberry_pi_get_started
  • breadboarding
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
  • raspberrypi2
Related

Raspberry Pi 2 Model B Switches/Door Contact Switches

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I am new to the Raspberry Pi and I was wondering how I would connect door contact switches (or any kind of switch) to the pins on my Raspberry Pi. I have a Raspberry Pi 2, Model B. The purpose of this so that I could read if the door switches are together, and thus and are sending a voltage through the door switches, and I am aiming to somehow have the Raspberry Pi detect if this voltage has reached it, on one of its pins.  Does anyone have an idea of how I could use this door switches, or any switches, on the Raspberry Pi? I am a beginner in breadboarding and wiring, and I am wondering how exactly I could measure whether or not these door switches are in contact. Please ask if you need more information.

 

Thank you for your help.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Rather than connect direct to the PI, I would use an interface board to provide some level of protection in case of minor errors.

     

    The PI can be used by connecting switches directly of course and this is done all the time in prototypes etc or for a learning excersize

     

    The simples thing I can think of to help would be the PIFace Digital, this provides 8 Digital inputs via a buffer chip and 8 digital outputs (Two of which drive relays), the board is well suppported in the community and by the vendor

     

    here is a link to the canada Newark site http://canada.newark.com/piface/piface-digital-2/io-expansion-board-raspberry-pi/dp/78X5847?mckv=saxFsj780|pcrid|40869928673|plid|&CMP=KNC-GCA-GEN-SKU-PIFACE?gross_price=

     

    Prices will vary from region to region but this is a very popular board to extend the PI

     

    here is more info http://www.element14.com/community/docs/DOC-69001/l/piface-digital-2-for-raspberry-pi

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Rather than connect direct to the PI, I would use an interface board to provide some level of protection in case of minor errors.

     

    The PI can be used by connecting switches directly of course and this is done all the time in prototypes etc or for a learning excersize

     

    The simples thing I can think of to help would be the PIFace Digital, this provides 8 Digital inputs via a buffer chip and 8 digital outputs (Two of which drive relays), the board is well suppported in the community and by the vendor

     

    here is a link to the canada Newark site http://canada.newark.com/piface/piface-digital-2/io-expansion-board-raspberry-pi/dp/78X5847?mckv=saxFsj780|pcrid|40869928673|plid|&CMP=KNC-GCA-GEN-SKU-PIFACE?gross_price=

     

    Prices will vary from region to region but this is a very popular board to extend the PI

     

    here is more info http://www.element14.com/community/docs/DOC-69001/l/piface-digital-2-for-raspberry-pi

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Depending upon how many I/O pins I need I use either an MCP23008 or MCP23017 port expander.  I have an article in the Dec 2014 issue of The MagPi magazine about using two MCP23017s. I also made a PCB for a single MCP23008 that makes hooking up to the Pi easy.  The PiFace includes more than I usually need for a project; it does have the advantage of being able to do lots of things with s single board, however.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Ok thanks, that will help me with my project!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    if you would not mind, can you check the "Correct Answer" or "Helpful Answer" for me then, I need the badge image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to Robert Peter Oakes

    Peter Oakes great answer and I would mark correct as well (if I could). Thanks for the excellent explanation.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Sure, no problem!