Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 Wifi Adapter USB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 704 subscribers
  • Views 3905 views
  • Users 0 members are here
  • raspberry
  • wifi
  • raspberry_pi
  • adapter
Related

Raspberry Pi 2 Wifi Adapter USB

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

 

I'm new in Raspberry Pi. I bought a USB Wifi adapter, and I can't do it works.

I plug it on raspberry pi 2, and this detected the new hardware (with command lsusb the adapter appears in the list).

I checked if the chipset are in the list of compatible, but it isn't compatible, but the raspberry can detect it.

 

Any solution?

 

 

Thanks.

  • Sign in to reply
  • Cancel
  • DAB
    0 DAB over 11 years ago

    Did you follow the instructions on how to add wifi to the RPi 2?

     

    The one that came with the video board kit worked just fine with a few clicks.

     

    Do you have another device that you could put the plug into to see if it can find your local wifi?

     

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to DAB

    Thanks for you help.

     

    I don't know what are those instruccions. I have searched tutorials at Google, but any of them works.

    When I execute ifconfig, only appears eth0 and lo interfaces, never wlan0.

    But in /etc/network/interfaces, wlan0 are configured (I don't know if it's ok)

     

    Yes, I tested the adapter in my laptop, and it works fine (under windows).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 11 years ago in reply to e14 Contributor

    Go to the RPi website and get the new manual for the RPi 2.  They have the procedures included to put the wifi on the board and how to do a snoop for your local wifi.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to DAB

    DAB,

    I have checked on the raspberrypi.org site (is the one you cite?) and I have found nothing new. Please can you post a link where the new PI2 manual can be downloaded?

     

    Thank you. Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 11 years ago in reply to balearicdynamics

    No, I remember know that I got the book from the library and since returned it.

     

    As I remember, just enter sudo raspi-config

     

    Then select configure network.

     

    That should pop up the window where you can scan for your wifi link.

     

    Then just enter your access code and you should be good.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to DAB

    With the command rasp-config it is possible to enable only features, with the option to set-up them loading the corresponding kernel module at startup. I add a document just now with some more information on the Raspberry PI and WiFi usage and settings. I think it maybe helpful.

     

    The following document includes a pdf I collected from the Debian site, I have used to setup the USB WiFi on the Raspberry PI

    http://www.element14.com/community/docs/DOC-77197/l/how-to-use-the-wifi-interface

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deepankarmaithani
    0 deepankarmaithani over 11 years ago

    go to wireless network setting click on the scan button sand you should find the networks around you then it asks for password. Which model/brand do you have? If you would like to buy a new one  or if any one else who is reading this post . EDUP nano adapter EP-N8531 works out of the box on PI-2. it costed me INR 386  on amazon india  which is 6.08 US doller.


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 11 years ago

    Hello hlastras,

     

    I have no idea which USB WiFi adapter you've got, but you said it's listed under lsusb, so that's a start.

     

    If it's also listed under 'iwconfig' and/or 'ifconfig' then it has loaded the driver for it and you're ready to follow the steps here:

     

    https://www.raspberrypi.org/documentation/configuration/wireless/

     

    There's instructions for connecting via the command line at the bottom.

     

    If your device isn't listed under iwconfig or ifconfig, then you'll have to past here what your device identifies as (the full line) from lsusb and we can attempt to identify what driver it should be using - but you may have to recompile it which can take a long time.

     

    Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Please help. I have ordered a new Pi2B for myself and a this new EDUB 8553 wifi nanao adapter. Will it work with Pi?

    EDUP Mini Wireless Wi-Fi Nano USB Adapter Dongle WiFi Dongle EP-N8553 (New) - Buy EDUP Mini Wireless Wi-Fi Nano USB Adap…

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deepankarmaithani
    0 deepankarmaithani over 11 years ago in reply to e14 Contributor

    Hi puneet

    I am not sure about the one you have pointed to but the model below available on the same website definitely works EDUP Mini Wireless N 11n Wi-Fi Nano USB Adapter - Buy EDUP Mini Wireless N 11n Wi-Fi Nano USB Adapter Online at Low Pric…

    There is a page on internet i couldn't find it right now for u, but i have seen it in past that list all the compatible keyboards and wifi dongles. Search google

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>