Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Exploring alternate methods for providing DC power to Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 2 answers
  • Subscribers 700 subscribers
  • Views 13453 views
  • Users 0 members are here
  • raspberry pi power
Related

Exploring alternate methods for providing DC power to Raspberry Pi

colporteur
colporteur over 4 years ago

I'm in need of a battery power solution for a Raspberry Pi?

My plan was to use a 5VDC lithium-ion battery connected via the USB micro connector to power the Pi. I have had to rethink this because of extreme space limitations. The power connector on the Pi makes it a difficult fit in the space that I am using.

My next thought was to connect the battery directly to the 5V and GND pins. I seem to recall that this could be used on Pi's. I then stumbled across an article that suggested, if this method is used, the circuit would require a Universal Battery Eliminator Circuit (UBEC). I have no voltage level issues. The battery supply is 5VDC. Unless the UBED offers some protection I'm not aware of, I don't need its capabilities of managing different input voltages. This shook my confidence of using the pins.

What are your thoughts on providing alternate power to a Pi? Can I do it through the pin header? This is my preferred solution. Are there any requirements I need to be aware of to make this an alternate solution?

  • Sign in to reply
  • Cancel
Parents
  • robogary
    0 robogary over 4 years ago

    Pin header is cool, I've done it. I like to use 7.4V or 11.1V LiPos, and an adjustable buck power supply, fed into a diode , then to the Pi header pins.

    The buck PS can be adjusted for 5V + whatever voltage drop you get across the blocking diode. 

    I tend to overdo the battery size mA hr, if you just want to make it thru the track once , a baby size lipo, maybe  wire qty 2 150mAhr 3.7 V in series would do the trick. 

      https://www.etechnophiles.com/rpi-zero-2w-board-layout-pinout-specs-price/

    The DC-DC converter chip doesnt seem to have  significant transient protections built in. 

    imageimage

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gpolder
    0 gpolder over 4 years ago in reply to robogary
    robogary said:
    Pin header is cool

    how did you do this, what kind of jumper wires did you use, one pin or 2? a Pi 4 can draw 3A, so the connector should be suitable for that. 

    The Chinese jumper wires from my junk box are certainly not.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to robogary

    its still bugging me why I needed 5.5 V onto the 5V GPIO pins. 

    a guess: even though your meters don't show it, the voltage drops under what the Pi needs. Briefly.

    You'd need a fast meter or an oscilloscope on the input that can check - if you set 5V on the pin -
    if that 5V drops somewhere down the boot process. The meter you use doesn't have the capability to do that.

    A fast meter with min/max may be able to check this. Or an oscilloscope in DC mode that is set to trigger on negative flank, level (say) 4.9 V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 4 years ago in reply to Jan Cumps

    The scope is a great suggestion, thank you.   

    I also may need to reconsider the choice of blocking diode. I used a 3A .diode for this test, really want a diode that has a much smaller load dependent voltage drop from 0-3A, like .1 or .2V.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to robogary

    If you suspect that the diode is the cause, you could *test* it without one, with PSU set at 5V.

    It's a lab setup, so the only one that can connect it wrong is you Slight smile. Check 5 times before powering on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gpolder
    0 gpolder over 4 years ago in reply to robogary

    thanks for the thorough test, anyway it is clear that you loose a lot of voltage over the Dupont jumpers.

    Note that the official 3A Raspberry Pi power supply uses 18 AWG cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 4 years ago in reply to gpolder

    18 AWG would do the job for sure. I've had to make my own cables for wire sizes that big using Mate-N-Lock pins and hot glue as a homemade connector housing to keep pin separation & keep the sockets straight on the pins. It does look like an ugly hack job tho.  Please share if you find a nice solution for terminating 18 or 16 AWG wires into the GPIO header. 

    I also considered the standard GPIO ribbon cable, usually at 28 AWG. The case against them is the users dont often feed 5V to the RPI , the pins are used to source 5V for sensor use.  The 40 pin connector tho allows for a good mechanical fit. I'll have to give them a look too, do more measurements to check on voltage drop using multiple conductors in parallel, 2 for 5V and 2 for GND, on both the GPIO ribbon.

    I also need to the load measurements while the RPI is running code, for sure that also has impact.

    At the end, its mostly curiosity, a bigger wire size ultimately the simple answer, as long as it is mechanically stable and has some covering that keeps pins from shorting together. 

    Some of the smaller boards like Zero and Pico can likely get by with a smaller 5V feeder wire size. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anniel747
    anniel747 over 4 years ago in reply to robogary
    This reply was deleted.
    • Cancel
    • Cancel
  • colporteur
    0 colporteur over 4 years ago in reply to robogary

    image

    In the past, if larger gauge wire was used, I would solder the wire to a 2.54 pin. You can crimp it but it can make a mess of the insulation on the wire depending on how thick it is. I then heat shrink to protect the pin. It has worked for me and since I don't have another solution, I will use it again.. This will be the first power connection I have done using this method. I have always managed to make the PS work. This project doesn't afford me a PS.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gpolder
    0 gpolder over 4 years ago in reply to anniel747

    these connectors are 1A per pin, so with two 5V input pins you have 2A max.

    I would propose to buy an official raspberry pi 4 power supply, cut the wire with the cable and throw away the power supply.

    They are really cheap, price is comparable to a bare cable:

    Buy Now

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to gpolder

    I was thinking the same. But colporteur wrote in the first post that there's no room for the USB connector in his design.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gpolder
    0 gpolder over 4 years ago in reply to Jan Cumps

    ok, you are right, forgot about that, I was more thinking for a solution for my own project Sweat smile

    On the other hand he is not using a Pi 4, so in that case it could work with proper pin headers and wiring.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gpolder
    0 gpolder over 4 years ago in reply to Jan Cumps

    ok, you are right, forgot about that, I was more thinking for a solution for my own project Sweat smile

    On the other hand he is not using a Pi 4, so in that case it could work with proper pin headers and wiring.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 4 years ago in reply to gpolder

    much appreciate the input just the same.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 4 years ago in reply to gpolder

    Found these adapter cables on Amazon, sez 16 AWG, I have my doubts on that .....but here is a link to have a look https://www.amazon.com/Jienk-Terminal-Connector-Extension-Screwdriver/dp/B096RQNN8C/ref=sr_1_3?crid=1R8PJRO6AT2FN&keywords=Screw%2BTerminal%2BBlock%2BConnector%2Bto%2BUSB%2BC&qid=1649344174&s=electronics&sprefix=screw%2Bterminal%2Bblock%2Bconnector%2Bto%2Busb%2Bc%2Celectronics%2C132&sr=1-3&th=1

    Another option to backfeeding GPIO with 5V. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 4 years ago in reply to robogary

    Looks interesting, much appreciated. I have been doing some reading about power supplies and their impacts on Pi4s. 16gauge is a step up from the typical 18 found in some power supplies. I have added it to an Amazon wish list for the next time I place an order.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robogary
    0 robogary over 4 years ago in reply to colporteur

    The RPI4 uses the USB-C connector, the link is for that adapter. The RPi 3 uses a micro USB.   https://www.amazon.com/gp/product/B07PJYVH12/ref=ox_sc_act_title_2?smid=A3MDC9KUHU6B27&psc=1

    There are a variety of these adapters depending on the USB type. 

    I'm starting to really like the idea of powering a project this way. It makes it easy to unplug the upstream battery, interlocking & buck power supply, and plug in the AC power supply when doing the project development & debugging.   

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gpolder
    0 gpolder over 4 years ago in reply to robogary

    Looks great indeed, 16 AWG is 1.3 mm diameter, in this case 5 of them in the cable plus insulation, so I guess the cable diameter should be around 8 mm ???? From the image I don't think it is the case. So I share your doubts.

    But worth giving it a try.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to gpolder

    It can be a real pain to power Pi 4 once requirements deviate even slightly from what the official charger offers : (

    For that cable I think it's likely they are specifying 16 AWG for the connector screw-holes, not the attached wire. Still, if the length is short, maybe that could be ok. I had problems with this Anker charger and  what I believe is a good cable, but happened to be long. I swapped out the cable for a cheaper shorter cable (this one), 0.9m length) and now at least the Pi 4 isn't unexpectedly crashing! I've not subjected it to a lot of load though. I like that the charger has figure-8 mains cable.