Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum First experience with a Raspberry Pico - Setup toolchain, IDE, debug and FreeRTOS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 700 subscribers
  • Views 15603 views
  • Users 0 members are here
  • raspberry
  • pico_freertos_smp
  • pico
  • freertos
Related

First experience with a Raspberry Pico - Setup toolchain, IDE, debug and FreeRTOS

Jan Cumps
Jan Cumps over 4 years ago

I got a set of Raspberry Pico boards. This weekend I've worked on getting a C++ development environment set up, IDE (VSCode) and debugger working, and FreeRTOS running.

image

I'm using a Windows 11 laptop.

First activity was to get the toolchain running. I used the Getting Started guide.
To install, I used this automated install. The only thing I would do different than the automated version, is the openOCD build. I believe that the option in Fred27's blog is easier.

When I got the overall toolchain working, I continued with the next part: debug

You can use a second Pico as debug probe. Fred27's blog is again invaluable.

image

As soon as I was comfortable with that - being able to build SDK examples, run and debug them, I started the last part of the path: FreeRTOS.

The Pico has dual cores, and it's one of the Genoa pigs for the new FreeRTOS  Symmetric Multiprocessing (SMP) project. 

I downloaded it, added to VSCode, built, and started the first debug session - on a single core FreeRTOS example. That's where this weekend stops:

image

The future steps will deserve a real blog. How to run RTOS on core A or B. And to interact with the other core in the meantime.

Show All Blog Posts

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 4 years ago

    I got new toys recently too! A Pico W and a Micro:bit V2

    image

    The Micro:bit has an nRF52833 and runs micropython with a long list of interesting APIs to play with,

    https://microbit-micropython.readthedocs.io/en/v2-docs/accelerometer.html

    image

    https://github.com/microbit-foundation/microbit-v2-hardware 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 4 years ago in reply to scottiebabe

    I'm not a fan of micropython. I feel Python is good as scripting language - I've spent the last month using it to automate Unreal Engine. I just don't think it's suited to embedded devices where you want small deterministic complied code,

    Incidentally, the micro:bit is a good candidate if you want to play around with embedded Rust. It can be done on the Pico too, but the micro:bit has better support and examples.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 4 years ago in reply to scottiebabe

    I'm not a fan of micropython. I feel Python is good as scripting language - I've spent the last month using it to automate Unreal Engine. I just don't think it's suited to embedded devices where you want small deterministic complied code,

    Incidentally, the micro:bit is a good candidate if you want to play around with embedded Rust. It can be done on the Pico too, but the micro:bit has better support and examples.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Fred27

    related (I think). When I received the Picos, I did not know what to do with them. I was not going to start learning embedded Python. Nothing because of the language, but I'd like to learn new technology. As a boost, I forced @self to set up an efficient development chain. 

    The enthousiasm came when I saw that it was one of the platforms where you can test out multi core RTOS. That subject is close to my heart. And it looks like this little board is going to be an excellent test bed for learning - no ballast, not a lot on board hardware, most of the options uncommitted and (free) available.

    (side note: my first multi-core experience with FreeRTOS was on a Cypress PSoC kit I got from balearicdynamics. They have some very interesting examples, e.g. using 1 core solely to encrypt/decrypt, or to protect memory, while the other does the business logic.)