Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum MPS MA732 MagAlpha Angle Sensor Kit with Servo Motor - Industrial Sensing
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 700 subscribers
  • Views 1054 views
  • Users 0 members are here
  • raspberry pi
Related

MPS MA732 MagAlpha Angle Sensor Kit with Servo Motor - Industrial Sensing

JoCl
JoCl over 3 years ago

Hi, I'm interested in this kit " MPS MA732 MagAlpha Sensor Kit with Servo Motor-Industrial Sensing" but can't find it on the Farnell site.

Is it still available or can I order it on another site.

Kind regards

JoCl

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    Hi,

    That's a custom kit. The entire kit isn't one order code, it's actually at least three, which will get you a large subset of it:

    image

    All three of those links are on the right side of the page /products/roadtest/rt/roadtests/561/mps_magnetic_angle_p#pifragment-4106=9&pifragment-4100=4

    Once you have all three of those items, then you'll have the majority of the kit described on that page. However, you may also need a microcontroller board (e.g. Arduino Mega is suggested), and also a RS485 adapter board, which can be MAX485 based if you're using a 5V microcontroller board (like Arduino Mega), such as this one: https://www.waveshare.com/rs485-board-5v.htm  if you find you need programmable control of the motor (I needed that capability).

    Note that you'll also need to create a mount for the MA732, this is not part of the order codes above, plus a magnet (ideally a recommended one! [diametrically magnetised] - see the datasheet). A mount could be 3D printed. It is really dependent on your application, what kind of mount you use.

    99 percent of the information you may need is likely in all the roadtest reviews if not in the datasheet, since it was quite deeply roadtested. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    Hi,

    That's a custom kit. The entire kit isn't one order code, it's actually at least three, which will get you a large subset of it:

    image

    All three of those links are on the right side of the page /products/roadtest/rt/roadtests/561/mps_magnetic_angle_p#pifragment-4106=9&pifragment-4100=4

    Once you have all three of those items, then you'll have the majority of the kit described on that page. However, you may also need a microcontroller board (e.g. Arduino Mega is suggested), and also a RS485 adapter board, which can be MAX485 based if you're using a 5V microcontroller board (like Arduino Mega), such as this one: https://www.waveshare.com/rs485-board-5v.htm  if you find you need programmable control of the motor (I needed that capability).

    Note that you'll also need to create a mount for the MA732, this is not part of the order codes above, plus a magnet (ideally a recommended one! [diametrically magnetised] - see the datasheet). A mount could be 3D printed. It is really dependent on your application, what kind of mount you use.

    99 percent of the information you may need is likely in all the roadtest reviews if not in the datasheet, since it was quite deeply roadtested.