Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum So, compadres, this (57) being my birthday, gimme some free advice!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 707 subscribers
  • Views 882 views
  • Users 0 members are here
  • lm75
Related

So, compadres, this (57) being my birthday, gimme some free advice!

D_Hersey
D_Hersey over 9 years ago

I got am a (noobs) model B+  Rpi.  I got an LM75.  I have them connected, the I2C device shows up properly with I2Cdetect.  My question, to which there is no 'right' answer is what computer code should I use here.

 

My background is that I have been coding since 1975.  I know BASIC, Pascal, C, C++ and Prolog pretty well.  I am new to Python, but I do have experience with procedural coding from OpenSCAD.  My OS chops are on the spectrum leading to expertise, somewhere in the middle.  Mostly an apps guy.

  • Sign in to reply
  • Cancel
  • D_Hersey
    D_Hersey over 9 years ago

    I got am a (noobs) model B+  Rpi.  I got an LM75.  I have them connected, the I2C device shows up properly with I2Cdetect.  My question, to which there is no 'right' answer is: What computer code should I use here?

     

    My background is that I have been coding since 1975.  I know BASIC, Pascal, C, C++ and Prolog pretty well.  I am new to Python, but I do have experience with procedural coding from OpenSCAD.  My OS chops are on the spectrum leading to expertise, somewhere in the middle.  Mostly an apps guy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to D_Hersey

    Hi Don,

     

    Happy Birthday!

     

    Most online examples use Python. But if you want to use C, then there is some example I2C code here that you could check out:

    https://github.com/shabaz123/lcd3

    To simplify things I created a few high-level functions that are defined in i2cfunc.h.

    The actual underlying control is standard linux kernel i2c driver, I just wrapped it up with a tiny bit of code to make a more friendlier (to me)

    API than the standard one.

     

    To download the code type

    git clone https://github.com/shabaz123/lcd3.git

     

    The, follow the instructions at the section titled 'Software' at this URL:

    Building a Low Power Compact LCD Display

     

    Replace the code with the code below, which is a guess for LM75 (this code isn't tested and is also missing any error handling); if there

    is a permissions issue then try running as root user. If it still doesn't run, check to see that /dev/i2c-1 exists. You also may need to change the

    #define address value depending on what address is hard-coded on your LM75 board.

     

    I hope it works but it is untested. The code at github did work with an I2C LCD. And I have used the I2C library for several different I2C devices, just not the LM75 yet.

     

     

    #include <stdio.h>
    #include "i2cfunc.h"
    
    
    // look to see if /dev/i2c-x exists
    // (where x is usually 1):
    #define I2CBUS 1
    
    
    // LM75 address range is 0x48 to 0x4f depending on A2..0 values
    #define LM75_ADDR 0x48
    
    
    int handle;
    unsigned char buf[2];
    
    
    int
    main(void)
    {
      
      handle=i2c_open(I2CBUS, LM75_ADDR);
    
      i2c_read(handle, buf, 2);
      
      printf("temperature register values read are 0x%02x, 0x%02x\n", buf[0], buf[1]);
      
      i2c_close(handle);
      return(0);
    }

     

    There are probably other Pi-friendly libraries for GPIO and I2C, however I like using my library since it is portable and works with the BeagleBone black too, and doesn't have API names with the text 'Pi' in it.

     

    However, most on-line code examples for the Pi will probably use Python, which is not a language I'm familiar with to any real extent.

    If you're interested in using Python, the magpi PDF magazines will likely have lots of info (there is a search capability but sadly it isn't very good). https://www.raspberrypi.org/magpi/

    There is some general Pi GPIO information here, although I2C is not covered; the information is about a year old though, but most of it is still relevant although it doesn't mention the Pi 3 (since this wasn't available at that time):

    Raspberry Pi GPIO Explained

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago

    Happy Birthday Don, I am really glad that Shabaz jumped in there and gave you a good answer. You young guys are so quick with all this computer coding stuff. Have fun with the Rpi.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 9 years ago

    Happy birthday. If you prefer C to Python, wouldn't this be a suitable starting point?

     

    https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/hwmon/lm75.c

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago

    Yeah, there really is no correct answer. Python is fairly simple to learn and much of the low level stuff is abstracted out.

     

    I've done a few blog posts here on e14 and I've alternated between C and python. There are some cool toolkits available for python, such as flask which can allow you to easily make data read from sensors available via a URL.

     

    It's probably not a bad answer to get familiar with both C and python.

     

    Happy birthday!!!

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago

    Hi Don,

     

    Congratulations on your milestone.

     

    With an RPi, python is pretty easy to learn.

     

    You could go to Sketch, but with your experience python would be a better choice.

     

    DAB