Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum What would you like to see tested on the Raspberry Pi 4?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 50 replies
  • Subscribers 713 subscribers
  • Views 7564 views
  • Users 0 members are here
  • raspberry pi 4 testing
Related

What would you like to see tested on the Raspberry Pi 4?

cstanton
cstanton over 7 years ago

We have a couple of these in the office that we can run software / test some things on - so what would you like to see tested on the hardware that would help to swing the decision for you as to whether or not it's worth it?

 

I've seen a few questions about Sega Rally running on MAME, questions about h264 encoding, realtime transcoding - for some of these I'd have to find the software/setup but it's certainly do-able.

 

So let me know, what do you want to see tested on the Pi 4?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 7 years ago

    I'd like to see the maximum digital  IO toggle rate from a C programme.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 7 years ago

    I'd like to see the maximum digital  IO toggle rate from a C programme.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rew
    rew over 7 years ago in reply to michaelkellett

    When there wasn't anything like a raspberry pi GPIO library I wrote my own. You had to run that as root: It mmap-ed the GPIO module hardware. Then you'd be able to get into the tens of MHz range, maybe even hundreds (but the physical pin hardware will stop responding before that!)

     

    When you go through the Linux GPIO driver, I'd expect something in the order of 100-1000 kHz....

     

    Update:
    Ran the test. With "wiring pi" (blink example from: https://elinux.org/RPi_GPIO_Code_Samples  ) you get 10MHz. It seems to do the mmap that I thought would get decent performance.

    I tried a second "gpio access method"  (BCM library), but that failed the test (as in I couldn't get it to work on short notice).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • gpolder
    gpolder over 7 years ago in reply to michaelkellett

    rpitx (https://github.com/F5OEO/rpitx ) can go up to 1500MHz (I expect on a Pi 3) would be great to know the upper limit on the Pi 4.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to rew

    I think there maybe was a hard 250MHz physical I/O ceiling, because on an old Pi (I think Pi 2), in C code, with the WiringPi library (which offers an Arduino-like API) I was able to get a signal of approx 5.8MHz by toggling a pin up and down using the digitalWrite command (and compared it with Python etc here:  Raspberry Pi GPIO Explained  ) but the jitter was on certain discrete boundaries, i.e. the I/O seems to be clocked out at some rate of 250MHz, too fine to be from just usual context switching. I couldn't find any documentation at the time to support or un-support this theory though.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to rew

    Sorry, just saw your update. Very cool, 10MHz sounds about right, given the Pi 2 managed 5.8MHz.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to rew

    Thanks for the info - I'll take a look at that.

     

    I've finally bought a PI - CPC had 2GB Pi 4 in stock. I've got it booted up and now I had better make it do something.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gpolder

    Huh, I do have a HackRF One...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gpolder
    gpolder over 7 years ago in reply to cstanton

    that's great, that one will go up to 6 GHz.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 7 years ago in reply to shabaz

    Just FYI: This sounds plausible: The GPIO module is probably clocked at that 250Mhz. On simpler ARM processors like the STM32 family the same happens: the CPU core runs at some frequency and then you get a bunch of choices for the IO module clocks and bus clocks. Sometimes completely separate from the CPU clock sometimes your choice is restricted to "div2" or "div 1 or div2 as long as the result is below xxx". For the BCM2711 hardware running the IO modules at 250MHz base clock sounds reasonable.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to rew

    Using the link you provided I've got direct register access pin toggling working from C.

    Early days yet and I'll post some scope traces once I've made some high speed Pi compatible probes.

     

    First thing:

    The peripheral base address is 0xFE000000. It  took some time to find this - as ever the official documentation is poor (absent - there are broken links in the hardware documents on the RPi site). On the plus side it was on the RPi forum that I found the answer:

    https://www.raspberrypi.org/forums/viewtopic.php?f=33&t=244031

     

    I tweaked the code (from https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Felinux.org%2FRPi_GPIO_Code_Samples )  to make a burst of 4 pairs of:

    GPIO_SET = 127;

    GPIO_CLR = 127;

     

    I'd set this up so I could only reach it with a 200MHz scope with cheapo probes.

    The pins/probe/scope  can't toggle anything like fast enough but it looks as if the best interval between peaks is 10ns, implying a peak pin update rate of 200MHz and a toggle rate of 100MHz.

     

    I'll need to make a probe that plugs directly onto the header and move the whole caboodle to somewhere near enough to the 1GHz scope to measure the best that can be done.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 7 years ago in reply to michaelkellett

    Nice work! :-)

     

    I'd recommend not letting this run for minutes at a time. Consider running it for one second, and then let things cool for say ten. It is possible you'd overheat the IO pad if you keep going. When you toggle the IO pin at 100MHz oir more, the "outside" acts as a short. So for the chip it "feels" as if you order it to make the pin high, but then short the pin to ground. You wouldn't be surprised if that breaks things, so you shouldn't be if you try to toggle at 100MHz.

    Stuff like PCIE gets low swing output pads, and an encoding that ensures the pads get the lowest possible number of transitions to encode the datastream. 

    • Cancel
    • Vote Up +3 Vote Down