Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Making a Custom RP2040 Project with KiCad, Part 1!
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 24 Jun 2026 3:25 PM Date Created
  • Views 1313 views
  • Likes 9 likes
  • Comments 32 comments
  • kicad
  • pico
  • rpiexpert
  • rp2040
  • raspberry_pi_projects
  • pi pico
Related
Recommended

Making a Custom RP2040 Project with KiCad, Part 1!

shabaz
shabaz
24 Jun 2026

Partly out of curiosity, and partly to test some aspects of a workflow for other projects, I decided to create a custom RP2040 board. In most cases, there’s no need to do this; it may well be more expensive than simply using a ready-made Raspberry Pi Pico module and mounting it on a custom PCB, while saving a considerable amount of effort.

This short blog post describes how I’m approaching the project. It’s very much a work in progress.

The first thing I did was download the RP2040 hardware design guide PDF, and the minimal RP2040 design KiCad zip file from the Raspberry Pi website and extract and open the design with KiCad 10. This is what the minimal schematic looks like (click to enlarge):

image

The corresponding PCB layout is shown below. My plan is to reuse parts of this design while adapting it to fit the shape and requirements of my own PCB:

image

By examining the minimal PCB layout, it was possible to see that nearly all traces were on the top layer, with just a few on the underside, leaving the majority of the bottom copper being a ground plane.

Next, I modified the schematic by removing the components I didn’t need and adding the functionality I wanted. For example, I removed the pin headers and the Micro-B USB connector, replacing the latter with a USB-C connector. I also added RS-485 circuitry to one of the UART ports, since the board is intended to function as an RS-485 adapter.

You’ll also notice a 10-pin connector that appears to be underutilised. That’s intentional. I plan to route several unused GPIO pins to that connector in case I need them later. I haven’t assigned specific GPIOs yet; I’ll wait until the connector has been placed on the PCB so that I can choose whichever pins are physically closest. Anything that makes trace routing a little easier is worth considering!

image

With the schematic updated, I switched to the PCB editor and took a screenshot of the original layout for reference. I then selected the main central portion of the circuitry and moved it onto my new PCB outline.

image

The result looked promising:

image

The original design includes a top-layer +3.3 V copper fill zone, and I wanted to preserve part of that arrangement. To do this, I simply created a new fill zone and roughly followed the outline of the original design, almost like connecting the dots.

image

Once that was done, I moved the new fill zone into its final position. In hindsight, it would have been easier to create the fill zone first and move it together with the rest of the circuitry, but it only took a few moments to fix. The layout was already starting to come together nicely.

image

Next, I selected the voltage regulator section from the original PCB and moved it into the desired location on the new board. Since I no longer needed any of the remaining elements from the original PCB layout, I deleted them. At this point, the project had effectively become a normal PCB design exercise, with the remaining tasks being component placement and trace routing.

image

I’ll write a Part 2 (EDIT: Here is part 2: (+) Getting Custom RP2040 Boards Produced and Assembled with KiCad, Part 2! - element14 Community ) once the layout is complete. I suspect it will be an even shorter post, since everything appears to be progressing smoothly so far.

Thanks for reading!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 1 month ago +2
    I wonder if the Raspberry Pi people every got one of these PCBs assembled.. they have traces not running through the center of pads. These are lightweight 0402 parts, they will rotate as the solder reflows…
  • arvindsa
    arvindsa 1 month ago +1
    I came here from your Part 2 of this post. Looking at the PCB Layout of the original PCB, I see a lot of polygon on top layer for the 3.3V Net. Now before I say something more, I have to say that I believe…
  • arvindsa
    arvindsa 1 month ago in reply to geralds +1
    I know that the pcb was from 3rd party. I put the question to Shabaz for his take on the originaldesign cos he would have studied the original design with more context. If RPi foundation made it for maker…
  • shabaz
    shabaz 1 month ago in reply to geralds

    Hi Gerald,

    Thanks for this! I had swapped to 0603 resistors for the USB wires, just to pass the signal through the center of one, but I like your idea better, to use the vias. I also realized I'm adding $0.70 to the cost of each USB connector for through-hole soldering, so with hindsight it would have been better to have chosen a SMD connector part. I have written up the findings here:

    (1) Getting Custom RP2040 Boards Produced and Assembled with KiCad, Part 2! - element14 Community

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds 1 month ago in reply to shabaz

    Hi  shabaz 

    Now, this is the first version, it's not finished yet, but the important component ist inserted - the USB C receptacle.

    I've modified completely the USB C receptacle, including all pins, renaming, renumbering, component drawings, 3D image.
    Then I placed it in the schematic and routed the PCB area around the USB receptacle.
    The routing of the data-wires was in pair-routing.
    I think this is a possible way around this component. - This is just the first version, not yet improved.

    RP2040_minimal-edit.zip

    RP2040-minimal-edit-sch

    RP2040-minimal-edit-pcb image

    After the resistors for the D- I inserted two vias. I hope that is no problem for the data transfer speed, because the D- is a bit longer than the D+.
    Maybe this is usage for you, hopefully.

    minimal-edit_3D_top

    minimal-edit_3D_bot

    - You have drawn another PCB profile, as well your needing of the other components; I will do this next.

    Then, yes, I also imported the Ki-Cad files into the Fusion360 E-Cad (Eagle is now dead since July 2026) system without any errors.
    This works also very well. super.
    I the attachments you'll find the Ki-Cad files, I work with the last version 10.0.3.

    Best Regards
    Gerald
    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 1 month ago

    Very good post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to wolfgangfriedrich

    Hi! Yes, it's all pretty awful. In some places they've literally just got one ground via, and then several thermal relief connections to +3V3. They cannot have prepared this design very carefully. I've been making these sorts of changes:

    image

    However, annoyingly I need to redo most of the board, because I just realized they are using KiCad default 0402 pads.. they are oversized. I'm replacing them all, which means all traces no longer connect, so I now have to rip up trace endings and reattach.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago in reply to shabaz

    Something else I noticed after you talked in an above comment about copper balance around pads. C15 and C16 are in danger of tombstoning, as one side is connected through 3 wide thermal traces and the other side is just a single small trace. 

    image

    The solder on the ground pads will melt earlier and pull the 0402 parts up, before they can connect to the +3V3 side. The thermal relief connection might not be enough with 3 thick trace going into a small pad. Similar for C1 and C3 but they are 1206 or 0805, their weight might be enough to counter to tombstoning. And from EMI perspective it is a good practice to have a think and as short as possible trance from decoupling caps to the via into the GND plane. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>