Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi 3 Cooling / Heat Sink Ideas
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 3 Mar 2016 5:03 AM Date Created
  • Views 22637 views
  • Likes 20 likes
  • Comments 142 comments
  • pi 3
  • heatsink
  • rpibeginner
  • heat_sink
  • rpi3
  • raspberry_pi
  • heat sink
  • rpi
  • raspberry_pi_projects
Related
Recommended

Raspberry Pi 3 Cooling / Heat Sink Ideas

shabaz
shabaz
3 Mar 2016

Note: This is part 1 of a 2-part post. For part 2, click here: Raspberry Pi 3 Dynamic Current Consumption, Power and Temperature Tests

To see an implementation using a heat pipe, see the Outdoor Pi 3 Image Recognition Security Camera project (aka HAL-CAM 9001)

image

Inspired by Christopher's cstanton  Raspberry Pi Operating Temperature report (with thermal photos from Gareth Halfacree) regarding the heat dissipated by the Broadcom chip on the Raspberry Pi 3, and the discussion with bwelsby we started searching around for ways to keep the Pi cool.

Ceramic heat sinks have an innovative structure (vias or micro-pores) which allow a heightened thermal conductivity compared to traditional aluminium heat sinks. They also can have the advantage that they won't affect radio frequency (RF) communications as much, when positioned close to the wireless antenna that is present on the Pi 3.

Furthermore, ceramic heat sinks are not electrically conductive and therefore there is no risk of accidentally shorting something on the Pi.

Back-of-the-envelope calculations (we don't have all parameters since we don't have a copy of the Broadcom datasheet to examine the device operating conditions in detail, nor a copy of the schematic to examine if we can measure device power consumption isolated from the remainder circuitry) suggests that a heat sink with thermal resistance of around 10 degrees C/W might be effective to keep the Broadcom chip's internal temperature below 120 degrees C when the ambient temperature is below around 40 degrees C. These are guesstimates until practical measurements have been taken.

image

Armed with this information, I searched for a suitable sized heat sink and I found a cheap aluminium one. However bwelsby and cstanton suggested that there may be issues with the heatsink getting in the way of connected HAT boards on top of the Pi, and Brian suggested examining ceramic heatsinks.

In summary, I think these parts may be suitable although measurements still need to be done:

22x22x2.5mm MPC222225T22x22x2.5mm MPC222225T

15x15x2.5mm MPC151525T15x15x2.5mm MPC151525T

(Optional) 20x20x10mm 5V DC fan MC33873(Optional) 20x20x10mm 5V DC fan MC33873

(EDIT: after some discussions below, it looks like this Sunon 'DR-MagLev' design fanSunon 'DR-MagLev' design fan is a far better choice, it is 25x25x10mm, quieter, higher throughput, and more efficient with overall lower power consumption. There is also a 25x25mm finger guard25x25mm finger guard).

 

The Broadcom chip is about 14x14mm in size, and ceramic heat sinks do exist in approximately that size. However it is possible to attach a larger heat sink if desired.

The photo below shows the parts that were examined. All of these ceramic heat sinks come with adhesive tape on the underside; the protective tape is removed and the heat sink will stick to the top of the integrated circuit.

The photo at the top of the blog post shows the largest 22x22mm ceramic heatsink.

image

The photo below shows a heat sink closer to the size of the Broadcom chip, 15x15mm. It also shows a 10x10mm heat sink on top of the USB hub/Ethernet controller chip, however this is really not needed. It doesn't get very hot according to the thermal photos in the previous blog post.

image

The memory chip on the underside gets hot too. If desired, the 15x15mm heat sink could  be attached there too. The 22x22mm one is too large for that location due to nearby components (the memory chip has a lower height than the Broadcom chip on the top side).

image

So, I plan to attach a 22x22mm part to the Broadcom chip on the top of the board, and possibly a 15x15mm heat sink to the memory chip on the underside. I don't think a fan will be needed unless a very small enclosure with no natural ventilation was used, or if the Pi was in a very warm environment.

In that case, a fan may be an option. I tried the MC33873 fanMC33873 fan and it generates a usable level of air that can be felt from a distance of 10cm or more. However it does generate a small amount of noise too (possibly inaudible if the Pi will be behind other items such as a TV, but I think there is still a risk it could be audible. The voltage could be reduced from 5V to lessen the noise). It could be mounted on the heat sink as shown here although I think a small gap would be good to allow forced air to hit the entire top face of the heat sink. (The red dot on the fan was placed by me so that I could see it spinning). The fan could be secured with epoxy adhesive. The overall height is less than the height of the USB connectors on the Pi 3. The problem with this is that a HAT board cannot be plugged on top if there is a fan in the way.

image

A very nice solution would have been to put the fan on the side (to the left side of the photo above) so that the fan could blast air across the entire top face, and the underside of the board. However the display connector (the long white thing on the edge of the board in the photo above) is in the way and would block the flow of air which is extremely unfortunate. The Pi 3 wasn't designed with air flow in mind : ( However it might be possible with some 3D-printed duct design to achieve something that could work.

 

To summarize, some heat sinking ideas have been suggested however it is for further examination to see how well they perform. It will be good to see what solutions people come up with over time.

  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 10 years ago in reply to shabaz +6
    I received the ceramic heatsinks today but not the fans they didn't get shipped till today. I have quickly designed a small case to 3D print as a test, and I shall make a dummy HAT too. I can then play…
  • shabaz
    shabaz over 10 years ago +5
    There is a 1-page article on the heat topic in magpi: So it looks like the fix they have implemented is more aggressive throttling through software changes. The wording is interesting in places.. it is…
  • shabaz
    shabaz over 10 years ago in reply to clem57 +4
    Hi! They are the real thing, they actually look like that. They look like school erasers don't they ; ) I remembered I had these heat sinks around from another project. Might try getting some measurements…
  • clem57
    clem57 over 10 years ago in reply to shabaz

    We are ready for some baked Pi image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to clem57

    Close.. : ) You were along the right lines.

    It was a baking tray!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to shabaz

    Is that picture of a Pi 3 inside a sink drain?

    Clem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to bwelsby

    I drilled a 2.3mm partial hole in mine, drilled to just stop short of egressing to the other side.

    The datasheet said the maximum diameter for the thermistor I'm using is 2.4mm) but with hindsight I should have started with 2.0mm or 2.1mm, because the resultant hole was too large for a friction-fit.

    image

    Luckily I had some (9-years expired!) "Gap Filler 2000" that still seems to work lol.

    After curing it possesses a 'dried plasticene' like consistency, and holds the part in place (it is not intended to be

    as strong as an epoxy adhesive, more for gap filling thermal purposes).

    This is the final result:

    image

    The thermistor protrudes slightly as can be seen, your thermistor is slightly smaller and is probably a better choice.

    Still, most of the protrusion is the part of the wires that are coated in the thermistor's shell epoxy material, and the body

    of the thermistor is within the heat sink.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to shabaz

    shabaz wrote:

     

    And the last pad has a 'P' marked on the silkscreen just like the 25mm Sunon one, perhaps to indicate PWM.

    Looks like these fans are very ideal for modifying to get this additional functonality.

    Yes I just tested, pad 3 produces the speed pulse and pad 4 controls speed with a PWM input signal.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>