Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog Raspberry Pi 3 Cooling / Heat Sink Ideas
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 3 Mar 2016 5:03 AM Date Created
  • Views 22631 views
  • Likes 20 likes
  • Comments 142 comments
  • pi 3
  • heatsink
  • rpibeginner
  • heat_sink
  • rpi3
  • raspberry_pi
  • heat sink
  • rpi
  • raspberry_pi_projects
Related
Recommended

Raspberry Pi 3 Cooling / Heat Sink Ideas

shabaz
shabaz
3 Mar 2016

Note: This is part 1 of a 2-part post. For part 2, click here: Raspberry Pi 3 Dynamic Current Consumption, Power and Temperature Tests

To see an implementation using a heat pipe, see the Outdoor Pi 3 Image Recognition Security Camera project (aka HAL-CAM 9001)

image

Inspired by Christopher's cstanton  Raspberry Pi Operating Temperature report (with thermal photos from Gareth Halfacree) regarding the heat dissipated by the Broadcom chip on the Raspberry Pi 3, and the discussion with bwelsby we started searching around for ways to keep the Pi cool.

Ceramic heat sinks have an innovative structure (vias or micro-pores) which allow a heightened thermal conductivity compared to traditional aluminium heat sinks. They also can have the advantage that they won't affect radio frequency (RF) communications as much, when positioned close to the wireless antenna that is present on the Pi 3.

Furthermore, ceramic heat sinks are not electrically conductive and therefore there is no risk of accidentally shorting something on the Pi.

Back-of-the-envelope calculations (we don't have all parameters since we don't have a copy of the Broadcom datasheet to examine the device operating conditions in detail, nor a copy of the schematic to examine if we can measure device power consumption isolated from the remainder circuitry) suggests that a heat sink with thermal resistance of around 10 degrees C/W might be effective to keep the Broadcom chip's internal temperature below 120 degrees C when the ambient temperature is below around 40 degrees C. These are guesstimates until practical measurements have been taken.

image

Armed with this information, I searched for a suitable sized heat sink and I found a cheap aluminium one. However bwelsby and cstanton suggested that there may be issues with the heatsink getting in the way of connected HAT boards on top of the Pi, and Brian suggested examining ceramic heatsinks.

In summary, I think these parts may be suitable although measurements still need to be done:

22x22x2.5mm MPC222225T22x22x2.5mm MPC222225T

15x15x2.5mm MPC151525T15x15x2.5mm MPC151525T

(Optional) 20x20x10mm 5V DC fan MC33873(Optional) 20x20x10mm 5V DC fan MC33873

(EDIT: after some discussions below, it looks like this Sunon 'DR-MagLev' design fanSunon 'DR-MagLev' design fan is a far better choice, it is 25x25x10mm, quieter, higher throughput, and more efficient with overall lower power consumption. There is also a 25x25mm finger guard25x25mm finger guard).

 

The Broadcom chip is about 14x14mm in size, and ceramic heat sinks do exist in approximately that size. However it is possible to attach a larger heat sink if desired.

The photo below shows the parts that were examined. All of these ceramic heat sinks come with adhesive tape on the underside; the protective tape is removed and the heat sink will stick to the top of the integrated circuit.

The photo at the top of the blog post shows the largest 22x22mm ceramic heatsink.

image

The photo below shows a heat sink closer to the size of the Broadcom chip, 15x15mm. It also shows a 10x10mm heat sink on top of the USB hub/Ethernet controller chip, however this is really not needed. It doesn't get very hot according to the thermal photos in the previous blog post.

image

The memory chip on the underside gets hot too. If desired, the 15x15mm heat sink could  be attached there too. The 22x22mm one is too large for that location due to nearby components (the memory chip has a lower height than the Broadcom chip on the top side).

image

So, I plan to attach a 22x22mm part to the Broadcom chip on the top of the board, and possibly a 15x15mm heat sink to the memory chip on the underside. I don't think a fan will be needed unless a very small enclosure with no natural ventilation was used, or if the Pi was in a very warm environment.

In that case, a fan may be an option. I tried the MC33873 fanMC33873 fan and it generates a usable level of air that can be felt from a distance of 10cm or more. However it does generate a small amount of noise too (possibly inaudible if the Pi will be behind other items such as a TV, but I think there is still a risk it could be audible. The voltage could be reduced from 5V to lessen the noise). It could be mounted on the heat sink as shown here although I think a small gap would be good to allow forced air to hit the entire top face of the heat sink. (The red dot on the fan was placed by me so that I could see it spinning). The fan could be secured with epoxy adhesive. The overall height is less than the height of the USB connectors on the Pi 3. The problem with this is that a HAT board cannot be plugged on top if there is a fan in the way.

image

A very nice solution would have been to put the fan on the side (to the left side of the photo above) so that the fan could blast air across the entire top face, and the underside of the board. However the display connector (the long white thing on the edge of the board in the photo above) is in the way and would block the flow of air which is extremely unfortunate. The Pi 3 wasn't designed with air flow in mind : ( However it might be possible with some 3D-printed duct design to achieve something that could work.

 

To summarize, some heat sinking ideas have been suggested however it is for further examination to see how well they perform. It will be good to see what solutions people come up with over time.

  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 10 years ago in reply to shabaz +6
    I received the ceramic heatsinks today but not the fans they didn't get shipped till today. I have quickly designed a small case to 3D print as a test, and I shall make a dummy HAT too. I can then play…
  • shabaz
    shabaz over 10 years ago +5
    There is a 1-page article on the heat topic in magpi: So it looks like the fix they have implemented is more aggressive throttling through software changes. The wording is interesting in places.. it is…
  • shabaz
    shabaz over 10 years ago in reply to clem57 +4
    Hi! They are the real thing, they actually look like that. They look like school erasers don't they ; ) I remembered I had these heat sinks around from another project. Might try getting some measurements…
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    I'm thinking of trying something like this, they are replacements for screw basically! So reduced vibration into the enclosure.

    No idea how effective they are, some reviews are good some bad (but I'm betting the bad reviews are where people had nothing in-between the fan and enclosure).

    Akasa AK-MX003 - computer cooling components (Black): Amazon.co.uk: Computers & Accessories

    Also for the cushioning between the fan and enclosure, for that I might just try some black foam (as used on fan filters) just cut

    into a thin strip along each edge perhaps.

    EDTI: bwelsby also had a suggestion of a rubber draft seal, that might be a better option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rive

    I have used Evercool 40x40 and 80x80 fans before in cases.  They do the job but there was always residual noise.  Maybe I should revisit the mountings and the fan positions.

     

    Thanks for the information.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rive
    rive over 10 years ago in reply to e14 Contributor

    No holes drilled in case. It is velcro pads cut to strip size with scissors... if you look very closely at the images of the case and attached fan above, you will see where the white velcro is attached. The Velcro is very strong, and I can easily lift the whole pi3 just by the fan itself.

     

    You can get a whole pack of like 18 for like $3 at walmart. There is practically no heat where the fan is in any event. No noticeable vibration/noise. The pads are holding up good so far. If in a few months, or a year, or whenever the velco doesn't hold as well, then I will simply remove the old and add some new.  Double sided sticky tape works too. Something to give it a grip. Whatever works for you. You can get .30 cent foam sheets in crafts at walmart, cut them for vibration pads and adhere them if that is what you want to do.

     

     

    You should not use Cpuburn  If your pi3 is not properly cooled.

     

    MMMRF7120X.jpg

     

    The fan is removable... e.g., I can take it off If I want to reassemble the case top and side. I probably won't though (unless I comment out the overclocks). In any event, the heatsink needs ventilation. A heatsink without air movement/convection is useless.

     

    As for obtaining the fan, just google it.  Micro center carries them for like $7.99. No particular branding.The one I have is just a generic 12v 70mm x 70mm x 10mm.

     

    Evercool 70mm Case Fan EC7010M12CA FAN-EC7010M12CA - Micro Center

    0348038_248880.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rive

    rive  Followed the embedded link from the video to https://www.raspberrypi.org/forums/viewtopic.php?f=63&t=144391

    • Did you drill holes into the case to mount the fan or is it a 100% velcro mount?  Velcro wears (E.g. stretches), especially when exposed to heat.
    • Any noticeable vibration and noise from the fan or its mounting while in operation?
    • The 12V 70mm x 70mm x 10mm fan sells for $4?  Brand and make?  I  have had some noise lemons in the past.  You may have found a quiet effective fan!
    • You stated that the fan "is removable" but would you remove its cooling protection, given your config.txt?

     

    Folks, note the WARNING and "Use at your own risk" in the assembly language source code (cpuburn-a53.S).  An unlucky customer could lose their RPi3 when stress testing.  Monitor carefully.

     

    By the way, the source code for cpuburn-a53.S seems to have moved to:

    https://raw.githubusercontent.com/ssvb/cpuburn-arm/master/cpuburn-a53.S

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rive
    rive over 10 years ago in reply to shabaz

    Yes. Fan is operating at 5v on GPIO pins 4/6. Very quiet.

     

     

    For those who want to test their pi's, and determine whether it is sufficiently cooled or not:

     

     

    STRESS

    sudo apt-get install stress
    stress --cpu 4 & watch '(vcgencmd measure_temp; vcgencmd measure_clock arm)'

     

    CPUBURN-A53

    wget https://raw.githubusercontent.com/ssvb/cpuburn-arm/master/cpuburn-a53.S
    gcc -o cpuburn-a53 cpuburn-a53.S
    ./cpuburn-a53 & watch '(vcgencmd measure_temp; vcgencmd measure_clock arm)'

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>