Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi 2 Model B 1GB Technical Specifications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 23 Jan 2015 4:01 PM Date Created
  • Last Updated Last Updated: 10 May 2021 7:09 PM
  • Views 32988 views
  • Likes 6 likes
  • Comments 62 comments
Related
Recommended

Raspberry Pi 2 Model B 1GB Technical Specifications

image

image

The Raspberry Pi 2 Model B 1GB
6X Faster

Learn More

 

Buy NowBuy Now

 

Benefits  image
Technical Specifications  image
Features  image

Benefits:

Get personal with your Pi. Welcome to the Raspberry Piimage 2, the single board computer that thinks it’s a home PC.

Enhanced Quad Core Processor and 1GB RAM now provides you with the opportunity to:

  • Build your own workstation – create and manage your documents and spreadsheets with ease using LibreOfficeimage
  • Faster and more enjoyable gaming – experience less lag and more seamless gaming in all your favourites. Can’t wait to demolish buildings in Minecraftimage, trigger your TNT now and be amazed by the results!
  • No more buffer face – boots up Raspbian in less than half the time as the Model B+
  • More power for your favourite projects – create Space Progammes, Time Lapse Videos, GPS tracking, HD audio and lots more with a full ecosystem of supporting accessories.
  • All your previous Raspberry Pi projects are 100% backward compatible with the new Raspberry Pi 2 Model B 1GB

Technical Specifications:

  • Broadcom BCM2837 Arm7 Quad Core Processor powered Single Board Computer running at 900MHz
  • 1GB RAM
  • 40pin extended GPIO
  • 4 x USB 2 ports
  • 4 pole Stereo output and Composite video port
  • Full size HDMI
  • CSI camera port for connecting the Raspberry Pi camera
  • DSI display port for connecting the Raspberry Pi touch screen display
  • Micro SD port for loading your operating system and storing data
  • Micro USB power source

Raspberry Pi 2 Model B Features:

  • Broadcom BCM2837Arm7 Quad Core Processor powered Single Board Computer running at 900MHz
  • 1GB RAM so you can now run bigger and more powerful applications
  • Identical board layout and footprint as the Model B+, so all cases and 3rd party add-on boards designed for the Model B+ will be fully compatible.
  • Fully HAT compatible
  • 40pin extended GPIO to enhance your “real world” projects. GPIO is 100% compatible with the Model B+ and A+ boards. First 26 pins are identical to the Model A and Model B boards to provide full backward compatibility across all boards.
  • Connect a Raspberry Pi camera and touch screen display (each sold separately)
  • Stream and watch Hi-definition video output at 1080P
  • Micro SD slot for storing information and loading your operating systems.
  • Advanced power management:
  • You can now provide up to 1.2 AMP to the USB port – enabling you to connect more power hungry USB devices directly to the Raspberry PI. (This feature requires a 2Amp micro USB Power Supply)
  • 10/100 Ethernet Port to quickly connect the Raspberry Pi to the Internet
  • Combined 4-pole jack for connecting your stereo audio out and composite video out
  • raspberry
  • broadcom bcm2837
  • the
  • pi
  • 2
  • new
  • b
  • raspberry_pi_space
  • technical
  • 1gb
  • model
  • specifications
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • alnico
    alnico over 10 years ago in reply to Former Member +1
    I moved over 1000 miles from it, unfortunately. Fortunately, I have a buddy that is close and can buy and ship to me cheaper than the element 14 'personal' partner does.
  • shabaz
    shabaz over 10 years ago in reply to Former Member +1
    No full schematic is publicly available (it is not open source). But yes, you can directly connect 5V DC to the 40-way connector if you wish to.
Parents
  • dllahr
    dllahr over 10 years ago

    My brand new raspberry pi 2 has defective USB ports.  I have a brand new USB hub which is independently powered and connected to 2 USB hard drives. When I plug it into the pi and boot it up, the drives are not recognized - no entries in /dev, nothing in dmesg.  When I unplug it dmesg indicates they were recognized then recognizes they were disconnected.

     

    I bought another raspberry pi 2, same exact behavior.  I tried a different USB hub with different drives, same exact behavior.  It sees there is a systematic manufacturing defect in the USB ports.  For more details:

    raspberry pi model B USB ports - physical connection problems

     

    Distractions: Raspberry pi 2 and the case of the unreliable USB ports

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dllahr
    dllahr over 10 years ago

    My brand new raspberry pi 2 has defective USB ports.  I have a brand new USB hub which is independently powered and connected to 2 USB hard drives. When I plug it into the pi and boot it up, the drives are not recognized - no entries in /dev, nothing in dmesg.  When I unplug it dmesg indicates they were recognized then recognizes they were disconnected.

     

    I bought another raspberry pi 2, same exact behavior.  I tried a different USB hub with different drives, same exact behavior.  It sees there is a systematic manufacturing defect in the USB ports.  For more details:

    raspberry pi model B USB ports - physical connection problems

     

    Distractions: Raspberry pi 2 and the case of the unreliable USB ports

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • clem57
    clem57 over 10 years ago in reply to dllahr

    Oh! I came across this as a possible issue between USB 3.0 and 2.0 with Via chips :http://www.linuxquestions.org/questions/linux-hardware-18/via-labs-usb-3-0-hub-will-not-recognize-a-usb-3-0-device-873399/

    I believe your drives are 3.0 beacuse of the match of Pid from http://usb3speed.nirsoft.net/?pdesc=WD+Elements+10B8+USB+Device&vname=Western+Digital+Technologies%2C+Inc.&vid=4184&pid=4280

    The raspberry Pi are USB 2.0 only and maybe iffy with newer 3.0.

    Just saw,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dllahr
    dllahr over 10 years ago in reply to clem57

    The hubs and drives work fine with my raspberry pi 1, which is also USB 2.0, so I don't think that can be the issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to dllahr

    I read about this issue elsewhere (can't remember) and it has to do with USB hubs and also loss of data at high speeds. My son has a Rasp Pi 2 and I will need to connect a USB hub soon. Let me know if you find a solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dllahr
    dllahr over 10 years ago in reply to Former Member

    no solution in sight.  I contacted element14, even though their name is on the box, they said I had to contact the distributor, in my case since I bought it from Microcenter (Micro Center - Computers, Electronics, Computer Parts, Networking, Gaming, Software, and more!) they directed me to Microcenter's distributor "MCM Electronics".  I emailed them but they have not responded.  So needless to say I won't be using the raspberry pi from element14 (newark) and I certainly would recommend against anyone else using them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to dllahr

    Sorry dllahr you had such an unpleasant experience. The only things I noticed, was the Pi 2 is needs power source that is very good. I slipped a power hub from Rosewill (New Egg internal brand) onto new Pi 2 and it works like a charm handling keyboard, wireless mouse, wireless nano, and sdr-dtl USB connector with a 2.1 ampere wall plug (for the hub).

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dllahr
    dllahr over 10 years ago in reply to clem57

    Yep, I learned early on with my 1st generation raspberry pi the importance of the power supply.  Both USB hubs that I tried were independently powered, and the raspberry pi had a dedicated 1 A supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to dllahr

    The Pi 1 (before the A+/B+) and Pi 2 use a different USB controller. So clem57 's point is still potentially relevant. If you want to return it, element14jamie might be able to help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dllahr
    dllahr over 10 years ago in reply to cstanton

    Thank you Christopher, but I don't understand how it could be a software issue if the physical position of the USB connection solved the problem - twice.  And thank you for the offer of help returning, I was able to return it to Microcenter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to dllahr

    dllahr Glad you were able to return it, incidentally the USB controller is hardware, it is the chip which handles the USB ports and the Ethernet controller on the Raspberry Pi.