Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi 2 Model B 1GB Technical Specifications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 23 Jan 2015 4:01 PM Date Created
  • Last Updated Last Updated: 10 May 2021 7:09 PM
  • Views 32988 views
  • Likes 6 likes
  • Comments 62 comments
Related
Recommended

Raspberry Pi 2 Model B 1GB Technical Specifications

image

image

The Raspberry Pi 2 Model B 1GB
6X Faster

Learn More

 

Buy NowBuy Now

 

Benefits  image
Technical Specifications  image
Features  image

Benefits:

Get personal with your Pi. Welcome to the Raspberry Piimage 2, the single board computer that thinks it’s a home PC.

Enhanced Quad Core Processor and 1GB RAM now provides you with the opportunity to:

  • Build your own workstation – create and manage your documents and spreadsheets with ease using LibreOfficeimage
  • Faster and more enjoyable gaming – experience less lag and more seamless gaming in all your favourites. Can’t wait to demolish buildings in Minecraftimage, trigger your TNT now and be amazed by the results!
  • No more buffer face – boots up Raspbian in less than half the time as the Model B+
  • More power for your favourite projects – create Space Progammes, Time Lapse Videos, GPS tracking, HD audio and lots more with a full ecosystem of supporting accessories.
  • All your previous Raspberry Pi projects are 100% backward compatible with the new Raspberry Pi 2 Model B 1GB

Technical Specifications:

  • Broadcom BCM2837 Arm7 Quad Core Processor powered Single Board Computer running at 900MHz
  • 1GB RAM
  • 40pin extended GPIO
  • 4 x USB 2 ports
  • 4 pole Stereo output and Composite video port
  • Full size HDMI
  • CSI camera port for connecting the Raspberry Pi camera
  • DSI display port for connecting the Raspberry Pi touch screen display
  • Micro SD port for loading your operating system and storing data
  • Micro USB power source

Raspberry Pi 2 Model B Features:

  • Broadcom BCM2837Arm7 Quad Core Processor powered Single Board Computer running at 900MHz
  • 1GB RAM so you can now run bigger and more powerful applications
  • Identical board layout and footprint as the Model B+, so all cases and 3rd party add-on boards designed for the Model B+ will be fully compatible.
  • Fully HAT compatible
  • 40pin extended GPIO to enhance your “real world” projects. GPIO is 100% compatible with the Model B+ and A+ boards. First 26 pins are identical to the Model A and Model B boards to provide full backward compatibility across all boards.
  • Connect a Raspberry Pi camera and touch screen display (each sold separately)
  • Stream and watch Hi-definition video output at 1080P
  • Micro SD slot for storing information and loading your operating systems.
  • Advanced power management:
  • You can now provide up to 1.2 AMP to the USB port – enabling you to connect more power hungry USB devices directly to the Raspberry PI. (This feature requires a 2Amp micro USB Power Supply)
  • 10/100 Ethernet Port to quickly connect the Raspberry Pi to the Internet
  • Combined 4-pole jack for connecting your stereo audio out and composite video out
  • raspberry
  • broadcom bcm2837
  • the
  • pi
  • 2
  • new
  • b
  • raspberry_pi_space
  • technical
  • 1gb
  • model
  • specifications
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • alnico
    alnico over 10 years ago in reply to Former Member +1
    I moved over 1000 miles from it, unfortunately. Fortunately, I have a buddy that is close and can buy and ship to me cheaper than the element 14 'personal' partner does.
  • shabaz
    shabaz over 10 years ago in reply to Former Member +1
    No full schematic is publicly available (it is not open source). But yes, you can directly connect 5V DC to the 40-way connector if you wish to.
Parents
  • dllahr
    dllahr over 10 years ago

    My brand new raspberry pi 2 has defective USB ports.  I have a brand new USB hub which is independently powered and connected to 2 USB hard drives. When I plug it into the pi and boot it up, the drives are not recognized - no entries in /dev, nothing in dmesg.  When I unplug it dmesg indicates they were recognized then recognizes they were disconnected.

     

    I bought another raspberry pi 2, same exact behavior.  I tried a different USB hub with different drives, same exact behavior.  It sees there is a systematic manufacturing defect in the USB ports.  For more details:

    raspberry pi model B USB ports - physical connection problems

     

    Distractions: Raspberry pi 2 and the case of the unreliable USB ports

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to dllahr

    Oh! I came across this as a possible issue between USB 3.0 and 2.0 with Via chips :http://www.linuxquestions.org/questions/linux-hardware-18/via-labs-usb-3-0-hub-will-not-recognize-a-usb-3-0-device-873399/

    I believe your drives are 3.0 beacuse of the match of Pid from http://usb3speed.nirsoft.net/?pdesc=WD+Elements+10B8+USB+Device&vname=Western+Digital+Technologies%2C+Inc.&vid=4184&pid=4280

    The raspberry Pi are USB 2.0 only and maybe iffy with newer 3.0.

    Just saw,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dllahr
    dllahr over 10 years ago in reply to clem57

    The hubs and drives work fine with my raspberry pi 1, which is also USB 2.0, so I don't think that can be the issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to dllahr

    I read about this issue elsewhere (can't remember) and it has to do with USB hubs and also loss of data at high speeds. My son has a Rasp Pi 2 and I will need to connect a USB hub soon. Let me know if you find a solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 10 years ago in reply to dllahr

    I read about this issue elsewhere (can't remember) and it has to do with USB hubs and also loss of data at high speeds. My son has a Rasp Pi 2 and I will need to connect a USB hub soon. Let me know if you find a solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dllahr
    dllahr over 10 years ago in reply to Former Member

    no solution in sight.  I contacted element14, even though their name is on the box, they said I had to contact the distributor, in my case since I bought it from Microcenter (Micro Center - Computers, Electronics, Computer Parts, Networking, Gaming, Software, and more!) they directed me to Microcenter's distributor "MCM Electronics".  I emailed them but they have not responded.  So needless to say I won't be using the raspberry pi from element14 (newark) and I certainly would recommend against anyone else using them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to dllahr

    Sorry dllahr you had such an unpleasant experience. The only things I noticed, was the Pi 2 is needs power source that is very good. I slipped a power hub from Rosewill (New Egg internal brand) onto new Pi 2 and it works like a charm handling keyboard, wireless mouse, wireless nano, and sdr-dtl USB connector with a 2.1 ampere wall plug (for the hub).

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dllahr
    dllahr over 10 years ago in reply to clem57

    Yep, I learned early on with my 1st generation raspberry pi the importance of the power supply.  Both USB hubs that I tried were independently powered, and the raspberry pi had a dedicated 1 A supply.