Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116429 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • davidsmith71
    davidsmith71 over 5 years ago in reply to shabaz

    Yea mine is connected as shown in your link and I get nothing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to davidsmith71

    Hi David,

     

    There are some higher-res photos and perhaps some more written detail here: Raspberry Pi 7” Capacitive Touch Display: Assembly and Enclosure

    in the section "Assembling the LCD Panel Interface Board and Pi" there, that may help for comparison purposes just in case you spot anything different there compared to your setup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davidsmith71
    davidsmith71 over 5 years ago in reply to heavy714

    Having the same problem with mine.  Were you able to solve this or had to replace?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davidsmith71
    davidsmith71 over 5 years ago

    I just received my touch-screen display.  The display does not come on at all - regardless of how it is powered on based on the instructions above.

     

    How do I go about getting a replacement?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to dlblandjr

    Hi Donald,

     

    I don't think what you're requesting exists, unfortunately. There isn't any documentation explaining those things. The connector you're referring to is a USB connector, however, it won't do what a normal USB interface does.

    It is labelled 'Pwr Out' so it will supply a bit of power to other mystery unexplained devices : )

    A lot of the 'features' of that board are experimental (just a personal opinion) and could cause frustration more than anything else if used beyond the steps described in this blog post.

    It's best to assemble the unit as described in the steps here, and avoid using the extra connections.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dlblandjr
    dlblandjr over 5 years ago

    Hey folks,  where can i find a drawing or an id photo of  what the various components on the "adapter board are & do. ?

    Specifically  I see a female  plugin which to my deteriorated 80 year old eyes could be a USB or

    maybe one of the SATA style port that some  older computers used to  run a early HDMI  out  (say to a remote monitor)?

    So,     what the hell is it please ?

    many hearty thanks ,I appreciate your time

    Ol" Dony B.

    dlblandjr@gmail.com

    1-314-599-3886

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • smertje
    smertje over 5 years ago

    Hi there and thank you for that perfect HowTo!  After following your instructions, everything is running quite fine. I've got just one question concerning display rotation. Here is what I'd like to do...

     

    I have rotated the display to the right (portrait mode) using the screen configuration inside Raspbian. Now my screen is in the right position, but the touchscreen is acting weird, since it seems to remain in landscape mode. Is there a solution to fix that problem? Any help is welcome.

     

    Thanks, Roland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to hobantech

    Hi Michael,

     

    Soldering worked for me, some photos are here:

    Raspberry Pi 7” Capacitive Touch Display: Assembly and Enclosure

    I used epoxy glue for some strain relief on the connections afterward.

    It likely invalidates any warranty to solder and glue directly to the board, but that wasn't an issue as far as I was concerned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hobantech
    hobantech over 6 years ago

    I am trying to set up a 7" touchscreen and a digione Signature on the same raspberry pi 4 8 GB. The Allo Digione Signature connects to the 40 pin GPIO connector. The 7" Touchscreen needs to connect to the ground, 5V, (pin 6, and pin 2) of the GPIO. Since the GPIO connector on the top surface of the raspberry pi is occupied by the Digione Signature I am going to try to solder the touchscreen jumper cables to the underside of the raspberry pi. Is this a good idea, or am I trying to overload the raspberry pi? My thought are it should work since these are power and ground connectors.

    Thanks

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 6 years ago in reply to swfanman

    Not clear what the problem you're experiencing here is or where you're connecting the power. I believe if you're powering the display and the Pi, you plug the power into the display expansion board and not the Raspberry Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>