Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116430 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • cstanton
    cstanton over 6 years ago in reply to jack.chaney56

    Pi 4 does not do display over USB-C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 6 years ago in reply to swfanman

    Not the same, bu has anyone tried using the Asus USB portable monitor? With USB-C on Pi4 I m thinking it might make for a good portable solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to swfanman

    Hi Travis,

     

    Separate supplies is not a supported scenario, because then it is dependant on power sequencing, and might not function if (say) the display power is removed and then reapplied while the Pi is running. You might be able to get it to work under certain conditions or with certain commands, but you'd have to experiment.

    The Pi display isn't hot-swappable like a HDMI monitor, it should all be treated as one whole unit along with the Pi, with a single power source, once it is attached.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • swfanman
    swfanman over 6 years ago

    I just received one of these as a gift and love it, but I need help with a power issue. If I connect the power to the Raspberry Pi 3B+ GPIO then it works fine. However I want to use a separate power supply and that does not seem to be working. I have tried three different power supplies - a small iPhone adapter, a larger 2 amp adapter and the power supply I am currently using on my 3B+ which is a 2.5 amp supply. What exactly power supply do I need to power this display on its own or is there just an issue with the port and maybe I need to return it? Any assistance would be appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • iuriaranda
    iuriaranda over 6 years ago

    I'd like to power the Pi and the screen independently, so I haven't connected the GPIO ports with the jumpers. The setup works correctly, but the problem comes when the screen is powered off and powered back on. In such case the Pi keeps running, but not the screen. The problem is that when the screen is powered on again, it doesn't turn on. I guess the Pi initialises the screen board when it boots. Is there a way to initialise the screen without the need to reboot the Pi?

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 6 years ago in reply to tonygibbs9525

    tonygibbs9525 depends on the version of the software on your raspberry pi, some guides claim it isn't necessary because it's possible for this information to transfer over the ribbon cable, however some people do find it is necessary. Your mileage may vary.

     

    There doesn't appear to be any official way to calibrate the display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tonygibbs9525
    tonygibbs9525 over 6 years ago

    Hi... the PiDisplay info does not mention connecting SDA & SCL (yellow & green).. is this not necessary...

     

    also...  how do I calibrate the touch (cursor) position on the screen ?

     

    Tony

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • responsible
    responsible over 6 years ago

    It is generally expensive. Where can I find it cheaper from?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gstory20
    gstory20 over 7 years ago

    Just got mine as a gift.  (Looks like it is pre-owned because the adaptor board is already attached to the display (both physically via the stand-offs and electrically (via the ribbon cables). 

     

    I have two questions:

     

    1.  What if anything are the yellow and green wires for?  They're not mentioned in the installation instructions.

    2.  I'm not sure I understand how to correctly insert the ribbon cable into the adaptor board. 

     

    Thanks.

    Glenn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jorytsai

    Hi Jory,

     

    If you mean the white cable that connects to the Pi, then it is a 15-way, 1mm pitch 'flat flex' cable, not ribbon cable, with connections on opposite sides, and you can search for that on distributor websites for the length you want. Farnell and Newark do not have it at 12" length, but Adafruit does: https://www.adafruit.com/product/3671

    It may work fine, no guarantee of that though in all conditions (it will only have been tested at the shorter supplied length) so you will have to test yourself. Adafruit website suggests it may work fine unofficially but they won't guarantee it either.

    The known reliable working solution is to use it as designed (i.e. with the short length cable). Any time you try to exceed the boundaries, you'll need to test to a level that you're satisfied with, in the environment that you intend to use it in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>