Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116435 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • jorytsai
    jorytsai over 7 years ago

    What is the max length ribbon cable? Can we use 12” ribbon cable? If yes, where to get it?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 7 years ago

    I used the product in a project to build a working HO scale model railroad Drive-In movie theatre using a Raspberry Pi. The Walthers Cornerstone Skyview Drive-In Theater kit will accommodate the Pi 7 inch screen. A little plastic cutting is needed to fit the Pi but other than that it is a great fit. I created some scripts and made a few Pi operating system changes to create the classic dancing hot-dog commercial that is motion activities. Show starts in 3 minutes!

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • leelabks
    leelabks over 7 years ago in reply to shabaz

    Hi Shabaz,

     

    Thanks for the clearer photo from the website that you mentioned and the flex cable from the RPI board to the display adapter board connect wrongly, after fixing it, the display is working now!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to leelabks

    Hi k c,

    There is detail here worth double-checking with: Raspberry Pi 7” Capacitive Touch Display: Assembly and Enclosure

    in particular the photos showing the connector detail and the text from the section "Assembling the LCD Panel Interface Board and Pi" onward. It is very easy to connect things with an error, so it is worth examining the flat flex orientation, and power connection details there.

    Have you confirmed that the Pi works _without_ the display, i.e. standalone, first? It is only worth connecting the display once you have confirmed the Pi works standalone, to isolate the issue.

    There could also be power supply issues. Are you using the official 5.1V 2.5A supply? Or are you using a 5V supply? A non-official supply might not work, because a mobile phone charger is different to the Pi's power supply. A thicker or different USB cable might work, but it's not guaranteed.

    Regarding the LCD backlight question, it is unlikely that it is causing the issue, it is more likely a red herring. Anyway, it is controlled in software, there is a driver for it. It is a huge assumption that lack of display is being caused by this though - way more likely to be caused by (a) connection issue, or (b) power supply issue, or (c) bad SD card image - the point (c) can be confirmed or ruled out, by running the Pi without the display first.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • leelabks
    leelabks over 7 years ago

    I use the Raspberry Pi 7” Touchscreen Display, https://www.element14.com/community/docs/DOC-78156/l/raspberry-pi-7-touchscreen-display#installI, to connect to the Raspberry Pi 2 Model B. The hardware connection I followed the website, https://www.element14.com/community/docs/DOC-78156/l/raspberry-pi-7-touchscreen-display#installI. The image that I use is “Raspbian Stretch with desktop”  version November 2018. After the hardware connection and the SD card inserted in, there is no display seen, may I know any suggestion to troubleshoot the problem?

     

    I found an unofficial reversed engineered adapter board schematic, https://imgur.com/a/24TFn. According to the schematic, the LCD backlight driver U1 pin-4 (SHDN) is 0V, anyone has any idea what is controlling this LCD backlight shutdown pin function? Where can i get the official display pin arrangement and the adapter board schematic to help my troubleshooting?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to soundadb

    There is a comment here about the screen size.

    https://raspberrypi.stackexchange.com/questions/72735/openplotter-pi3-800x480-screen-cut-off

    They also show the settings, which may have changed (or need to change) when runnign openplotter.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • soundadb
    soundadb over 8 years ago

    Hello,

     

    I am new here .

    Did read all the comments in this section . And found not a solution.

    Bought a Rasberry Pi 3 B+ together with the 7" touchscreen about 2 weeks ago.

    Started with a NOOBS Rasbian stretch and with a Hdmi screen all is working fine,

    did the updates and installed Openplotter. Wich works great.

    Now, with the 7" Pi screen its not working at all. At startup it reacts and gives all kind

    of stripes and colours to a screen that ends up like the attached picture.

    Did reassemble all the flatcables as suggested in this topic. When the Pi goes to sleep

    the screen turns black , when I touch the screen it wakes up. So no problems with touch.

    Symptoms are the same using a NOOBS Rasbian stretch SD or a NOOBS openplotter SD.

     

    Any suggesions?

     

    Best regards, Andreimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to doobiedoo

    Hi,

     

    The syntax

    lcd_rotate=2

    is needed in a file and then reboot issued, see here for detail:

    https://www.raspberrypi.org/forums/viewtopic.php?t=121263 

     

    Bear in mind, the contrast won't look as great if you do this. Better to physically rotate if you can, but sometimes that is not possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • doobiedoo
    doobiedoo over 8 years ago

    my problem: I assembled the 7 in screen, its board, and the case. Boots up great, but the on the display is upside down. Is there a way to flip the image without mounting the display board turned 180 degrees?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ve3ell
    ve3ell over 8 years ago

    I assembled as instructions indicate but it does not work at all. Power supply is good.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>