RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs EA LPC11U37H LPCXpresso Board with ULINKPLUS
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: snidhi
  • Date Created: 30 Jun 2018 1:57 PM Date Created
  • Views 1137 views
  • Likes 8 likes
  • Comments 0 comments
Related
Recommended
  • keil_ulink
  • roadtest; roadtest
  • keil
  • arm keil mdk
  • ulinkplus
  • lpc11u37h

EA LPC11U37H LPCXpresso Board with ULINKPLUS

snidhi
snidhi
30 Jun 2018

EA LPC11U37H Board with ulinkplus debugger in KEIL uVision

 

The (EA) Embedded Artists OM13074 LPCXpresso LPC11U37 board has been used for tests here. As one can see this board also has another version OM13062 which is sold by NXP and not EA.

 

image

In the EA LPC11U37H LPCXpresso Board Schematics I checked that the board is supported by 10-pin, 0.05" SWD connector. The pinout for the SWD connector can be seen in the first page of the blog.

This board is powered by USB and ARM ulink plus is used to program the LPC11U37H via SWD.

 

 

{gallery} LPC11U37H LPCXpresso Board

image

Fig1: Powering up the LPC11U37H LPCXpresso Board

image

Fig 2:

image

Fig 3: The Working Setup

image
image
image
image
image
image

 

As mentioned in my first blog page, not all micro-controllers are supported by KEIL MDK uVision 5. The LPC11U37xx micro-controller family needs the KEIL MDK uVision 4 Legacy Support tool.

  • Install the KEIL MDK uVision 4 Legacy Support from KEIL website.
  • Download the LPCXpresso LPC11U37 board support files from NXP.
  • This board is also supported for the LPCOpen Software Development Platform.

 

ULINKplus Debugger Settings in KEIL MDK4 Legacy Support

 

Setup the KEIL MDK4 environment to be interfaced with the ARM ulinkplus debugger.

Fig 1: Setup the ulinkplus debugger and the target Driverimage

 

Fig 2: Setup the ulinkplus debugger in Utilitiesimage

 

image

Fig 3: Setup the Target Driver for Flash Download

 

A maximum of only 4 debug breakpoints are allowed with ulinkplus debugger as mentioned in the data-sheet. I tried to set 6 breakpoints and during runtime 2 breakpoints were automatically disabled as I would have expected it.

 

image

 

image

 

The asm and linker must be set in the KEIL MDK4 to point to the complied libraries as shown below.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Blinky Test on the LPCLPC11U37H using ARM ulinkplus

 

After the debugger settings are done. Now we are ready to flash the blinky code on the LPC11U37H LPCXpresso Board.

 

The successful test of Blinky

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

This Road-test is further divided into the following blogs

 

EA LPC11U37H LPCXpresso Board with ULINKPLUS

Power and Events Measurements with ULINKplus

Difficulties in interfacing ulinkplus with Keil MDK