RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Keysight InfiniiVision MSOX3034T RoadTest | Function Generator & Other Misc. Functionality
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: Attila Tőkés
  • Date Created: 8 Oct 2020 4:26 PM Date Created
  • Views 892 views
  • Likes 2 likes
  • Comments 1 comment
Related
Recommended

Keysight InfiniiVision MSOX3034T RoadTest | Function Generator & Other Misc. Functionality

Attila Tőkés
Attila Tőkés
8 Oct 2020

Previous blog posts of my MSOX3034T Road Test:

Keysight InfiniiVision MSOX3034T RoadTest | Unboxing & First Impressions

Keysight InfiniiVision MSOX3034T RoadTest | Analog Specs & Basic Functionality

Keysight InfiniiVision MSOX3034T RoadTest | Low Speed Analog Experiments

Keysight InfiniiVision MSOX3034T RoadTest | Digital Channels & Serial Decoding

Keysight InfiniiVision MSOX3034T RoadTest | Bandwidth & Update Rate Measurements

Keysight InfiniiVision MSOX3034T RoadTest | High Speed & RF Experiments

 

  • 1. Arbitrary Waveform Generator
  • 2. Voltmeter and Frequency Counter
  • 3. VGA and Web Interfaces+

 

Hi Everyone,

 

This is the last blog post before my final review on the Keysight InfiniiVision MSOX3034TMSOX3034T mixed signal oscilloscope.

 

In the previous blog posts, I covered the Analog and Digital Signal Capturing functionality of the scope.

 

What is left is the Function / Arbitrary Waveform Generator, the Digital Voltmeter, the Frequency Counter and some other Miscellaneous Functionality of the instrument.

 

So, let's see what we got!

1. Arbitrary Waveform Generator

 

The scope comes with Function / Waveform Generator that is capable to generate signals with frequency up to 20 MHz. The voltage of the generated can be adjusted from 0 to +/- 2.5V,

 

The output signal is available the front panel BNC connector marked "Gen Out". The output impedance can be either 50 Ohm or High Z.

 

We get a set of standard waveform built-in:

 

Sine

(up to 20MHz)

imageimage

Square
(up to 10 MHz)

imageimageimage

Ramp:

(up to 200kHz)

imageimageimage

Pulse:

(up to 10MHz)

imageimage

DC:

image

 

Noise:

imageimage

 

Sine cardinal:

(up to 1MHz)

imageimage

 

Exponential Rise:

(up to 5MHz)

imageimage

 

Exponential Fall:

(up to 5MHz)

imageimage

 

Cardiac:

(up to 200kHz)

imageimage

 

Gaussian Pulse:

image

 

And as well an interface to define Arbitrary Waveform-s:

imageimageimage

The waveform can either input manually, or by capturing it from one of the analog channels.

image

 

 

2. Voltmeter and Frequency Counter

 

The scope comes with a built-in Digital Voltmeter (DVM) and Frequency Counter.

 

The Digital Voltmeter can be used to do an AC RMS, DC or DC RMS measurement with 3 digits resolution.

 

The source can be any of the input signals. The RMS measurements are accurate between 20kHz and 100KHz

image

(source MSOX3034TMSOX3034T User's Guide)

 

The Frequency Counter can be used to measure the frequency of the input signals, with a max resolution of 8 digits.

image

 

3. VGA and Web Interfaces+

 

The scope came with a LAN + VGA module, that offers the possibility of remote access and connecting the scope to an external monitor.

image

Unfortunately, the external monitor connection is the kind of outdated VGA, so you may need an older monitoring to be able to use it. The resolution is 800 x 600px, which is the native resolution of the scope's screen

image

 

If we connect the scope to our network, a web based remote control interface becomes available:

image

The interface allows controlling the scope. If we install an application to the scope, we also get a remote VNC view:

 

image

 

The scope also support Keysight's BenchVue software, but did not tried this yet.

 

In terms of export functionality, the scope offers Data and Screen Captures saved on an USB stick. I used these to export screen captures for this and my previous blog posts.

 

The next update will be my final Road Test Review of the MSOX3034TMSOX3034T. This will include a summary of what we did till now, comparison with other scopes, and some conclusions.

 

Hope you enjoyed this blog post! image

  • Sign in to reply
  • DAB
    DAB over 5 years ago

    Good post.

     

    DAB