RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Review Blogs Ras Pi CM5 roadtest - 01 - unboxing
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: saramic
  • Date Created: 22 Aug 2026 5:48 AM Date Created
  • Views 290 views
  • Likes 8 likes
  • Comments 7 comments
Related
Recommended
  • vnc
  • Raspberry Pi CM5
  • headless
  • unboxing

Ras Pi CM5 roadtest - 01 - unboxing

saramic
saramic
22 Aug 2026

To keep myself accountable, I thought it best to blog my progress with the Raspberry Pi Compute Module 5 Development Kit before doing a full RoadTest review. My roadtest plan was to build a remote-control dog feeder that, with a bit of Machine Learning, could make the dogs sit and wait for their food. But to get started, it was a question of unboxing and getting some DX (Developer Experience) up and running.

What’s in the box

image

The kit is a CM5 Wireless (4GB RAM / 32GB eMMC), the CM5 IO Board pre-fitted inside the IO Case, the official cooler, an antenna kit, a 27W USB-C PD power supply, two HDMI-to-HDMI cables, and a USB-A to USB-C cable.

image

Packaging and build quality are genuinely nice — everything sits in its own tray, cables included, a pleasure to actually unpack. A few things were missing that would’ve smoothed the first hour out, though:

  • No Quick start guide something short and succinct to get you up and running without having to read all the docs and second guess if you understood them correctly
  • No spare jumper for the boot-mode header. Forcing USB boot mode needs a small 2-pin shorting jumper on J2, and the kit doesn’t include a spare one. Had to raid an old parts bin for it — worth having a couple of 2.54mm jumpers on hand before you start.
  • No CR2032 RTC battery. Probably OK and I had one lying around anyway.

Working out how it goes together

The kit ships with a stack of datasheets rather than one guide, and it wasn’t immediately obvious which document actually covers the physical assembly — seating the CM5 onto the IO Board and closing up the IO Case. Once I found the right pictures there really was only one way it could go together, which helped, but a single quick-start card in the box pointing at “open here for assembly” would have saved some flipping between PDFs.

Actually getting the board seated and screwed into the case was fiddlier than expected in practice: four screws, four spacers, and making sure the cooler and its fan cable landed correctly along the way, all in a fairly tight fit. Nothing went wrong, it just took more care than I expected for what’s ultimately a four-screw job.

image

First boot: no surprises, no OS either

Before touching anything else, I hooked it up to a monitor just to see what happened. No surprise, really — the bootloader was upfront that there was no bootable image on the eMMC, and dropped straight to looking for a network boot server instead. Presumably that’s a real option if you’ve got a PXE-style network-boot server sitting on the LAN already, but that’s not something I have set up, so: on to imaging the eMMC directly instead.

image

Flashing the eMMC

The process is: fit the boot-mode jumper, connect USB-C from the board’s slave port to a computer, then use that computer to write an OS onto the eMMC over USB rather than booting from it.

image

Raspberry Pi Imager was the obvious first tool, but on its own it couldn’t find the board at all — no drive showed up anywhere for it to target. Downloading the separate rpiboot utility and running that directly fixed it immediately: it found the board straight away and confirmed the eMMC as 32GB. From there, Imager’s normal prompts took over — creating a user account, enabling SSH, and setting a hostname. In keeping with the household convention (Pollyanna and Athena are already on the network), this one’s called Quintessa.

brew install rpiboot
sudo rpiboot -d "$(brew --prefix rpiboot)"/share/rpiboot/mass-storage-gadget64

  ...
  Sending bootcode.bin
  Successful read 4 bytes
  Waiting for BCM2835/6/7/2711/2712...
  Second stage boot server
  File read: mcb.bin
  File read: memsys00.bin
  File read: memsys01.bin
  File read: memsys02.bin
  File read: memsys03.bin
  File read: bootmain
  ...
  Second stage boot server done

image

CPU heat and fan test

With SSH up, first real test was seeing how the CM5’s four Cortex-A76 cores (the same BCM2712 silicon as Pi 5) handle sustained load, and whether the official cooler’s fan ever needs to kick in.

Baseline, idle:

vcgencmd measure_temp
vcgencmd get_throttled
vcgencmd measure_clock arm

temp=32.3'C
throttled=0x0
frequency(0)=1900016256

A normalised CPU speed number, for comparison against other boards:

sudo apt-get update
sudo apt-get install -y stress-ng sysbench

sysbench cpu --cpu-max-prime=20000 --threads=4 run

General statistics:
    total time:                          10.0009s
    total number of events:              40567

Latency (ms):
         min:                                    0.98
         avg:                                    0.99
         max:                                    1.51
         95th percentile:                        0.99
         sum:                                39995.46

Threads fairness:
    events (avg/stddev):           10141.7500/14.43
    execution time (avg/stddev):   9.9989/0.00

~4,057 events/sec across 4 threads.

Then a 60-second all-core stress test, sampling temperature and clock speed every 5 seconds:

stress-ng --cpu 4 --timeout 60s --metrics-brief > /tmp/stress_result.txt 2>&1 &
STRESS_PID=$!

for i in $(seq 1 12); do
  sleep 5
  t=$(vcgencmd measure_temp)
  c=$(vcgencmd measure_clock arm | cut -d= -f2)
  echo "t=+$((i*5))s  $t  clock=${c}Hz"
done

wait $STRESS_PID

vcgencmd measure_temp
vcgencmd get_throttled
cat /tmp/stress_result.txt

t=+5s  temp=38.9'C  clock=2400033792Hz
t=+10s  temp=41.7'C  clock=2400023808Hz
t=+15s  temp=41.7'C  clock=2400027136Hz
t=+20s  temp=42.2'C  clock=2400020480Hz
t=+25s  temp=43.9'C  clock=2400020480Hz
t=+30s  temp=42.8'C  clock=2400030464Hz
t=+35s  temp=43.3'C  clock=2400030464Hz
t=+40s  temp=44.4'C  clock=2400033792Hz
t=+45s  temp=45.0'C  clock=2400030464Hz
t=+50s  temp=45.5'C  clock=2400030464Hz
t=+55s  temp=45.0'C  clock=2400037120Hz
t=+60s  temp=41.7'C  clock=2400027136Hz

=== after ===
temp=43.9'C
throttled=0x0

=== stress-ng result ===
stress-ng: metrc: [2259] stressor       bogo ops real time  usr time  sys time   bogo ops/s     bogo ops/s
stress-ng: metrc: [2259]                           (secs)    (secs)    (secs)   (real time) (usr+sys time)
stress-ng: metrc: [2259] cpu               54542     60.02    239.83      0.02       908.78         227.41

All four cores boosted to 2.4GHz immediately and held it for the whole run, temperature climbed from 35.6°C to a peak of 45.5°C, and throttled stayed 0x0 the entire time — no throttling at all.

Checked whether the fan actually spun up for any of this, via the board’s PWM fan sensor:

cat /sys/class/hwmon/hwmon2/name
cat /sys/class/hwmon/hwmon2/fan1_input

pwmfan
0

0 RPM for that first run — 45°C never got close to the fan’s trip point, so the passive cooler alone handled a single 60-second burst with headroom to spare.

Ran it a few more times back-to-back right after, though, and the heat had nowhere to go between runs — by a later pass, t=+60s was reading 52.7°C, clock still pinned at 2.4GHz, and this time the fan was actually on:

cat /sys/class/hwmon/hwmon2/fan1_input

1481

1,481 RPM. So the trip point sits somewhere between 45.5°C and 52.7°C — one clean 60-second run isn’t enough to reach it, but a couple of them back-to-back is. Good to see the fan does work.

The VNC rabbit hole

Raspberry Pi OS here ships both realvnc-vnc-server and wayvnc (the desktop runs on labwc, a Wayland compositor, not X11) — raspi-config picks the right one automatically, so turning it on is one command:

sudo raspi-config nonint do_vnc 0
sudo reboot

(Interactive equivalent: sudo raspi-config → Interface Options → VNC → Yes.)

First attempt at connecting, with macOS’s built-in Screen Sharing, just silently failed:

open vnc://quintessa.local

Turned out this was never going to work. A raw RFB handshake against port 5900 shows why:

python3 -c "
import socket
s = socket.create_connection(('quintessa.local', 5900), timeout=4)
banner = s.recv(64)
s.sendall(banner)
n = s.recv(1)[0]
print('security types offered:', list(s.recv(n)))
"

security types offered: [19, 129, 5]

19 is VeNCrypt — wayvnc needs a client that actually speaks it. macOS Screen Sharing only understands classic VNC password auth and Apple’s own ARD scheme, neither of which is in that list, so it just hangs with no useful error.

Next tried RealVNC Connect:

brew install --cask realvnc-connect

This immediately prompted for a sign-in/trial — turns out that’s just it pushing its own cloud-relay service. You can skip that entirely and type an address straight into its search bar for a direct LAN connection, no account needed — but in the end went with a plainer option instead and removed it:

brew uninstall --cask --zap realvnc-connect
brew install --cask tigervnc-viewer

TigerVNC connected fine — it speaks VeNCrypt natively. But the redraw was painfully slow. Chased that down and found three compounding causes, none of them TigerVNC’s fault:

  1. Two separate wayvnc processes were running at once. Alongside the one raspi-config enabled, Raspberry Pi Connect — Raspberry Pi’s own cloud remote-access tool — was already active and signed in from first-boot setup, running its own wayvnc instance (rpi-connect-wayvnc.service), both capturing the same compositor output at once:

    systemctl status wayvnc.service
    systemctl --user status rpi-connect-wayvnc.service
    rpi-connect status

    Signed in: yes
    Subscribed to events: yes
    Screen sharing: allowed (0 sessions active)
    Remote shell: allowed (0 sessions active)


  2. A real monitor was attached, so it wasn’t compositing some small headless framebuffer — it was encoding a full 1920×1080 desktop every frame:
    wlr-randr

    HDMI-A-1 "Dell Inc. DELL U2312HM FX01R27KCU1L (HDMI-A-1)"
      Modes:
        1920x1080 px, 60.000000 Hz (preferred, current)

  3. It’s on Wi-Fi, not Ethernet, and already showing real retry traffic:
    cat /proc/net/wireless

    wlan0: 0000   49.  -61.  -256        0      0      0    881      0        0

    (that’s 881 retries — the link level column reading -61dBm.)

In the end I decided I will be happy enough with SSH and to turn VNC off.

rpi-connect off
sudo systemctl disable --now wayvnc.service

Going console-only

None of that is really TigerVNC’s problem to fix — for a board that’s meant to run headless as a camera/AI appliance, not something anyone sits in front of, running a full desktop plus two competing VNC captures 24/7 is just overhead for a GUI that’s rarely needed. Switched the boot target to console-only instead of chasing VNC settings further:

sudo raspi-config nonint do_boot_behaviour B1
sudo reboot

Confirmed after reboot:

systemctl get-default

multi-user.target

  Desktop, VNC off Console-only, VNC off
free -h used 449Mi 286Mi
top used 431.8Mi 270.6Mi

labwc, pcmanfm (desktop icons), wf-panel, and the two xdg-desktop-portal processes are the difference — all present at 449Mi, all absent at 286Mi. ~163Mi, consistently, across both measurement tools — that’s the actual cost of the desktop GUI on this board, isolated from the VNC question entirely.

Switching back to desktop, if ever needed

sudo raspi-config nonint do_boot_behaviour B4   # desktop, autologin
sudo reboot

(B3 for desktop with a login prompt instead of autologin, B2 for console with autologin — B1 is what we’re running now.)

Up Next

  • I might do a few more tests to confirm all IO board ports work: USB 3.0, Gigabit Ethernet, maybe GPIO headers.
  • Wi-Fi association check, dual-band, note RSSI and link rate
  • Connect some cammeras and check them for steaming
  • A CPU-only YOLOv8s inference baseline over a real camera feed
  • I have also started to train the dogs to respond to the speakers via a sound board, inspired by hambreros and tamadillo's  Hall-w-EV robot voice
    image

  • and much more …

Source

https://github.com/saramic/paws-and-wait

  • Sign in to reply
  • saramic
    saramic 1 month ago in reply to saramic

    yeah my line

    rpi-connect off

    means irrelevant of VNC will turn off the Ras Pi Connect - will update once I get another blog post up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saramic
    saramic 1 month ago in reply to trkn

    reading up on Ras Pi Connect - it seems that will give you remote shell and desktop access https://connect.raspberrypi.com/ I will try that in an upcoming blog post I hope

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • OwainM
    OwainM 1 month ago

    Hey,

    I'm glad your kit arrived all in one piece. Thanks for posting your unboxing experience for the kit and the quirks of getting set up!

    I'm looking forward to what you test out with the kit and reading your review.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • trkn
    trkn 1 month ago

    Thanks for documenting the VNC troubleshooting! Looking forward to part 2 and seeing the dog feeder in action.

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago

    Love to see the NGFF m.2 connector accessible. Seems to be a M key for mass storage. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>