RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Comments for using RPi with SPI memory
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 2 answers
  • Subscribers 2748 subscribers
  • Views 4867 views
  • Users 0 members are here
  • ram
  • raspberry
  • microchip
  • pi
  • spi
  • sram
Related

Comments for using RPi with SPI memory

clem57
clem57 over 11 years ago

image

Here are my notes so far. Any comments or issues please let me know. I think I am on the right track.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Ok!

     

    I have learned that I should use pins 24/26 as CE0/CE1 instead of pin15(GPIO 22) because this alleviates me writing extra code. I plan on using Python SPIDEV from GitHub...

     

    Thanks for Elektor Academy - Hardware Hacking the RPi pointing this out. Excellent if you want the details image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Question: What to do with HOLD pin? I need it to stayhHigh. Also how to make the CS pin be high but go low when transmitting?

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 11 years ago in reply to clem57

    Hi Clem,

     

    Use a pull-up resistor (10K should be just fine) with the HOLD pin.

    The CS handling is done by the driver.

    I found an example here involving MCP3008. This chip uses an active low chip select as well as the 23K256. Good luck!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bbolo1
    0 bbolo1 over 11 years ago in reply to clem57

    Hi Clem,

     

    Use a pull-up resistor (10K should be just fine) with the HOLD pin.

    The CS handling is done by the driver.

    I found an example here involving MCP3008. This chip uses an active low chip select as well as the 23K256. Good luck!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Sure I will sum this up experiences and all. Thanks @Michael Kellett for kind words of encouragement image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    I'm glad it's working - how fast are you running the spi clock and how long are the wires ?

     

    Any chance of a picture ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Well guess what...

    I decided to pull everything and remount changing colored wires and new positions and the thing is working! image So cannot tell what is wrong!?! I have a few bit flips, but that may be timing or something. But progress is being made. Thanks for the help. Next is a code rewrite/cleanup because so much extra stuff

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    Well post the code here and I'll see if I can pick my way though it.

     

    If you are bit banging the SPI you can add logging features to the code to trace each pin state as it runs.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to bbolo1

    HI @bbolo1

         No scope (Yet), but have voltmeter and was thinking to use over SO/MISO and ground. It is also a current meter as well. Will do some I2C next after this works.

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    You've now reached the stage where I would connect the 4 channel scope or a logic analyser !

     

    Do you have either ?

     

    If not you can try posting your code and we'll see if we can pick our way through it.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to bbolo1

    Well I am stuck again, but this time I think software. I can program using python, but nothing gets stored(?) and the chip does not respond (0XFF) ! If I unplug the chip's +3 volts, all responses are 0X00... I am too close to this to figure it out. Ask me questions to send me on the right track.

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 11 years ago in reply to clem57

    Hi Clem,

    Congrats!!! It is good to hear everything works fine with the SPI memory. Good luck with the tests! image

    After you play with SPI maybe you can try some I2C chips as well. There are so many interesting I2C chips (pressure, temp, acceleration sensors, gyros, magnetometers, ...) you can attach to the RPi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to bbolo1

    With the pullup resistor on HOLD, I can boot RPi with power to SPI memory. Thanks @bbolo1 ! image image image

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 11 years ago in reply to clem57

    Yes, you are correct about the HOLD pull-up resistor.

    As for the CS state, I have to check it on my board as well. Can you try to disconnect the SO pin of the 23K256? Of course, this means the SPI communication with this chip won't work but it is worth checking if this is the cause of the strange errors you're seeing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer