RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Comments for using RPi with SPI memory
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 2 answers
  • Subscribers 2748 subscribers
  • Views 4867 views
  • Users 0 members are here
  • ram
  • raspberry
  • microchip
  • pi
  • spi
  • sram
Related

Comments for using RPi with SPI memory

clem57
clem57 over 11 years ago

image

Here are my notes so far. Any comments or issues please let me know. I think I am on the right track.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Ok!

     

    I have learned that I should use pins 24/26 as CE0/CE1 instead of pin15(GPIO 22) because this alleviates me writing extra code. I plan on using Python SPIDEV from GitHub...

     

    Thanks for Elektor Academy - Hardware Hacking the RPi pointing this out. Excellent if you want the details image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Question: What to do with HOLD pin? I need it to stayhHigh. Also how to make the CS pin be high but go low when transmitting?

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 11 years ago in reply to clem57

    Hi Clem,

     

    Use a pull-up resistor (10K should be just fine) with the HOLD pin.

    The CS handling is done by the driver.

    I found an example here involving MCP3008. This chip uses an active low chip select as well as the 23K256. Good luck!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Sure I will sum this up experiences and all. Thanks @Michael Kellett for kind words of encouragement image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    I'm glad it's working - how fast are you running the spi clock and how long are the wires ?

     

    Any chance of a picture ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Well guess what...

    I decided to pull everything and remount changing colored wires and new positions and the thing is working! image So cannot tell what is wrong!?! I have a few bit flips, but that may be timing or something. But progress is being made. Thanks for the help. Next is a code rewrite/cleanup because so much extra stuff

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    Well post the code here and I'll see if I can pick my way though it.

     

    If you are bit banging the SPI you can add logging features to the code to trace each pin state as it runs.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to bbolo1

    HI @bbolo1

         No scope (Yet), but have voltmeter and was thinking to use over SO/MISO and ground. It is also a current meter as well. Will do some I2C next after this works.

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to bbolo1

    HI @bbolo1

         No scope (Yet), but have voltmeter and was thinking to use over SO/MISO and ground. It is also a current meter as well. Will do some I2C next after this works.

     

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Sure I will sum this up experiences and all. Thanks @Michael Kellett for kind words of encouragement image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    I'm glad it's working - how fast are you running the spi clock and how long are the wires ?

     

    Any chance of a picture ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to michaelkellett

    Well guess what...

    I decided to pull everything and remount changing colored wires and new positions and the thing is working! image So cannot tell what is wrong!?! I have a few bit flips, but that may be timing or something. But progress is being made. Thanks for the help. Next is a code rewrite/cleanup because so much extra stuff

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to clem57

    Well post the code here and I'll see if I can pick my way though it.

     

    If you are bit banging the SPI you can add logging features to the code to trace each pin state as it runs.

     

    MK