RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Discussion: How Would You Roadtest the MagAlpha Angle Sensor Kit
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 2562 subscribers
  • Views 5329 views
  • Users 0 members are here
  • MPS MA732 MagAlpha Angle Sensor Kit with Servo Motor
Related

Discussion: How Would You Roadtest the MagAlpha Angle Sensor Kit

rscasny
rscasny over 3 years ago

imageI usually provide the technical details and documentation on a roadtest page for people to look over at their leisure.

This material usually gives people ideas on how they would like to roadtest a product. But I think sometimes, it's good to actually talk about how one would roadtest a product, due to perhaps it's something new for many people, or it needs a little more background.

I think this angle sensor kit is one of those products.

When we decided to roadtest this kit, we initially provide the sensor and the communications board. But with only those things, the roadtester would have to mount the magnet and the sensor to the motor shaft. Seemed like heavy lifting, so the supplier came back with the kit that's on this page (right):

community.element14.com/.../mps_magnetic_angle_p

The sensor board is mounted to the end of the motor shaft already (as well as the magnet). The roadtester would need to hook it all up, connecto the Arduino board (not shown in the image at the right) and spin the motor.

But still, how do you actually test it.

More importantly, why is this sensor important to roadtest?

This clip from the sponsor's website pretty much explains it:

The ability to detect position or speed is a fundamental requirement in the control and monitoring of many mechanical systems. Slow speed position measurement in applications such as motorized actuators has historically used resistive potentiometers. In high-speed applications such as servo motors, optical encoders have typically been used. Though potentiometers are inexpensive, they suffer from the drawback of being a moving contact-based assembly, which brings the associated issues of mechanical contact wear and susceptibility to damage from external environmental factors including moisture and dirt ingress. Optical encoders offer high accuracy, but come at a higher price due to the complex nature of their construction. Engineers can solve this dilemma by using contactless rotary magnetic angle sensors that implement Hall-effect sensing.

This page goes into detail about the angle sensor, specifically about its SpinAxis technique: www.monolithicpower.com/.../introduction-to-the-magalpha-magnetic-angle-sensor-family

The kit we are providing to the roadtester is a motor control kit. But we would like to get roadtesters to take a closer look at the angle sensor. Run some tests, play with it, and give some feedback or thoughts about it.

So, that's my backgrounder.

What do you think?

How would you test the sensor?

Even if you don't have the time to take on this roadtest, I'd appreciate your input. It would benefit those members who are thinking about applying.

Thanks.

Randall Scasny
RoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +6
    Hi Randall, That sensor has incredibly high granularity for position sensing, and works to a very good speed (60,000 RPM) and so the uses for it could span across a lot of things that traditionally would…
  • shabaz
    shabaz over 3 years ago +4
    Having read a bit more on it, the sensor is very interesting and designed for new and existing applications. The sensor can be read digitally (SPI interface), or it offers a normal rotary encoder output…
  • robogary
    robogary over 3 years ago in reply to ajmorin369 +4
    Hi A.J. - I can't speak officially for the Road Test selection committee, and I dont know what and how many Road tests you've applied for, but I can share my experience. When I first got going with Road…
  • andyclarke67
    andyclarke67 over 3 years ago

    Seems to me that this will fill the bill for a project my friend asked me to take on.  Looking to track wind direction on a sailboat relative to the boat frame of reference, and display on an lcd display.   Stretch goal is to get boat heading with a differential gps.  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ajmorin369
    ajmorin369 over 3 years ago in reply to robogary

    Thank you for your response, it was very helpful and gave me an insight to what I might need to change to be able to get selected. Again, thank you and I appreciate your time in responding to my question.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ajmorin369
    ajmorin369 over 3 years ago in reply to shabaz

    Hello again Shabaz, thank you so much for spending some of your time to respond my question. I greatly appreciate your response because you gave me lots of different things that I may not have considered before and gave me some information that I knew already but from a different perspective. I have definitely gained knowledge that hopefully will help me in being selected for a roadtest in the future.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to ajmorin369

    No problem at all! I was thinking, another thing to do meanwhile could be to write any short blog, it will get you familiar with the editor menu/toolbar that is used for blogs and reviews, and you'll be able to insert photos etc. It could be on any tech topic, or tech related news you've heard, or any problem you want to solve, or anything to be honest. For example, I was going to write a paragraph or two today about a power cut in my area, and how I couldn't tell if things were damaged, for instance, since some faults may reveal themselves later. Any blog you write could be used as an example in your RoadTest applications, of material you've written. Not saying it will definitely help, but I suspect it will because it proves you're committing time and reporting stuff just as if it were a review, and that can be more important that prior technical knowledge in a specific area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to shabaz

    I think it would be fair to say, the level of community participation has an impact on the application. Your suggestion of a blog post is one such example.  This would be especially true for first-timers. You need to establish a presence for the committee to get to know you. If I was on the committee and the application was my introduction that is a pretty tough call to say yes I will go with an unknown. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 3 years ago in reply to ajmorin369

    Start small and then go for the more expensive devices after you get your trusted road tester rating.

    My first road test was for a MEMS microphone.

    It was easy to test and led to better things to test in the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<