RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum ROADTEST POLL - Would you be interested in Roadtest a MCU board with High-Precision On-Chip Analog Front End?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 2750 subscribers
  • Views 4474 views
  • Users 0 members are here
  • RTK0ESXB10C00001BJ
  • RX23e-a
  • roadtest survey
  • renesas
Related

ROADTEST POLL - Would you be interested in Roadtest a MCU board with High-Precision On-Chip Analog Front End?

rscasny
rscasny over 3 years ago

I've been speaking with a supplier who would like element14 to roadtest a MCU board. I'd like to gauge your interest. Here's some information about it and some documentation links:

imageSolution Starter Kit for RX23E-A MCU

Using the evaluation board (RSSK RX23E-A) equipped with RX23E-A and peripheral circuits for sensor measurement, and software that can be downloaded from the web, you can start analog characteristic evaluation immediately after purchasing the kit. By using this kit, it is possible to shorten the development period and bring it to market quickly.

About RX23E-A MCU

RX23E-A is a group from the RX MCU family with integrated high-precision analog front-end. Thanks to low noise and low drift of analog front-end features, the high-precision sensor measurement can be achieved with computation performance, system control, and communication in one chip. Refer to the RX23E-A product page for more detail.

RSSK Configuration and Evaluation Circuit

The kit consists of an evaluation board with the RX23E-A and peripheral circuits for sensor measurement, a K-type thermocouple, and is provided with the GUI and sample programs. These ready-to-use tools enable users to start evaluation of the A/D converter without hardware modification or software development.

The kit can be utilized to evaluate the measurements of thermocouples, RTD, and strain gauges, which are typical sensors in industrial equipment. Our evaluation of K-type thermocouples using the RSSK shows that the measured temperature error is within ±0.6°C under environments between -40°C and 85°C and the effective resolution is 19.4 bit, which means temperature deviation is equivalent to 0.0015°C at rms value. The measured temperature error, which is within the sensor error, validates the evaluation board as a reference design.

Documentation

RX23e-a datasheet 
Analog Front-End Mounted 32-bit Microcontroller Ideal for High Precision Sensing, Test and Measurement Equipment 

For more information

  • Sign in to reply
  • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    This sounds familiar:

    image

     Keithley DMM6500 Scanner Card - mystery component hidden in one of the channels 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    Link to the kit: https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/rtk0esxb10c00001bj-renesas-solution-starter-kit-rx23e

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 3 years ago

    I was wondering why they would choose a thermocouple as a high-precision sensor given thermocouples are slow to react and are not very precise. 

    rscasny said:
    temperature error is within ±0.6°C

    I see closer to ±2.5°C with K-type thermocouples until you get down to the 40 AWG wire size and depends a lot on the type of weld at the tip.

    The micro could be easily used in a datalogger design with CAN bus, I2C, SPI, and multiple serial ports.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • neerajrd82
    neerajrd82 over 3 years ago

    Yes, i would like to road test this MCU because this can help us to reduce the cost of oscilloscope design. But still i have voted "Maybe" because of compiler & licensing issues. if GCC for this is available, then there should be No problem in evaluation of this board. I would like similar ARM based board.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to Jan Cumps

     Jan Cumps  I admit, the strain gauge application is pretty intriguing.  With that level of resolution, you could probably count coins by weight with almost 100% accuracy.  Maybe even wind speed - and direction.  Accurate flow meter.  I'm sure that someone is going to do great things with it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to kmikemoo

    It would be an opportunity for engineers that want to gain expertise with a manufacturer that's used a lot in industry.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 3 years ago

    A very interesting board.

    If my current ability was up to it, I can see lots of uses for this board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    It's very interesting but I doubt that I could do more with the MCU than the included examples.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • manojroy123
    manojroy123 over 3 years ago

    I am very much intrested in this kit I want to use it as a temperature sensor for PCB desoldering. while reworking on pcb using hot air gun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to misaz
    misaz said:
    Also Renesas provide port of GCC for their RX family. jancumps know more information about it and If I remember correctly he mentioned some restrictions like that some example projects are hard to compile with free GCC and crypto accelerator is impossible to use, but generaly it should be possible to develop for this MCU for free at least in a limited way.

    That was for the RX65 member of the RX proprietary core:

    • Generic examples were easy to switch to GCC
    • Examples where you had to modify linker scripts (to reserve big areas of memory for display buffers) were somewhat harder, because the Renesas toolchain has a very different memory map / linker way of working. But doable. see  Renesas RX65 Envision Kit - part 12: RAM Use with GCC ToolChain and Renesas RX65 Envision Kit - part 10: Reserve LCD Frame Buffer in Expansion RAM with GCC.
    • Examples that used FAT and encryption were not portable at the time, because only provided as Renesas toolchain precompiled blobs. See  Renesas RX65 Envision Kit - part 3: Port an example from Renesas toolchain to GCC .
      This has now somewhat changed: Renesas customers that use the GCC toolchain can now request the crypto source code: www.renesas.com/.../crypto-library. 

      Obtaining the product
      We will provide the product to customers who will be adopting or plan to adopt a Renesas microcontroller. Please contact your local Renesas Electronics sales office or distributor.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>