I am trying to install TMCL-IDE for windows. I am getting this error. Please help me in solving it.

I am trying to install TMCL-IDE for windows. I am getting this error. Please help me in solving it.
After asking on chatgpt it says that you need to configure the motor from Wizard Pool in TMCL-IDE 4.x. But Wizard Pool is not showing any motor. Bellow is the pic of it.

How to know what has caused the error of device not detection on Wizard Pool of the TMCL-IDE 4.x
May be relevant ?
"I found that most of my plugins were disabled.
Once I enabled them again, I was able to use the wizard."
May be relevant ?
"I found that most of my plugins were disabled.
Once I enabled them again, I was able to use the wizard."
It looks like it turns red once the motor supply voltage reaches an acceptable threshold but it's the type of behaviour that would be best verified by referring to the user documentation for the TMCL-IDE.
For motion control which board to select TMC9660-3PH-EVKIT(BOOT) or TMC9660-3PH-EVKIT(PARAM)
But what about driver board. Which driver board should I select.
This may be relevant

and may explain why it isn't showing in TMCL-IDE device tree on the Linux version.
This may be an issue as you don't really want to commit to using the OTP just yet, and looks like the config data is lost if the board is power cycled/reset.
Perhaps need to consider resolving this first before jumping ahead to the Wizard Pool ?
There appears to be a separate tool
that can configure the bootloader independently of the one built into TMCL-IDE
https://www.analog.com/en/resources/app-notes/an-2601.html
If nothing else, the following two commands look like they could give useful information:
Command: inspect chip
Command: inspect config
Do you mean this one ?


Which driver board to select and what HW ID to set.
Yes. I am using a 12 volt 8 amp power supply.