Browse By Tags

  • Corrupt libraries

    Hello Experts! My name is Jocke. I'm working in a engineering office together with 2 colleagues, we are all using Altium Designer. We are in the progress of merging all our "private libraries" living on our individual CAD station to an server folder…
  • Circuit Studio Crashing when editing a library

    Hi, I've got an issue with my Circuit Studio crashing. I have a few libraries (schlib / pcblib, not intlib) that I use. All bar one work fine, and I can open, edit etc with no issues. However, one of my symbol libraries causes CS to completely lock up…
  • Editing and recompiling an Integrated Library

    Integrated libraries are a useful feature of CircuitStudio (and Altium Designer). These libraries contain schematic symbols, footprints and 3D models all compiled into the one single file. Many integrated libraries are made freely available by Altium…
  • Using componentsearchengine.com libraries with CircuitStudio

    SamacSys provide a large online component library that supports a number of different PCB design tools and they have now added full instructions for using their library with CircuitStudio. The parts are free and it's great to see support for our favourite…
  • CircuitStudio Hidden Commands

    Applies to Versions: [1.5.1] CircuitStudio, through its use of a modern ribbon interface, is designed to be easy to use and accessible to those whose full time job is not PCB design. Those wishing to access the full power of the product will be interested…
  • Can Vault components be edited and saved in local libraries?

    The Vault components are intended for consumption only, not for modification, so creating a local library is not officially supported, and copied components will revert to their original form due to being updated with the original information from the…
  • Visibility of Designator and Comment in Schematic Library(SCHLib)

    Applies to Versions : All Since Designators and Comments for schematic symbols are default to autoposition behavior, their visibility while editing within the Schematic Library Editor can be disabled so you do not have to worry about their positions.…