3D Printing
  • Technologies
  • More
3D Printing
Blog Obsolete Potentiometer Controls: 3D Printing to the Rescue!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Jul 2025 1:38 AM Date Created
  • Views 5052 views
  • Likes 16 likes
  • Comments 23 comments
  • slide control
  • potentiometer
  • hifi
  • hi-fi
  • rotary control
Related
Recommended

Obsolete Potentiometer Controls: 3D Printing to the Rescue!

shabaz
shabaz
11 Jul 2025

I suspect this is a common problem; lots of old Hi-Fi equipment have worn out pots and other controls, and it can be quite difficult locating exact replacement parts.

A friend had a music device (It’s a sort of DJ CD player with a lot of controls) around 30 years old, and it had a really worn down front panel. The controls were scratchy to operate, and in some cases, the grease had hardened, and the controls were very stiff. Some controls didn’t work, and others were crackly. Someone had already tried to clean it with a can of WD40.

Ordinarily I would turn down such a repair request, but it’s a friend, and he was pretty passionate about this particular device, he had no desire to replace with a modern digital solid-state music player. I decided to fix it, and ran into the problem that I simply couldn’t find alternative potentiometers that would precisely fit.

I briefly considered reverse-engineering the entire front panel board to rebuild it from scratch, but that would have been a lot of work. I decided to focus on the potentiometers instead.


I searched around and found some potentiometers that had the correct shaft (my friend didn’t want the plastic knobs to be altered from the original ones), but the potentiometers themselves were a lot smaller. After some brainstorming, I realized that I could make a little plastic adapter, and use a flexible PCB to route the pins of the potentiometer to match the original potentiometer.


I designed it using FreeCAD (I am still a learner, hence the design is simplistic).

image



I don’t own a 3D printer, so I had to use a 3D printing service (I used J.L.C.), it was surprisingly low-cost. I chose to print in nylon, which is quite tough and reasonably heat-resistant.

I designed the flexible PCB using KiCad, and again used the overseas manufacturer to order it. See  Creating a Flexible PCB!  

For the potentiometer pins, I used 2.54 mm pin headers, and pulled out every other pin since I needed 5.08 mm spacing.

image



For the slider potentiometers, I did a similar thing, only I was able to use a normal PCB instead of a flexible one:

image


And here’s the final result! I used epoxy glue to fix the rotary potentiometer into its new 3D printed housing, and to attach the slider pot PCB onto its 3D printed base.

image

One down, about 23 more to go!

image

Thanks for reading.

  • Sign in to reply

Top Comments

  • kmikemoo
    kmikemoo over 1 year ago +1
    shabaz NICE! That's a brilliant solution.
  • shabaz
    shabaz over 1 year ago in reply to kmikemoo +1
    Hi Mike, Thanks! First it felt extreme to repair like this, but on the other hand music enthusiasts get obsessive regarding their equipment they love, so it only seemed proportionate!
  • Fred27
    Fred27 over 1 year ago +1
    shabaz You've helped me so much (both directly and indirectly) on here that Id be happy to churn out a few 3D prints for you. One of the best things about 3D printing is not creating an object but being…
Parents
  • Fred27
    Fred27 over 1 year ago

    shabaz  You've helped me so much (both directly and indirectly) on here that Id be happy to churn out a few 3D prints for you.

    One of the best things about 3D printing is not creating an object but being able to iterate. For something small I sometimes create V1 as a test fit and almost expect a V2 to follow.

    I recently ditched fiddling with Creality printers and grabbed a Bambu P1S with AMS when it was on sale for £699. Night and day difference on the need for fiddling and tweaking. It really is reliable enough to click "go" and just come back later to a finished print. It's since dropped to £549. If you're close to getting on then I'd really recommend it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 1 year ago

    shabaz  You've helped me so much (both directly and indirectly) on here that Id be happy to churn out a few 3D prints for you.

    One of the best things about 3D printing is not creating an object but being able to iterate. For something small I sometimes create V1 as a test fit and almost expect a V2 to follow.

    I recently ditched fiddling with Creality printers and grabbed a Bambu P1S with AMS when it was on sale for £699. Night and day difference on the need for fiddling and tweaking. It really is reliable enough to click "go" and just come back later to a finished print. It's since dropped to £549. If you're close to getting on then I'd really recommend it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 1 year ago in reply to Fred27

    Hi Fred thanks for the kind comments, and really nice offer! I'll keep an eye out for a Bambu model, maybe get one at some point this year. Not sure how much I want to spend just yet, but it does make sense to at least have a quick way to test a V1 now that Im getting a bit more familiar with 3D work (although I still can only design very blocky stuff!). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to Fred27

    I've been thinking about the Bambu , very interested to see your comments.

    MK