3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Building a 3D printer out of Hp G85 Office jet printers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 341 subscribers
  • Views 2878 views
  • Users 0 members are here
Related

Building a 3D printer out of Hp G85 Office jet printers

e14 Contributor
e14 Contributor over 12 years ago

Hello there my friends... so i saw these 3D printer things... and i thought it would be cool to try to make one... now i have no background with Arduino at all... but i do have a little bit of knowlege when it comes to CNC's... see my father purchased 6 of these Hp G85 office jets this was a loooong time ago at least 12 years ago recently the last of them died and was replaced with a newer inkjet...

and so with the permission of my father i started disassembling one of these printers to see if they could be of use...

 

parts of notable significance

 

steppers 2 steppers per printer... both have encoders not sure if they are useful to me though

rails there are 2 rails per printer aswell

belts two belts per printer and gears/ sprockets to go with the belts...

cold cathode light (from the scanner) useful for other projects and possibly for built in lighting on the 3d printer...

Glass plate from the scanner

various springs and stuff

 

that seems to be it

 

so my question is could i use 2-3 of these printers to build a 3d printer

will the steppers be adequate?

if not what steppers are recommended?

where can i find a mc-mega dev board and a RAMPS Sheild?

 

my goal design is to build one similar to the portable one ben heck built... although mine wont be portable...

 

any information you have to share with me would be greatly appreciated!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    That sounds like a Cartesian-format layout (take a look at the Mendel or Prusa i3) and definitely the Arduino MEGA + RAMPS is a good way to go. Most of the other common boards (RAMBO, etc) are just combined…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Here is a extremely basic 2d drawing of what i plan to build

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago in reply to e14 Contributor

    A comment is that the two steppers on one belt was listed as a major design fault in the Prusa Mendel.

    It may be easier to use a single stepper with a tension belt system to avoid the pains in alignment, maintenance and the case of where you need to manually move the Z axis (for example, if it jams)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago in reply to e14 Contributor

    A comment is that the two steppers on one belt was listed as a major design fault in the Prusa Mendel.

    It may be easier to use a single stepper with a tension belt system to avoid the pains in alignment, maintenance and the case of where you need to manually move the Z axis (for example, if it jams)