3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum 3D printer help - Parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 341 subscribers
  • Views 1299 views
  • Users 0 members are here
Related

3D printer help - Parts

e14 Contributor
e14 Contributor over 12 years ago

Hi, I am building a CNC Router at the moment and I inspired my cousin to build a 3D printer.. ive pretty much told him what he will need to build it, quite similar to a CNC Router im pretty sure..

These are the parts I think he will need:

4x Stepper Motors

1x 3 Axis Driver Board

1x 24v Power Supply

1x 200x200 heated bed

1x Extruder

and something to feed the plastic (Thats what the 4th stepper motor is for)

 

Just needed some recommendations on what driver board he should use, and what extruder. The bed is going to be about 200x200mm and I was just wondering what size the stepper motors should be.. We are going to design it so that the bed moves instead of all the uprights for one of the axis so that should scale down the motors a bit, my 1200x750mm Router is only using 287oz steppers and the bed will move for that aswell so i was guessing he might only need like 200oz or like 150oz  motors? Help would be appreciated!

 

Any more info needed? feel free to ask!

 

-Bailey

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 12 years ago +1
    Hello Bailey The way it sounds your design would be similar to a Reprap (Cartesian style). The bed moves in the y while the print head moves in the x and the whole extruder platform moves in the z. I would…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Bailey,

     

    Nate has it right there - NEMA 17 motors typically afford more than enough torque for most 3D printers, as they do not have the robust force requirements of a subtractive-manufacturing system like a CNC cutter. RAMPS (1.4 is the current standard) is a shield for the Arduino MEGA microcontroller board, and then the stepper motor drivers are fit to the RAMPS interface points.

    image

    I typically use something like the Pololu controllers, and you will need one per stepper motor you are controlling. A complete set of RAMPS+Arduino MEGA+Pololu drivers (x4-5) costs around $40 USD on eBay if you watch for a good deal. I also use the all-in-one combinations like the Mightyboard or RAMBO for more compact printers but those are produced in lower volume, so tend to run around $80 USD each for the same capability in a single board.

     

    The J-head and Budaschnozzle are very popular, and available from several vendors for a good price.

     

    Kirk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks heaps for you replies!

     

    We have looked around and found everything we may need, ill link them all below and tell me what you think, if you think i should change anything, and feedback would be great!

    Stepper Motors

    Controller Board

    Extruder

    Heated Platform

    Power Supply

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Bailey,

     

    That looks like a great start! The heated bed is nice to have, but you can print using PLA or Nylon filament without it as a requirement if you are trying to cut your costs. You definitely need a heated build plate for ABS filament, though. You will need filament, so selecting the type(s) of filament you want to use early can help you decide if you need components like the heated build plate. You will also need to plan your structural elements, to ensure that your printer can move where needed (linear bearings, guide rods, etc) but will be rigid enough to support the build.

     

    Kirk Hausman

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Okay cool, are they good size stepper motors and hows the controller board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Okay cool, are they good size stepper motors and hows the controller board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Nate1616
    0 Nate1616 over 12 years ago in reply to e14 Contributor

    The Gen6 controller board will work just fine.  Just remember that having a single board solution isn't always the best.  I'm not trying to persuade you into another one but just want you to be aware that if a stepper driver fails, which I have had numerous times over the years your soldering skills will need to be up to par.  Where for example with the Ramps you just purchase a new module and swap out for the faulty one.  Like I said before the Gen6 is a great board.

    Your selected stepper motors will work great!

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Nate1616

    Do you know if them stepper motors would hold an aluminium frame well?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Bailey, you can use aluminum framing or other materials, and the stepper motors can be directly connected or mounted using a milled or 3d printed mount depending on what you have available. I am not sure what you are asking if the steppers can "hold" the frame though. Can you provide more detail?

     

    Kirk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    We would do it similar to Ben Hecks 3D Printer.. there will be two motors pulling up the whole cross section with threaded rods.. if you dont know what im talking about check out his video here: Double Decker 3D Printer Part 3 - YouTube

     

    Except, if obviously possible it will pretty much all be aluminum..

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    In that configuration, your aluminum framing should be low-mass and should work well with the NEMA 17 or larger stepper motors. I would not use smaller NEMA 14 motors although those might work in a pinch.

     

    Kirk