3D Printing
  • Technologies
  • More
3D Printing
Files Robox Quick Start Guide
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Next
  • Previous
  • Share
  • More
  • Cancel
  • Author Author: joeman
  • Views 1415 views
  • Downloads 0 downloads
  • Likes 3 likes
  • Comments 7 comments
Related
Recommended

Robox Quick Start Guide

This is Robox! Designed to be the simplest, most reliable and comprehensive 3D printing platform available.

  • start
  • quick
  • guide
  • robox
joeman
joeman
  • 23 Jun 2015
  • 0 Downloads
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to chappy1978 +2
    In quick Order Yes it has a heated bed yes it is in an enclosure yes it can do ABS, PLA, PET and many others no it is not proprietary filament, you can get their reels that have chips for very easy setup…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    I have had mine for a few months now and im currently not so convinced at that statement " This is Robox! Designed to be the simplest, most reliable and comprehensive 3D printing platform available." I…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    so an update on my Robox CEL Printer, it appears I had a faulty power cable *Intermittent connection ) going to the head that ultimately caused the head to overheat and also flickering LEDs , fan stopping…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to chappy1978

    your welcome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • chappy1978
    chappy1978 over 10 years ago in reply to Robert Peter Oakes

    That was a quick and straightforward response. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to chappy1978

    In quick Order

     

    Yes it has a heated bed

    yes it is in an enclosure

    yes it can do ABS, PLA, PET and many others

    no it is not proprietary filament, you can get their reels that have chips for very easy setup or you can use 3rd party ones and set the parameters your self

    yes it is very easy to use yes it will run on its own once the file is uploaded from your pc

    yes it suffers from the same issue as most other printers in that ABS has a tendency to curl on the corners, PLA is way better

    yes it has a 2 year warranty and the folks at Robox are excelent to work with

     

    How do I know this

    I have had one for a year now and have needed to use the warranty and was very satisfied with the process and outcome

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • chappy1978
    chappy1978 over 10 years ago

    I would really like to have a chance to see one in person so I could test out how easy they claim it to be. Does it have a heated print bed. Can it print ABS? The other thing that comes to mind are those filaments propriety?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    so an update on my Robox CEL Printer, it appears I had a faulty power cable *Intermittent connection ) going to the head that ultimately caused the head to overheat and also flickering LEDs , fan stopping etc when running, sent the printer in to CEL USA repair center for warranty repair and now have it back. CEL center in the USA for repairs makes it much more viable for North America servicing. and they where excellent, kept me informed through the entire process and even sent back the calibration / test print with the printer to show it was working well.

     

    BEN was my contact and repair technician there, Well done and thanks

     

    So with the head replaced and the power cable to the head also replaced I now have no flickering lights, or intermittent head not detected issues (This time the system accepted a head the first time I attached it, I had never had that since new), so far the test prints are showing up very well and no sign of previous issues, time to try some real print jobs (20Hr run types)

     

    in summary, when these printers are working they are excellent, most people do not have issues and if you do, CEL / Robox have proved to me that they will go the extra mile to get the issues resolved and get you up and running again. so I would still recommend this printer to anyone where the print size fits there needs.

     

    Cons of the printer, like pretty much all 3D printers, ABS is a pain in the ass to get right and use of skirts or additional thin islands on corners etc is essential to improving the print, Filament from CEL is expensive compared to other sources

     

    PRO, when using PLA I have yet to have a bad print and the quality has been very good, the printer is well built and has all the features needed like bed heating, enclosed print area for better quality prints, the ability to take the entire gcode for the print allowing you to disconnect or power off your pc while the job runs

     

    notes:

    It is essential to keep up to date with the Firmware and Desktop Software, the latest version massively improves bed leveling detection and has made a big difference in the print quality of the first few layers

    A new dual extruder head is imminent for the printer and is supposed to be at a reasonable price, still waiting for the laser head though image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>