3D Printing
  • Technologies
  • More
3D Printing
Documents 3D Printing Wishlist - What do I need to begin 3D Printing?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 20 Oct 2021 2:54 PM Date Created
  • Last Updated Last Updated: 17 Jan 2023 5:52 PM
  • Views 32521 views
  • Likes 7 likes
  • Comments 22 comments
Related
Recommended

3D Printing Wishlist - What do I need to begin 3D Printing?

image

 

One of the coolest technologies to emerge in the last decade is 3D printing. 3D printers are incredibly versatile tools that can print virtually anything you need. The technology has improved by leaps and bounds since its inception, and incredibly accurate, high resolution 3D prints can now be made pretty inexpensively.

We've put together a wish list with all the fundamental items needed to set you up for a life in 3D Printing

3D Printers

Let's start with the 3D printer itself. There is a wide range to choose from. Select based on what you want to print, your skill level, the materials you want to print with, the size of the prints you want to make, and most importantly, budget. Whether you're printing industrial parts for machine automation or little knick-knacks to decorate your desk, there's a 3D printer for you.

Flashforge Adventurer 3

Flashforge Adventurer 3

 

image

Ultimaker S3

Glue Stick

In order to create a great 3D print, build plate adhesion is extremely important. If your print won't stay still, accuracy will suffer. Hairspray is popular for adhesion, but glue is more precise and creates less of a mess.

image

Magigoo Glue Stick

Deburring Tool

Many 3D prints end up with small pieces of protruding plastic that have to be cleaned up. A deburring tool makes the process easier, and with less chance of screwing up and destroying your print. Deburring tools are especially good for cleaning up modeled holes.

image

Ruko Deburring Tool

Pliers

Pliers are useful on any bench and 3D printing is no exception. Use your pliers for print core maintenance, repairs, or removing support material.

Needle-nose pliers

Flat Nosed Pliers

Masking Tape

Masking tape is incredibly versatile in 3D printing. Add it to the print bed to protect it from scratches and to help 3D prints adhere. Heat resistant masking tape is preferred for heated beds.

Masking Tape

Masking Tape

Dremel

Dremels make smoothing a lot easier, but be careful! A Dremel can get hot, and material like PLA can melt. The sanding attachments work well, but keep those RPMs low.

image

Dremel Multitool

Different-sized Nozzles

Grab a vriety of nozzles for your 3D printer. Larger ones can print faster at the expense of resolution. Smaller ones can print with more detail, but are slower.

This example works with Ultimaker 3D printers.

0.4mm

image

0.4mm Nozzles

Filament

Don't forget to stock up on filaments in a variety of colors, including the shiny and translucent ones.

image

Multicomp Silver PLA Filament

Measuring Tools

Measuring tools are required for checking machine setup and print accuracy. You've probably already got a nice ruler, but adding something like digital calipers will take your accuracy to a new level.

image

Digital Calipers

Raspberry Pi to run OctoPrint.

OctoPrint (https://octoprint.org) is software that can control and monitor every aspect of your 3D printer from within a browser. You can do things like viewing a webcam feed of your print, monitor temperatures, or start/stop/pause the current print job. It's completely free. OctoPrint is also open source, and there are already a bunch of plugins from 3rd party developers available for it.

imageimage

Raspberry Pi 4 Starter Kit

How to 3D Print Webinar Series

Watch our 4 Part Webinar Series on 3D Printing on demand. We'll take you from your first print to designing prototypes.

image

Introduction to 3D Printing

image

Create your own 3D Models

image

Maintenance and Diagnosing Bad Prints

image

First Print Basics

  • 3d printer giveaway
  • 3D Printing
  • 3dprinting
  • 3dprintin
  • 3d print
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • qbytes.dq
    qbytes.dq over 4 years ago +11
    1) What's the first thing you're going to print and why? I would print a flow rate square. After printing, I would calculate my flow rate and update my Extrusion Multiplier (you should do this for every…
  • Fred27
    Fred27 over 4 years ago +1
    1) I've bought a couple of printers over the last couple of years - an Anycubic Photon resin printer and a Creality Ender 3 to replace a very old FDM printer that broke. One of the first things I printed…
  • fmilburn
    fmilburn over 4 years ago +1
    3D printers don’t make precise holes, especially on vertical sides, so a drill and bits / step bits are useful. A pin vise and small set of bits works well for small holes. I now use 3mm heat set threaded…
Parents
  • embeddedguy
    embeddedguy over 4 years ago

    Hi,

    I have previously used Ultimaker CURA 3D printer. Based on my past experience I would first print something like a small plate which assures me that the printer is working.

    Then as I am embedded systems and RaspberryPi fan, I would print some kind of enclosure for the RPI or any other board. I would also print tiny parts to stick RGB LED's on the nicely saped strips which can hold and increase the lifespan of RGB strips.

    2) What are we missing from this list?  Any special tools/procedures/secrets that you use to get the best 3D prints?

    I am not quite sure that weather you already thought about software design part of the 3D printing. It is one of the most important thing to consider when you design a 3D printing parts that how I will create my design. The option which I used was Autodest fusion 360 but there are other options as well. 

    The procesure is that first a 3D design needs to be prepared properly. While making a design one has to have a sense of how gravity works, because there are some shapes like a ball which can not be designed in one part. it needs two bouls to be joined together to create a ball out of this. How would one do this? What are the options?Thinking

    Lastly, the 3D design is exported to 3D printing software which might suggest to remove/make changes to some of the design parts, cause the software knows better and it is optimised for 3D printing itself rather than a 3D design software. Finally once the software gives thums upThumbsup one can print. The printer will suggest estimated time when the print will be ready.

    Finally you can start printing in the evening if you dont want to wait to much during the day. You have to make sure that the safety is considered. Like there is Fire alarm and fire safety where the 3D printer is kept.!! 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • embeddedguy
    embeddedguy over 4 years ago

    Hi,

    I have previously used Ultimaker CURA 3D printer. Based on my past experience I would first print something like a small plate which assures me that the printer is working.

    Then as I am embedded systems and RaspberryPi fan, I would print some kind of enclosure for the RPI or any other board. I would also print tiny parts to stick RGB LED's on the nicely saped strips which can hold and increase the lifespan of RGB strips.

    2) What are we missing from this list?  Any special tools/procedures/secrets that you use to get the best 3D prints?

    I am not quite sure that weather you already thought about software design part of the 3D printing. It is one of the most important thing to consider when you design a 3D printing parts that how I will create my design. The option which I used was Autodest fusion 360 but there are other options as well. 

    The procesure is that first a 3D design needs to be prepared properly. While making a design one has to have a sense of how gravity works, because there are some shapes like a ball which can not be designed in one part. it needs two bouls to be joined together to create a ball out of this. How would one do this? What are the options?Thinking

    Lastly, the 3D design is exported to 3D printing software which might suggest to remove/make changes to some of the design parts, cause the software knows better and it is optimised for 3D printing itself rather than a 3D design software. Finally once the software gives thums upThumbsup one can print. The printer will suggest estimated time when the print will be ready.

    Finally you can start printing in the evening if you dont want to wait to much during the day. You have to make sure that the safety is considered. Like there is Fire alarm and fire safety where the 3D printer is kept.!!