Artificial Intelligence and Machine Learning
  • Technologies
  • More
Artificial Intelligence and Machine Learning
Blog Accelerating the MediaPipe models on Raspberry Pi 5 AI Kit
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Artificial Intelligence and Machine Learning to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: albertabeef
  • Date Created: 16 Sep 2024 6:54 PM Date Created
  • Views 9230 views
  • Likes 5 likes
  • Comments 7 comments
  • tria
  • rpi5 ai kit
  • hailo8
  • palm detection
  • mediapipe
  • object detection
  • hailo8l
  • artificial intelligence
  • landmark detection
  • hailo
  • raspberry pi
  • machine learning
Related
Recommended

Accelerating the MediaPipe models on Raspberry Pi 5 AI Kit

albertabeef
albertabeef
16 Sep 2024
Accelerating the MediaPipe models on Raspberry Pi 5 AI Kit

Introduction

This project is part of a series on the subject of deploying the MediaPipe models to the edge on embedded platforms.

In this project, I will describe how to reproduce our results on the Raspberry Pi 5 AI Kit, which contains a Hailo-8L acceleration module, and report the profiling results.

Hailo Flow Overview

Hailo's AI Software Suite allows users to deploy models to the Hailo AI accelerators.

image
Hailo AI Software Suite - Workflow (Camera: Hailo)

In addition to the Hailo AI accelerator devices, Hailo offers a scalable range of PCIe Gen 3.0 compatible M.2 AI accelerator modules:

image
Hailo AI Acceleration Modules (Camera: AlbertaBeef)

This project will only cover the following Hailo AI acceleration modules:

  • Hailo-8L : M.2 B+M Key (PCIe Gen 3.0, 2 lanes), 13 TOPS

Setting up the Raspberry Pi 5 AI Kit

In order to setup the RPI5, please refer to the following documentation:

  • [github/hailo-ai] hailo-ai/hailo-rpi5-examples
image
RPI5 AI Kit Hardware Components (Camera: AlbertaBeef)

I purchased a pre-assembled kit from CanaKit, and followed their getting started instructions:

  • https://www.canakit.com/pi5-ai
image
Pre-assembled RPI5 AI Kit with Hailo-8L Acceleration (Camera: CanaKit)

The first step, after configuring the Raspberry Pi OS, was to open a terminal, update the system, and install the Hailo package:

sudo apt update
sudo apt full-upgrade

sudo apt install hailo-all

sudo reboot

After rebooting, I was able to identify the Hailo-8L acceleration module:

lspci
hailortcli fw-control identify
image
Identifying the Hailo-8L module on RPI5 AI Kit (Camera : AlbertaBeef)

Next, the Hailo example repository was cloned, and virtual environment created:

git clone https://github.com/hailo-ai/hailo-rpi5-examples.git
cd hailo-rpi5-examples

source setup_env.sh

Inside the virtual environment, the python requirements were installed, and demo resources downloaded

pip install -r requirements.txt

./download_resources.sh

Finally, the detection demo was launched

python basic_pipelines/detection.py --input resources/detection0.mp4
image
python basic_pipelines/detection.py --input resources/detection0.mp4 (Video camera : AlbertaBeef)

Now that we have verified that the Hailo-8L acceleration module is working, we can move on to our accelerated MediaPipe demo application.

A Note on the pre-compiled models for Hailo-8L

My understanding is that the RPI5 Hailo-8L integration was performed with Hailo AI SW Suite v2024–04, with models compiled with DFC v3.27.0. In preparation for this, I have compiled the Hailo-8L models using DFC v3.27.0:

  • Hailo8L models : blaze_models_hailo8l_dfc_v3.27.0.zip (compiled with DFC v3.27.0)

It turns out, the models compiled with the previous version of tools also worked fine, which is a testimony to the forward version compatibility of models in the Hailo flow.

  • Hailo-8L models : blaze_hailo8l_models.zip (compiled with DFC v3.25.0)

Installing the python application on the Raspberry Pi 5 AI Kit

The python application can be accessed from the following github repository:

git clone https://github.com/AlbertaBeef/blaze_app_python
cd blaze_app_python

The python demo application requires certain packages which can be installed as follows:

pip3 install tflite_runtime matplotlib plotly kaleido numpy==1.24

In order to successfully use the python demo with the original TFLite models, they need to be downloaded from the google web site:

cd blaze_tflite/models
source ./get_tflite_models.sh
cd ../..

In order to successfully use the python demo with the Hailo-8L models, they need to be downloaded as follows:

cd blaze_hailo/models
source ./get_hailo8l_models.sh
unzip -o blaze_hailo8l_models.zip
cp hailo8l/*.hef .
cd ..

Although I provide pre-compiled models for the face/pose detection and landmark models, only the palm detection and hand landmark models are currently working with the python demo application.

You are all set !

Launching the python application on the Raspberry Pi 5 AI Kit

The python application can launch many variations of the dual-inference pipeline, which can be filtered with the following arguments:

  • --blaze : hand | face | pose
  • --target : blaze_tflite |... | blaze_hailo |
  • --pipeline : specific name of pipeline (can be queried with --list argument)

In order to display the complete list of supported pipelines, launch the python script as follows:

rpi5aikit@raspberrypi:~/blaze_app_python# python3 blaze_detect_live.py --list
[INFO] user@hosthame : rpi5aikit@raspberrypi
[INFO] blaze_tflite supported ...
...
[INFO] blaze_hailo supported ...
...
Command line options:
--input :
--image : False
--blaze : hand,face,pose
--target : blaze_tflite,blaze_pytorch,blaze_vitisai,blaze_hailo
--pipeline : all
--list : True
--debug : False
--withoutview : False
--profilelog : False
--profileview : False
--fps : False

List of target pipelines:
...
07 hai_hand_v0_10_lite blaze_hailo/models/palm_detection_lite.hef
blaze_hailo/models/hand_landmark_lite.hef
08 hai_hand_v0_10_full blaze_hailo/models/palm_detection_full.hef
blaze_hailo/models/hand_landmark_lite.hef
...

In order to launch the Hailo-8L pipeline for hand detection and landmarks on the rpi’s desktop, use the python script as follows::

python3 blaze_detect_live.py --pipeline=hai_hand_v0_10_lite

This will launch the 0.10 (lite) version of the model, compiled for Hailo-8L, as shown below:

image
python3 blaze_detect_live.py --pipeline=hai_hand_v0_10_lite (Video camera : AlbertaBeef)

The previous video has not been accelerated. It shows the frame rate to be the maximum 30 fps when no hands are detected (one model running : palm detection), approximately 26-28 fps when one hand has been detected (two models running : palm detection and hand landmarks), and approximately 22-25 fps when two hands have been detected (three models running : palm detection and 2 hand landmarks).

It is worth noting that this is running with a single-threaded python script. There is an opportunity for increased performance with a multi-threaded implementation. While the graph runner is waiting for transfers from one model's sub-graphs, another (or several other) model(s) could be launched in parallel...

There is also an opportunity to accelerate the rest of the pipeline with C++ code...

Benchmarking the models on the Raspberry Pi 5 AI Kit

For reasons which I have not resolved, the "--profileview" argument does not work well on the Raspberry Pi, so we will use the "--profilelog" argument instead.

The profiling functionality uses a test image that can be downloaded from Google as follows:

source ./get_test_images.sh

The following commands can be used to generate profile results for the hai_hand_v0_10_lite pipeline using the Hailo-8L models, and the test image:

rm blaze_detect_live.csv
python3 blaze_detect_live.py --pipeline=hai_hand_v0_10_lite --image --withoutview --profilelog
mv blaze_detect_live.csv blaze_detect_live_rpi5aikit_hai_hand_v0_10_lite.csv

The following commands can be used to generate profile results for the tfl_hand_v0_10_lite pipeline using the TFLite models, and the test image:

rm blaze_detect_live.csv
python3 blaze_detect_live.py --pipeline=tfl_hand_v0_10_lite --image --withoutview --profilelog
mv blaze_detect_live.csv blaze_detect_live_rpi5aikit_tfl_hand_v0_10_lite.csv

The same is done for the hai_hand_v0_10_full & tfl_hand_v0_10_full models.

The results of all.csv files were averaged, then plotted using Excel.

Here are the profiling results for the 0.07 and 0.10 versions of the models deployed with Hailo-8L, in comparison to the reference TFLite models:

image
Palm Detection + Hand Landmarks - Hailo-8L Acceleration (Camera: AlbertaBeef)

If we plot the acceleration ratios of the execution times for the Hailo-8L models with respect to the TFLite models, we get the following results:

image
Palm Detection + Hand Landmarks - Hailo-8L Acceleration ratios (Camera: AlbertaBeef)

The models were accelerated by a factor of 5.6x, and the full palm+hand pipeline was accelerated by a factor of 3.8x.

Again, it is worth noting that these benchmarks have been taken with a single-threaded python script. There is additional opportunity for acceleration with a multi-threaded implementation. While the graph runner is waiting for transfers from one model's sub-graphs, another (or several other) model(s) could be launched in parallel...

There is also an opportunity to accelerate the rest of the pipeline with C++ code...

Conclusion

I hope this project will inspire you to implement your own custom application.

What applications would you like to see built on top of these foundational MediaPipe models ?

Let me know in the comments...

Acknowledgements

I want to thank Gianluca Filippini (EBV) for his pioneering work with the Hailo-8 AI Accelerator module, and bringing this marvel to my attention. His feedback, guidance, and insight have been invaluable.

References

    • [Google] MediaPipe Solutions Guide : https://ai.google.dev/edge/mediapipe/solutions/guide
    • [Hailo] Hailo AI SW Suite Documentation :https://hailo.ai/products/hailo-software/hailo-ai-software-suite
    • [Hailo] Hailo Developer Zone : https://hailo.ai/developer-zone
    • [AlbertaBeef] blaze_app_python : AlbertaBeef/blaze_app_python
    • [Hackster] Blazing Fast Models
    • [Hackster] Accelerating the MediaPipe models with Hailo-8
    • [Hackster] Accelerating the MediaPipe models with Raspberry Pi 5 AI Kit
    • Sign in to reply
    • ralphjy
      ralphjy over 2 years ago in reply to albertabeef

      Mario,

      I have a newer (than the C525) eMeet C980 webcam that I just tried and it does run around 30 fps.  I'll have to compare the profile logs from the two cameras later.  I haven't modified your blaze_detect_live.py script so I should be using 640x480.  I have to admit that the logs aren't the easiest to interpret.  Probably just an issue with the camera interface.  

      Ralph

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • albertabeef
      albertabeef over 2 years ago in reply to ralphjy

      Ralph,

      Yes, I ran my profililing using the webcam with input size of 640x480.

      Which input resolution are you using ?  If you have a higher resolution, then the resize of probably slowing down your pipeline.

      If you enable "--profilelog", you will see detailed measurements for each component (including resize & pre-processing).

      Cheers !

      Mario.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • albertabeef
      albertabeef over 2 years ago in reply to ralphjy

      Ralph,


      Thank you.  The group I am part of, Avnet Embedded, is now called "Tria Technologies".

      Mario.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • ralphjy
      ralphjy over 2 years ago

      albertabeef 

      Hi Mario,

      Finally got to try this out today.  It appears that you are only running with a webcam?  I didn't see an option for a CSI cam.

      I'm only getting around 15 fps running the hai_hand_v0_10_lite model.  I verified that I have PCIe Gen3 enabled in the config.

      I seem to do okay running the hailo-rpi5-examples.  Any suggestions as to what to check in my setup?  I don't have the preassembled unit like yours but the base components are essentially the same.  I'm using a RPi Camera 3 module and a Logitech C525 webcam.  Maybe my webcam interface is slow.

      Great work putting this together!

      Thanks,

      Ralph

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    • DAB
      DAB over 2 years ago

      Very good informative post.

      Well done.

      • Cancel
      • Vote Up 0 Vote Down
      • Sign in to reply
      • More
      • Cancel
    >