Artificial Intelligence and Machine Learning
  • Technologies
  • More
Artificial Intelligence and Machine Learning
Forum Update on LB
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Artificial Intelligence and Machine Learning to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 94 subscribers
  • Views 326 views
  • Users 0 members are here
Related

Update on LB

e14 Contributor
e14 Contributor 5 months ago

Hi there i have been away for a bit but now i am back with an update on my Little *** Project. 
Little *** is my AI car i am building. I am no tech expert and i am putting this together through pure passion for modified cars and tech. 

So lets get in to it.... 

Little *** AI – Project Update

The Little *** AI project is continuing to evolve from a modified car concept into a fully integrated AI-driven vehicle system combining embedded control, local AI processing, visual systems, sensors, and custom electronics.

The original goal was never to build a polished corporate system or a supercar-style showcase. The aim has always been to create something unique, experimental, modular, fun, repairable, and achievable using affordable hardware and a lot of hands-on design work.

This is still very much an active build and development project. A lot of the system is currently being prototyped, redesigned, rebuilt, and refined as the project evolves.

Current Core Hardware Direction

Planned Main AI System

  • Lenovo Legion 5 gaming laptop

  • Intel i7 CPU

  • RTX 3060 GPU

  • Local AI model hosting and processing

The next major step for the project is moving Little *** AI onto a dedicated RTX-powered laptop system to allow proper local AI processing inside the vehicle.

The goal is for the laptop to eventually handle:

  • local language models

  • voice processing

  • reasoning

  • future AI camera processing

  • advanced vehicle behaviours

The move to a dedicated RTX system comes from wanting faster local AI performance while still allowing the vehicle to operate offline when needed.

At the moment, I am still sourcing the laptop and hoping to have this side of the project moving properly by the end of June.


Vehicle Control & Embedded Systems

Current hardware already being integrated includes:

  • Raspberry Pi 5 (16GB)

  • M5Stack module

  • ESP32-S3 controllers

  • NodeMCU ESP8266 controllers

The Raspberry Pi 5 is currently acting as the main bridge between systems, controllers, sensors, networking, and future AI integration.

The M5Stack is planned to handle lightweight fast-response interaction and quick vehicle actions while the larger AI systems process deeper requests.

The ESP32-S3 and NodeMCU boards are being distributed throughout the vehicle to control:

  • lighting

  • visual effects

  • displays

  • sensors

  • future smart-mod systems

A lot of people ask why I use NodeMCUs and S3 boards instead of more expensive industrial hardware.

The answer is simple:

  • they are affordable

  • easy to replace

  • easy to prototype with

  • widely supported

  • ideal for modular experimentation

This project is heavily focused on practical iteration and learning through building rather than chasing expensive hardware for the sake of it.


Wiring Philosophy

Another thing people usually notice is the use of screw terminal adapters instead of permanently soldering every connection directly.

This is intentional.

The system is being designed to stay:

  • modular

  • serviceable

  • replaceable

  • easier to debug

When experimenting with large distributed electronics systems inside a vehicle, being able to quickly swap or isolate a controller is far more practical than repeatedly desoldering wiring.


Sensor Systems

Current and planned sensors include:

  • digital microphones

  • PIR sensors

  • human presence sensors

  • mmWave presence detection

  • AI camera systems

  • vehicle telemetry integration

The long-term goal is for the vehicle to eventually react differently depending on:

  • presence

  • interaction

  • environment

  • AI state

  • security/sentry conditions


Rear “Circuit Display” System

One of the biggest custom fabrication parts of the project so far has been the rear AI circuit display.

The display combines:

  • mirrored surfaces

  • custom-cut perforated hex paneling

  • distributed controller mounting

  • RGB lighting systems

  • a custom illuminated “processor core”

  • visible modular electronics

The processor core has recently been redesigned to use an 8x8 LED matrix behind an opal acrylic diffuser after earlier LED strip prototypes produced uneven lighting results.

The controller layout has also already gone through several redesigns to improve:

  • symmetry

  • accessibility

  • cable routing

  • serviceability

  • visual balance

The aim is to make the display feel less like decorative RGB lighting and more like an exposed AI-powered electronic system.


Software Direction

The software side is also slowly evolving into a more structured “Little *** AI” architecture.

The long-term goal is for the system to eventually support:

  • local-first AI operation

  • offline functionality

  • distributed controller communication

  • AI-assisted vehicle interaction

  • onboard visual and sensor feedback systems

  • sentry/security behaviours

  • Android head-unit integration

The system will likely eventually be designed around multiple layers including:

  • local AI reasoning

  • fast-response embedded systems

  • distributed controller nodes

  • vehicle state systems

  • visual feedback systems

A large amount of the AI side is still being actively planned and rebuilt as the hardware direction becomes more finalised.


Current Focus

Current development is mainly focused on:

  • controller integration

  • wiring architecture

  • visual system refinement

  • processor core behaviour

  • embedded communication systems

  • modular mounting systems

  • preparing the project for the future AI migration

There is still a huge amount left to build, redesign, and learn, but the project is finally starting to move from scattered prototypes into a more cohesive system.

More updates soon.

Starting LBs circuit displayWhat started as a rectangle boardQuickly evolved into LBs circuit display. New red hex perforated plate looks wicked
Now it is looking like an AI DNA SYSTEMThis is where it goes in the car.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB 5 months ago

    Interesting project.

    I look forward to future updates.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB 5 months ago

    Interesting project.

    I look forward to future updates.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor 5 months ago in reply to DAB

    Thank you, i will post updates soon. I hope to do tests on the voice visual very shortly. One of the s3 in the display is dedicated to the job using a neopxl at the 7 strips in the grill and running cat6 for data lines. I did post a question about this a bit back because i was getting interference when the voice of LB finished and it was supposed to drop back to knightrider scan mode but i have hopefully sorted that out now. As you can see it is all on the go at once, but it is coming along and hopefully be on the home stretch soon!! 

    imageimageimageimageimage