Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum 40pin LVDS LCD Interface on laptops
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 128 subscribers
  • Views 908 views
  • Users 0 members are here
Related

40pin LVDS LCD Interface on laptops

e14 Contributor
e14 Contributor over 16 years ago

Hello,

 

I am in the process of designing a prototype which will utilize a ~10" LCD display.

 

I was wondering if someone out here could help me with one part of this: the 40pin LVDS interface that is common on many laptops and netbooks.

 

As I understand it, this interface is common accross many LCDs and laptops but I cant quite figure out what it is!

 

Is it a standard? If so does it have a name? Are there timing diagrams I can look at? Common connectors and pinouts?

 

I've searched around but so far I can't find any mention of it, only "this product has a standard 40 pin....etc etc"

 

Searching for information on this is like trying to nail jelly to a wall, or understand what SOAP is/does!

 

Anyone have experience with this?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi Sebastian,

     

    JAE is a supplier to Farnell and there Product Manager has sent me your details. Your right finding the right connection for LVDS can be quite a minefield.

     

    JAE has a great deal of experience within this market and are major suppliers to Compaq, Toshiba, Dell, Fujitsu and are supplying different types of LVDS connections.  In the fist instance I propose you check our website

     

    www.jae.co.uk and then click on products.  Series you need to possible consider is FI-NX this is a 40 pin using FPC or our  FI-J, FI-JH which is Microcoax cable.

     

    I hope this helps but please do not hesitate to contact me if you need any further help.

     

    Best regards

    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Hello Peter,

     

    Yes I've used JAE connectors for laptop IDE drives before.

     

    What I was having trouble with wasn't the connectors so much as the actual interface.

     

    I have found two interfaces: FPD-Link and OpenLDI (OpenLDI is based on FDP-Link). FDP-Link (Flat Panel Display Link) is apparently used in many laptops to connect the display, but im not sure its what I need since 1. there appears to be some sort of reciever between the LCD 'driver' and the FPD-Link transmitter - maybe FDP-Link is just some interim method to get alot of data through a few cables in the laptop hinge? which brings me on to 2. The term "40 pin LVDS" sounds very specific, FDP-Link does not use 20 data lines, its 5 at most for 24 bit colour:

     

    http://www.national.com/an/AN/AN-1032.pdf

     

     

    I'm pretty sure the connection to which I refer is the same as used on embedded PCs which have LVDS LCD Ports. Apparently these need specific settings in the BIOS for timing purposes but I find it hard to believe that companies would sell LCDs claiming compatability with "90% of laptops" without some sort of standardization.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Hello Peter,

     

    Yes I've used JAE connectors for laptop IDE drives before.

     

    What I was having trouble with wasn't the connectors so much as the actual interface.

     

    I have found two interfaces: FPD-Link and OpenLDI (OpenLDI is based on FDP-Link). FDP-Link (Flat Panel Display Link) is apparently used in many laptops to connect the display, but im not sure its what I need since 1. there appears to be some sort of reciever between the LCD 'driver' and the FPD-Link transmitter - maybe FDP-Link is just some interim method to get alot of data through a few cables in the laptop hinge? which brings me on to 2. The term "40 pin LVDS" sounds very specific, FDP-Link does not use 20 data lines, its 5 at most for 24 bit colour:

     

    http://www.national.com/an/AN/AN-1032.pdf

     

     

    I'm pretty sure the connection to which I refer is the same as used on embedded PCs which have LVDS LCD Ports. Apparently these need specific settings in the BIOS for timing purposes but I find it hard to believe that companies would sell LCDs claiming compatability with "90% of laptops" without some sort of standardization.