Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog EZ-MCXN: Simple Dev Board for NXP MCX N-Series Microcontrollers!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 30 Sep 2026 5:40 PM Date Created
  • Views 663 views
  • Likes 11 likes
  • Comments 51 comments
  • MCX
  • mcuxpresso
  • audio
  • Cortex-M
  • EZ-MCXN
  • MCXN
  • i2s
  • MCXN547
  • cortex-m33
  • nxp
  • pdm
  • arm
  • FRDM-MCXN236
  • MCXN236
  • MCXN235
Related
Recommended

EZ-MCXN: Simple Dev Board for NXP MCX N-Series Microcontrollers!

shabaz
shabaz
30 Sep 2026

Table of Contents

  • Introduction
  • MCX Overview
    • MCXN236
  • Circuit Diagram
    • Supply Decoupling
    • USB and Boot
    • Audio Interfaces
    • SPI, TFT, LEDs and Buttons: User Interface
    • I2C and more SPI: microSD Card
    • ADC and Spare GPIO Pins
  • Board Layout and Parts List
  • Summary

Introduction

Recently, I wanted to play a little bit with audio projects, and noticed that NXP has some interesting new microcontrollers with just the interfaces I was hoping for. There are low-cost ready-made development boards for the MCXN range, but not for the particular package I was interested in, so I decided to make my own of sorts. In addition, I find I make less errors in future projects, if I take the time to produce a little test board for the microcontroller I plan to use. It’s a great opportunity to test out the CAD footprint, and decide what pins and peripherals to use, and determine the minimal viable circuit to bring up the part and program it.

This blog post details the test board I plan to make, in case anyone else is interested in this particular microcontroller too, and wishes to follow along. The KiCad project, footprint and other relevant files are all in an ez_mcxn project repository. Please note I have not tested this board yet, I have yet to receive the PCBs. The PCBs have arrived and have been assembled.

In a follow-up blog post I’ll explore how to build and run a demo app, assuming the hardware works!

image

MCX Overview

According to NXP, MCX microcontrollers are intended for “simplified system design”. The MCX N-Series (which I plan to use; specifically the N23 series) offers high-performance, but there are other options, such as the general A-series, low-cost C-series, and wireless W-series. There are even some ultra-tiny 3 x 3 mm sized (QFN16 0.5 mm pitch) microcontrollers offered; the part I was interested in comes in a 100-pin QFP package.

The MCX parts have been around for just a year or two; I believe they contain a blend of older NXP LPC microcontroller features, along with Kinetis features from the Freescale acquisition (I’m basing this on the fact that I see lots of Freescale copyright notices in the SDK source code).

By “simplified system design” NXP may mean that the software development environment is a bit more modern (the old Eclipse platform is still offered, plus the usual IAR and Keil development environments, but now users can download and run using a VS Code plugin I believe; I decided to do things via the command line for now (apart from microcontroller configuration, for which I prefer the desktop graphical app from NXP, called MCUXpresso Config Tools. The app auto-generates source and header files which can be included within project builds.

Freescale microcontroller reference manuals used to be top notch, so I suspect that amount of documentation excellence may have been carried over onto the MCX series.

The SDK from NXP is called MCUXpresso SDK (HTML API Guide), and seems fine at first glance, I cannot comment much so far (I have built a blinky and a UART transmit project, but I have not explored further until I have hardware to try these things on). The NXP diagram below shows the functionality provided within the SDK.

image

Image source: NXP

Since I was not interested in downloading a complete development environment, I just installed the MCUXpresso SDK using manual installation, and the MCUXpresso Config Tools app. I already had a compiler installed on my PC previously (called the ARM GNU Toolchain, downloadable from the ARM website).

My initial coding experiments are in the project GitHub repo, but have not been tested on real hardware currently. I plan to use a SWD CMSIS-DAP debug probe for firmware uploading/debugging, but direct upload is possible using the built-in bootloader within the microcontroller ROM. If you’re new to ARM devices, for an introduction to SWD and debug probes, see here:  Using SWD with ARM Microcontrollers: An Introduction to Firmware Programming and Debugging! 


MCXN236

The particular part I went for contains a Cortex-M33 core that runs at 150 MHz, 1 Mbyte Flash (their diagram below has a typo, it’s not 1 Mbit!), and RAM space totalling 352 Kbyte.

image

Image source: NXP

Many of the integrated features look very useful for a lot of projects. There is High Speed USB (480 Mbps), two simultaneous-sampling ADCs (great for measuring instruments, or even software-defined radio!), CAN FD interfaces, plus lots of audio interfaces (simultaneous I2S receive and transmit, plus up to 4 PDM MEMs mics). For more info, download the MCXN236 PDF Data Sheet, or the huge PDF Reference Manual. There is also a higher-end MCXN547 part that is (I believe) pin-compatible, with double the Flash, extra RAM, Ethernet, and dual-core.

The NXP development board for the MCXN236 (but in a different package) is called FRDM-MCXN236, and is quite low-cost in case anyone wants to immediately experiment with this part!

image

Image source: NXP

Circuit Diagram

The entire circuit diagram follows, but in bite-size pieces with explanation (the full KiCad source file is within the project repository).

Supply Decoupling

I decided to supply the microcontroller with a 3.3V source.

The package has 100 pins, and quite a lot of capacitors for power supply decoupling are needed, for some of the microcontroller internally generated rails as well as the 3.3V supply. Most of the 100nF capacitors are 0402-sized, to squeeze close to the microcontroller. There is an exposed ground pad on the underside of the package incidentally.

Some components are crossed out in red in the circuit below, for instance, L1 and C20 at pin 53 are omitted, they enable a DC-DC converter for greater efficiency, but I left those unpopulated to reduce noise since I may wish to experiment with the built-in ADC channels one day.

image

USB and Boot

The 3.3V microcontroller supply comes from a USB socket (which provides about 5V), followed by a 3.3V LDO. Optionally, the 5V power entry can come from the screw-terminal connector J14, so it's not essential to power via USB.

The debug probe attaches to the SWD connector. If there is no debug probe, it is possible to upload firmware to the device via USB or UART [a USB-UART adapter would be used], by holding down the BOOT button while pressing RESET; there is NXP software to perform the firmware transfer from the PC in that case.

image

Audio Interfaces

I used three connectors for the audio; PDM, and I2S (PDF I2S specification document) input and output. There is a second data line on each of the three connectors, i.e. the microcontroller supports up to four channels of audio (stereo per data signal) on each connector.

image

SPI, TFT, LEDs and Buttons: User Interface

I wired the J13 header so that up to eight of the GPIO on port 3 could be used for keypad scanning. The pins are arranged so that typical 4x3 or 4x4 keypads should be able to easily connect, and there are three buttons on the PCB if no external keypad is used, and the GPIO could be used for other purposes if a keypad is not needed.

The SPI interface could be used to drive a TFT screen, or used for interfacing other devices. At the lower-right of the circuit in the diagram here, it can be seen that the MISO connection can optionally be routed elsewhere; that’s for making the board easier to use with the MCXN547 microcontroller, if Ethernet was required (unfortunately then the MISO line is no longer usable due to the particular set of pins chosen for the rest of the SPI interface; that won’t affect things if the SPI interface was used just for a display of course, as that would only require MOSI and not MISO).

There are two LEDs on the PCB attached to a couple of GPIO pins.

image

I2C and more SPI: microSD Card

Another SPI interface was wired up to a microSD card socket, perhaps useful for audio file storage and so on (in the block diagram earlier, it can be seen that the SDK contains file system capabilities, so this should be straightforward to include into projects hopefully).

image

ADC and Spare GPIO Pins

Nearly all remaining connections on the GPIO were wired to header pins. Header J9 (labelled P4/ADC) could be particularly useful, since a lot of the ADC inputs are available there. The P1MISC header J5 can be used for attaching an Ethernet PHY if desired, when using the MCX547 microcontroller. The P1_2 signal shown at the top-right of the disgram is wired (via a normally unpopulated zero-ohm resistor) to the SPI MISO connection mentioned earlier (that signal is repurposed for the Ethernet capability).

image

Board Layout and Parts List

The board is 4-layer 70x70 mm, with mostly 0603-sized passives, but there are a few 0402-sized ones where space was constrained (particularly the many 100 nF decoupling capacitors are 0402-sized). I placed some bare SMD pads near the ADC header, in case small additions are required, for instance to supply power to the microcontroller ADC pin from a separate LDO.

For the parts list, see the Readme file in the project GitHub repo.

image

The underside has exposed copper to hopefully make it easier to hand-solder the microcontroller center pad. The inner layers are not shown, but they don't contain anything apart from 0V (layer 2) and 3.3V (layer 3).

image

Summary

The MCX series N microcontroller MCXN236 looks very useful for a lot of projects, so a little test board was designed, that brings out most of the connections to 2.54mm pin headers, and the project files (including Gerber files) are in the project GitHub repo. 

If things don't go wrong, the next blog post, hopefully in a few weeks time, will cover board bring-up and a bit of coding.

Thanks for reading!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz 1 month ago in reply to michaelkellett +1
    Unfortunately that's an older screenshot (it's the usual problem, the more recent updates get hidden by the site : ( I'd made it a solid pad, but didn't enlarge the holes further (I have made them larger…
  • shabaz
    shabaz 18 days ago in reply to shabaz +1
    The drag soldering eventually got easier.. just one or two bridges to fix per chip by the end. But, I needed to use preheater+hot-air later anyway, because the crystals looked impossible otherwise. This…
  • shabaz
    shabaz 15 days ago in reply to Jan Cumps +1
    Interesting video! If cleaning doesn't work, I think maybe TL59 could be a close match: Or possibly this from AliExpress comes in 6x6x4.3 and 6x6x5 variants but I couldn't tell the precise spacing…
Parents
  • shabaz
    shabaz 18 days ago

    That was not fun, it took an hour of concentration to get three of the microcontrollers soldered down!

    I should have considered using the preheater+hot air tool. Instead, I put a dab of solder paste on the center pad, then taped the chip to the board.

    image

    Kapton tape is really good for this. Plus it is only slightly stretchy, so for that last 0.1-0.2 mm of adjustment, it is possible to lift up one end, stretch and place it down. 

    image

    To check the alignment closer, I used a very low-cost Carson magnifier.. It gives an amazingly well-lit and sharp image (hard to photograph that).

    image

    Then I flipped the board and used a large 3mm tip at 360 deg C, for about 10-12 seconds, to reflow that paste.

    After that, I removed the tape, and then did drag soldering (and I always mess up the last couple of pads when drag soldering, so those were fixed with desoldering wick). Then scrub board clean (I used IPA, I don't have any flux cleaner). 

    My procedure isn't very good, and probably the board should be properly reflowed to activate all the flux residue, otherwise it will affect the current consumption and maybe even ADC measurements etc. I will worry about that later!

    Lots of difficult soldering still to do (some 0402 since I didn't have a lot of room close to the chip, and a couple of very small crystals).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz 18 days ago

    That was not fun, it took an hour of concentration to get three of the microcontrollers soldered down!

    I should have considered using the preheater+hot air tool. Instead, I put a dab of solder paste on the center pad, then taped the chip to the board.

    image

    Kapton tape is really good for this. Plus it is only slightly stretchy, so for that last 0.1-0.2 mm of adjustment, it is possible to lift up one end, stretch and place it down. 

    image

    To check the alignment closer, I used a very low-cost Carson magnifier.. It gives an amazingly well-lit and sharp image (hard to photograph that).

    image

    Then I flipped the board and used a large 3mm tip at 360 deg C, for about 10-12 seconds, to reflow that paste.

    After that, I removed the tape, and then did drag soldering (and I always mess up the last couple of pads when drag soldering, so those were fixed with desoldering wick). Then scrub board clean (I used IPA, I don't have any flux cleaner). 

    My procedure isn't very good, and probably the board should be properly reflowed to activate all the flux residue, otherwise it will affect the current consumption and maybe even ADC measurements etc. I will worry about that later!

    Lots of difficult soldering still to do (some 0402 since I didn't have a lot of room close to the chip, and a couple of very small crystals).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kk99
    kk99 18 days ago in reply to shabaz

    Well done !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 18 days ago in reply to shabaz

    The drag soldering eventually got easier.. just one or two bridges to fix per chip by the end.

    But, I needed to use preheater+hot-air later anyway, because the crystals looked impossible otherwise. This one is wonky but I think it's making contact.

    image

    32.768 kHz:

    image

    For the crystals I first cushioned them upside-down on Blu-Tack, then tinned the pads of them, then tried wiping them clean (not easy since they are tiny) then after the board was at about 100 deg C, syringed a tiny bit of flux paste onto the PCB pads, and placed the crystals with tweezers, and then used hot air, tapping down on the parts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 17 days ago in reply to shabaz

    Other things got in the way and I didn't solder as much as I hoped, but got a lot of 0402 decoupling capacitors complete (13 x 100nF per board).

    These were actually not difficult at all, provided solder blobs are tolerable. I painted on watery flux, then used a pointy bent conical tip, works superbly even on the tiny footprint. To reduce blob size I'd have to use even thinner solder wire, but then there's little flux in the solder, so I'd rather the blobs.

    Hot air tool could have been an option, but I tend to accidentally crack (and short-circuit) 0402-sized capacitors (because of uneven heating perhaps..) so I'd much rather hand-solder these.

    image 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 16 days ago in reply to shabaz

    > I should have considered using the preheater+hot air tool.

    A pre-heater does magic, even if you just moderately heat up the board. Each °C that you pre-heat-up the board is a degree less that has to be conquered by the iron or air gun.

    I'm replacing the little push buttons on my CD player, and each of them has one pin on the big ground copper. Without thermal relief.
    I used a preheater to bring it up to 100°C. Still safe for all parts on it.

    image

    Then used a solder sucker on 350°C to unsolder each pin.
    Solder melted virtually immediately, and all switches nicely fell out by gravity. Without damaging a path or trace.

    image

    image

    If I start from room temperature, the sucker struggles somewhat. And that results in having to put that 350°C longer on the PCB. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 16 days ago in reply to Jan Cumps

    Nice use-case. Pre-heaters are extremely helpful, very underrated tool! 

    Did the switches oxidize on the inside do you think? Or were they just worn out mechanically. Where I am, I frequently see the component leads getting oxidized heavily, especially on tact switches (even good brands like Omron). I assumed they are are plated on the contact area though, to reduce that, but have still wondered about how long they would last without replacement.