Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog MSPM0 analogue front-end: general purpose amp as buffer for ADC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 22 Jun 2026 7:11 PM Date Created
  • Views 226 views
  • Likes 6 likes
  • Comments 2 comments
  • MSPM0
  • easyL1105
  • texas_instruments
  • ti
Related
Recommended

MSPM0 analogue front-end: general purpose amp as buffer for ADC

Jan Cumps
Jan Cumps
22 Jun 2026

The MSPM0 has a general purpose amp (GPAMP). It's an internal OpAmp that, for example, can buffer a signal for the ADC without external components. That's an example that I'm trying out in this post. Roughly based on the Resource Explorer gpamp_buffer_to_adc example.

image

Setup

For this example, the GPAMP is configured with x1 gain (a buffer or input follower). And its output is internally routed to the ADC input.

image

source: wikipedia all rights released (Public domain)

GPAMP settings:

image

The non-inverting input (+) is routed to pin PA26. The output is internally routed to the inverting input (+).

image

The internal routing to the ADC is done by setting the ADC channel:

image

image

The C code is unchanged from TI's gpamp_buffer_to_adc example.

ChatGPT info:

image

Test

The test source is a 2.5 V reference. The ADC reference is VDDA (3.3 V). I've done 3 tests: measure the ADC reference voltage, and the 2.5 V test signal.

  • buffered by GPAMP,
  • directly to the ADC
  • with a Brymen BM235 DMM
GPAMP (0 - 4095) ADC (0 – 4095) BM235 (mV)
ADC ref 4085 4095 3290
input 3110 0.761321909424725 3097 0.756288156288156 2498 0.759270516717325

This will work for the EasyL1105 board and with an L1306 Launchpad.

Thank you for reading.

Related posts

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps 3 months ago in reply to DAB +1
    DAB , yes. They aren't the only ones. Renesas has a very neat RX23-E controller. It has an impressive front end with programmable gain, precision ADC. And then digital filtering. Capable of doing…
Parents
  • DAB
    DAB 3 months ago

    Nice post Jan.

    I did not know that this device included opamps withing the architecture.

    It looks like TI is copying capability from the PSOC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB 3 months ago

    Nice post Jan.

    I did not know that this device included opamps withing the architecture.

    It looks like TI is copying capability from the PSOC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps 3 months ago in reply to DAB

    DAB , yes. They aren't the only ones.

    Renesas has a very neat RX23-E controller. It has an impressive front end with programmable gain, precision ADC. And then digital filtering.

    Capable of doing load cell measurement, and thermocouple temperature measurements with compensation. Without external active components.