Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Taiyo Yuden BLE EVK : Miniature BLE Automation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: navadeepganeshu
  • Date Created: 22 Aug 2020 12:00 PM Date Created
  • Views 1807 views
  • Likes 2 likes
  • Comments 1 comment
  • ble
  • taiyo yude
  • holidayspecial20ch
  • wireless
  • embedded system
  • bluetooth®
Related
Recommended

Taiyo Yuden BLE EVK : Miniature BLE Automation

navadeepganeshu
navadeepganeshu
22 Aug 2020

Taiyo Yuden BLE EVK : Toggling GPIOs and Taiyo Yuden BLE EVK : Wireless LED Control gives insights on basic configuration, setting up, toggling GPIOs and wireless LED control by interacting with MPU core + SoftDevice of Taiyo Yuden BluetoothRegistered Low Energy EYSNSNZWW Evaluation Kit . This blog will be all about building a 1miniaturised home automation system using BLE with UART communication with Arduino Nano. For this, I downloaded the following software tools

 

  • Segger Embedded Studio V5.10.
  • Nordic Semi nRF52 SDK with Soft Device 12,13.
  • nRF Toolbox Android Application

 

Taiyo Yuden EYSNSNZWW comes with ARMRegistered Cortex M4 32bit processor and 192KB Flash + 24KB RAM having SPI, UART, I2C, PDM and 12bit ADC GPIO interphases. It is also integrated with Bluetooth 5.2 totally said to be Nordic nRF52811 / ARMRegistered CortexTm-M4 32-bit processor. To control the appliances over BLE, access to the processor core layer and soft device must be implemented (used Soft Device 13 here). First, I connected debugger to BLE module with SWD cable. Then on, USB  interphase to the computer running Segger Embedded IDE. With connections being planned, I interphased Pin8(Tx)  and Pin20(Rx)  of Taiyo Yuden module with respective Rx and Tx of Arduino Nano. Since I needed 5 digital IO's and easy implementation, I chose to add Arduino Nano.

 

image

 

Basically, Arduino Nano receives all the serial commands from the BLE module and accordingly controls the LEDs and a buzzer connected to it. There can be "n" number of unique commands and any number of IO's can be controlled. Nano makes this job handy. To do it, first, UART transmission must be implemented in Taiyo Yuden BLE module which is already given as an example.

In Segger Studio go to "File" >> "Open Solution" to open sample project from nRF52 SDK at "<location>" >> "examples" >> "ble_app_uart" >> "PCA10040e" >> "s112" >> "ses" >> "ble_app_uart". Sample projects are made for Nordic development boards which supports Taiyo Yuden BLE kit too with some modifications since they have same nRF5281x core. (files are also attached below)

 

 

{gallery} Firmware Setup

image

IMAGE TITLE: File Location

image

IMAGE TITLE: Clock Configuration

image

IMAGE TITLE: UART Pins

image

IMAGE TITLE: Change SoftDevice

 

image

IMAGE TITLE: Change SoftDevice

image

 

IMAGE TITLE: Change SoftDevice

image

IMAGE TITLE: Change Memory mapping

 

image

 

IMAGE TITLE: Build and Download to Hardware.

 

 

After making the following changes and building, Taiyo Yuden BLE Kit is ready! Pulling the serial wires (Rx/Tx) to Arduino Nano and interphasing LED's to some Digital IOs, its time to program Nano.

I have used basic serial read command and ran 5 test cases for 5 different commands namely "R", "G", "B", "Y", "S" for Red, Green, Blue, Yellow LEDs and Buzzer in pins D4, D5, D6, D7, D8 respectively. Then, I used a reset command "0" to set all the digital pins to state 0. Following is the implementation.

 

#include <SoftwareSerial.h> //for ser1ial communication within software.
#define TxD 2               //  in1itialize
#define RxD 3
SoftwareSerial mySerial(RxD, TxD);
void setup() 
{
  pinMode(4, OUTPUT);       //  R,G,B,Y LED's
  pinMode(5, OUTPUT);
  pinMode(6, OUTPUT);
  pinMode(7, OUTPUT);
  pinMode(8, OUTPUT);
  mySerial.begin(115200);
  Serial.begin(115200);
}

void loop() 
{
    char isValidInput; 
    do
{
  
char c;
while ( !mySerial.available());     
c = mySerial.read();
Serial.print(c);
switch ( c )
{

case 'R':
mySerial.println( "You've entered Red ON" ); //Red LED control
digitalWrite(8, HIGH);
isValidInput = true;
break;

case 'G':
mySerial.println( "You've entered Green ON " ); //Green LED control
digitalWrite(7, HIGH);
isValidInput = true;
break;

case 'B':
mySerial.println( "You've entered Blue ON" );  //Blue LED control
digitalWrite(6, HIGH);
isValidInput = true;
break;

case 'Y':
mySerial.println( "You've entered Yellow ON" ); //Ye11ow LED control
digitalWrite(5, HIGH);
isValidInput = true;
break;

case 'S':
mySerial.println( "You've entered Sound ON" );
digitalWrite(4, HIGH);
isValidInput = true;
break;

case '0':
mySerial.println( "You've pressed Reset!" ); //Resetting Pins
digitalWrite(4, LOW);
digitalWrite(5, LOW);
digitalWrite(6, LOW);
digitalWrite(7, LOW);
digitalWrite(8, LOW);
isValidInput = true;
break;

default:
mySerial.println( "Enter 'R'-Red/'G'-Green/'B'-Blue/'Y'-Yellow/'S'-Sound/'0'-Reset");
isValidInput = false;                           //User input decleration
break;
}
} 
while ( isValidInput == true );
}

 

image

 

 

All these being set up, its good to go! Opening the nRF Toolbox Application and connecting to "Nordic_UART" network will open the UART Terminal on the smartphone. The commands to enter will be displayed for choosing the device to toggle. Once the respective command is entered, you can see live toggling on the other end.

The BLE network range in Taiyo Yuden EYSNSNZWW Module isn't that good. Changing floors will cut the connection and network ranges about 10 meters.

 

imageimage

imageimage

 

image

 

Here is a quick video on working of Wireless BLE Miniature Automation.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Cheers!!!

Happy Making.

Attachments:
BLE_Miniature_Automation.zip
  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Nice expansion of your first post. DAB
Parents
  • DAB
    DAB over 6 years ago

    Nice expansion of your first post.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 6 years ago

    Nice expansion of your first post.

     

    DAB