The title should not be a surprise here in the USB Community since SuperSpeed USB is now in the market. Still this is a news for developers working on this. Talking about SuperSpeed USB, the USB 3.0 standard claims that i...
Here is a sample application that we have created using the CoreCommander board for mass storage on Altera FPGA. The video given below does not have voice. You can read the comments and view the mass storage implementation.
Attachmen...
The aim of this project is to control a Robotic Arm which is mounted on to the Traxster. Wii Nunchuck is used to control Robotic Arm and Traxster. We are just using the two buttons and the Joystick and this data is been transfers wireless...
Embedded software engineers only need to know one programming language to get through life: C. Most embedded software projects are written in C. So that leaves most other languages out of use (I insist, for embedded programmers). I ...
for my project i produced a security locking device where a new code was generated every hour. it used a one way encryption alogithm, to scramble the time and key data producing a new password. it has a number of features including admin login to gen...
The aim of this project is to control a Robotic Arm which is mounted on to the Traxster. Wii Nunchuck is used to control Robotic Arm and Traxster. We are just using the two buttons and the Joystick and this data is been transfers wireless...
Going into the 2011 Embedded Systems Conference Silicon Valley I was looking forward in particular to seeing and hearing more about new MCUs and ecosystem developments. The show did not disappoint. If there was one product to capture “bes...
Copper based ICs have reached nano-meter densities, with wire so small, that no current seizes to flow. The University of Cambridge professors John Robertson and Santiago Esconjauregui have devised a possible future solution. They are growing C...
Spacecraft and rockets with no personnel onboard are controlled by people on the earth's surface. There is one major issue with this arrangement, time to action responses. When a rocket's onboard sensors discover an error, it relays the inform...
CRISP has developed a multi-core processor that will test and repair itself, sort of. There is an on-board resource manager that will test to see if a core is malfunctioning, and if so, send the tasks to a functioning core. The idea is to creat...
“As electronics become more advanced, we are approaching the point where conventional materials like copper can’t take the heat. For computing to go faster and electronics systems to become more capable, better cooling solutions s...
The purpose is to watch the person who made the lunch, make it, while you eat it. And also, so the preparer can watch you eat it. A never ending cycle. Researchers at Ochanomizu University have embedded a camera and LCD touchscreen into a lunch...
The XIM 3 stand for XBOX Input Machine version 3. For those who do not know, the XIM 3 allows for a keyboard, mouse, joystick, and other USB based devices to be adapted to the console. But that is not the end of the device's features. In ...
www.youtube.com/watch Missouri University of Science and Technology is resolved to make a handheld scanner that can see through anything. Similar to airport scanners, this hand held camera used millimeter and microwave signals to peek inside. In...
Samsung has taken DRAM to a whole new level, 12.8GB/sec, a great increase over the former LPDDR2. In the process, reducing power consumption by 87%. The increase in data transmission is due to the increase of I/O pins to 512 from the 32 the pri...
A complete computer system in 1 cubic millimeter. Onboard is a low power microcontroller, memory, battery, wireless radio, solar cell, and a pressure sensor. This system is meant to be an implantable eye pressure monitor for glaucoma patients. I'm su...
The first (sequential) logic circuit has been built using carbon nanotubes. The fast manufacturing process has been developed to print these circuits on TFT with a plastic sub straight resulting in a flexible circuit board. Professors Yutaka Ohno fro...
Faster mobile device access is close at hand. SanDisk Corporation recently announced its next generation of iNAND and iNAND Ultra embedded flash drives featuring smaller and thinner form factors. Available in packages as small as 11.5mm x 13mm x 1mm,...
Pelican, a California startup company, is trying to make a big name for themselves by being a little outside the box. They a promoting a new camera for cellphones that consists of 25 small cameras. The concept is to spread available light over the 25...
Engineers and scientists collaborating at Harvard University and the MITRE Corporation have developed and demonstrated the world's first programmable nanoprocessor. “This work represents a quantum jump forward in the complexity and function of circui...
Graphene molecular model image.A new transistor made from graphene, the world's thinnest material, has been developed by a research team at the University of Southampton. The new transistor achieves a record high-switching performance which will make...
OK, so it can’t reach the energies produced at the LHC or Tevatron, but this is still pretty impressive. Engineers at a micro-electro mechanical systems conference that was held recently in Cancun, unveiled this tiny cyclotron device, which can speed...
Recently Marvell announced the world’s first ‘ultra-low power, ultra-high performance’ 1.5 GHz three-core processor that is the first to feature 3D graphics performance with quad unified shaders for 200 million triangles per second delivered on mobil...
Gallium nitride material holds promise for emerging high-power devices that are more energy efficient than existing technologies, but these GaN devices traditionally break down when exposed to high voltages. Now researchers at North Carolina State Un...