Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum STM32L4 With DMX512
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 11 answers
  • Subscribers 503 subscribers
  • Views 12255 views
  • Users 0 members are here
  • dmx512
  • stm32l4
Related

STM32L4 With DMX512

p.congre
p.congre over 5 years ago

Hello there,

 

I am trying to control 2 LED strips (one with a WS2811 LED driver and one with a USC512C4 LED driver) with my STM32L4 with integrated RS485.

Do you have any idea how to do this?

 

Best regard.

P.Congré

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago in reply to p.congre +2 suggested
    In xxx_project.h, #ifndef __C459_PROJECT_H #define __C459_PROJECT_H // INCLUDES #include "stm32f0xx.h" #include <stdio.h> #include <stdbool.h> #include <stdint.h> // DEFINES #define VERSION 100 #define…
Parents
  • jc2048
    0 jc2048 over 5 years ago

    I should have added that there's also useful material about DMX512 here on the community. Here are a couple of good examples from shabaz and from genebren

     

    DMX Explained; DMX512 and RS-485 Protocol Detail for Lighting Applications

     

    DMX diagnostic tool - Getting started
    DMX diagnostic tool - Sending and Receiving Data

    DMX diagnostics tool - running out of time

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • p.congre
    0 p.congre over 4 years ago in reply to jc2048

    Hello Jon,

     

    I managed to control my LED strip with the USC512C4 IC with my arduino, but I need to do it with my STM32L4 but I can't find anywhere how to do it.

    Do you have a code example for an STM32L4?

     

    Best regard.

    P.Congré

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • p.congre
    0 p.congre over 4 years ago in reply to jc2048

    Hello Jon,

     

    I managed to control my LED strip with the USC512C4 IC with my arduino, but I need to do it with my STM32L4 but I can't find anywhere how to do it.

    Do you have a code example for an STM32L4?

     

    Best regard.

    P.Congré

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jc2048
    0 jc2048 over 4 years ago in reply to p.congre

    Sorry, I don't have any code I can give you.

     

    Can't you port what you're doing with the Arduino to the STM32L4? It shouldn't be too difficult to send serial characters, so the tricky bit will be the break as that depends very much on what the particular serial peripheral can do. It might allow you to do it directly. Or you might be able to see a way to do it indirectly (by, for instance, enabling and disabling the peripheral so that it moves back to being an IO pin for a time, or by flipping the sense of the output pin if it can be changed from positive true to negative true). If you can't see a way to do it in the processor, you could always add an external logic gate to switch between serial and the break state. You'll probably need to use a timer to get the break period, so you'll have to work out how to do that too (I'm sure there's plenty of material on how to do that kind of thing).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • p.congre
    0 p.congre over 4 years ago in reply to jc2048

    Hello Jon,

     

    There is no communication between the arduino and the STM32L4, and i can't port yhe arduino code to the stm32.

    With the arduino, I managed to control my LED strip with DMX protocol (the LED strip has a USC512C4 IC).

    Now I want to control the LED strip with my STM32L4 but it is quite difficult.

     

    I use an RS-485 to create the DMX communication. I found some codes on the internet but it doesn't work.

     

    https://github.com/aleksandrgilfanov/stm32f4-dmx-transmitter/blob/master/Src/main.c

    https://github.com/carl3721/stm32-dmx512/blob/master/dmx-p103/src/main.c 

     

    Best regard.

     

    P.Congré

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 4 years ago in reply to p.congre

    The project at the first link you give appears to be based on some modified ST code. Perhaps you could ask ST for the original code if you can't find it on their website. It's very unlikely they would issue anything that didn't work.

     

    Is there a reason why you can't just use the Arduino, since you have that working?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • p.congre
    0 p.congre over 4 years ago in reply to jc2048

    I already tried to contact ST, but nothing for the moment.

     

    I can't use arduino because the next step of the project is to control the LED strip with an STM32.

     

    best regard.

     

    P.Congré

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 4 years ago in reply to p.congre

    If you don't mind a hardware engineer telling you how to deal with debugging, here's how I'd tackle it:

     

    Does anything at all emerge from the STM32? Can you see any sign of serial waveforms at the output pin, even if it just sends a frame of 513 characters and then freezes at the break?

     

    Is your 485 chip matched to the IO voltage standard of the processor? [Not all of the older ones would be ok on 3.3V]

     

    What can you see on the A and B outputs of the driver chip?

     

    Have you wired the outputs the right way round to the LED strip?

     

    If you see a lot of overshoot and the sigals are very messy, look carefully at how you've done the termination on the RS-485. [The strip might be much more fussy than a normal DMX receiver.]

     

    If there's still nothing, try hacking together a bit of very simple test code to repetitively send a serial character and look again.

     

    If that works, go back to the DMX code and disable the stuff that does the break [the fiddly stuff with a timer that could esily go wrong] and verify that it's sending the character stream ok, then start working on the break code, maybe even isolating it and just repetitively sending the break until you get the timing right.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • p.congre
    0 p.congre over 4 years ago in reply to jc2048

    I can see the waveform of my TX PIN when I send 513 times a "U".

    The 485 chip matches the IO voltage, I checked it and I can also see the waveform of the A and B output.

    I double checked the cable connection for the LED strip.

    I know it's not hardware but rather software, I couldn't create a correct code to control the LEDs.

     

    Best regard.

     

    P.Congré

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to p.congre

    ^ Great debugging tips from Jon.

    Right now I'm trying to get hardware and software working. I did not create the hardware nor the software, but I won't raise a case until I've:

    1. Verified connections and voltages

    2. Connected a 'scope or attached a logic analyzer (they cost less than $20) and examined if the interface signals are what I expect

    3.  Grabbed debug from the code

    4.  Tried different hardware and software combinations to try to narrow down the problem

    5. Sketch a diagram or take photos or video to show precisely what I'm doing

    6.  Supply any configurations or log file content

     

    For your scenario, maybe point 2 and 4 are also relevant, since you could compare the working scenario (Arduino) with the non-working scenario, and compare the signals, to see what the difference is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 4 years ago in reply to p.congre

    Here are a couple of things to check:

     

    1. Is the serial port setup correctly?  It should be baudrate of 250,000, 8 data bits and 2 stopbits.
    2. Is the Break pulse correct? The Break pulse needs to be at least 80uS, preferably larger (the specs are not always followed).  This pulse should be a low going pulse.
    3. Is the post Break correct?  The Post break needs to be at least 12uS, preferably larger (again the spec is not always followed).
    4. Is the Start Code (first byte of the DMX stream) correct?  Some devices need this byte to be a zero, others may have other special requirements.

     

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 4 years ago in reply to p.congre

    That's good. You're not far off a working system.

     

    Do you see the break, after the frame of data is sent, present in the DMX waveform?

     

    I've never used the devices on the LED strip, but they probably depend on the subsequent break as part of their operation.

     

    It's also part of the DMX spec that you have to keep sending the break and the frame repetitively. I don't think the spec says what the receiver should do if the DMX disappears, but I think it implies the designer of the receiver should do something for what is then considered to be a fault condition if it disappears for more than a second or two [for a lamp in a theatre setting, the normal thing would be for it to shut down on loss of DMX to stop it interferring with the rest of a lighting rig].

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • p.congre
    0 p.congre over 4 years ago in reply to shabaz

    The problem is that I don't really know what line to follow to create the code, I know I need to set up a uart communication with 250000 bauderate.

     

     

    I know the DMX protocol but I don't know how to implement it in my stm32.

    image

     

    The code for the arduino is an example that I modified to create different animations.

     

    best regard.

     

    P.Congré