Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Apollo 13 inside my car !  or how to get lower AMP for a heater ?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 339 subscribers
  • Views 2020 views
  • Users 0 members are here
  • heater
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Apollo 13 inside my car !  or how to get lower AMP for a heater ?

redgreenblue
redgreenblue over 8 years ago

Hi,

 

I'm having a problem with my car heater, which is completly dead. Yep houston we have a problem, winter is incredibly hard this year.  it's over -20 celcuis outside most of the time. While I wait for better weather to fix the radiator and not freeze my fingers till they droped,  I figure I can use for a while a small heater that could use the lighter switch.

 

The lighter switch is 12 volt @ 15 amps, which give me 180 watts.

I baught a pretty nice ceramic heater that use 120 volt @ 2.1 amps, which need 250 watts.

 

I know with a lower AMP the heater will generate less heat but on the other hand this is way better than having -15 cold inside the car, which would probably feel like being inside apollo 13 with no heat...

 

The heater is pretty simple, it use the AC to power the heater and use DC to power a fan.

The thing I'm not use to is to modify and work with AC.

So here plenty of pics that show how it's build and specs.

 

I'm wondering

 

1- does I need to modify the 3 ways switch  (off, lower, high)

or

2-I need to change the step down transformer on the circuit.

 

 

Thanks guys !

Attachments:
image
image
image
image
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi redgreenblue, What you are trying to do will be difficult as you are fighting design. Since the heater is designed for 120 VAC @ 2.1 Amps this means that the effective resistance of the heater element…
  • jw0752
    jw0752 over 8 years ago in reply to redgreenblue +1 suggested
    Hi Sorry I didn't look at the pictures before I wrote the first time. I have looked now and so I hopefully won't have a red face this time. The heater actually has (2) heaters that can be hooked up together…
  • jw0752
    jw0752 over 8 years ago +1 suggested
    I will bother you one more time. You mentioned that the heater is at 460 Watts when it is on high in the last posting. At 460 watts the heater would draw about 40 amps from the 12 volts. This would also…
Parents
  • redgreenblue
    0 redgreenblue over 8 years ago

    Alright,

     

    Now I understand probably why I coudn't find an easy solution on that... Like you expected, at 'high' level on the heater, the inverter shot down, I tried this option to see what it would do...also drain out the 30aH battery I had to test the whole thing.

     

    There just one thing that bother me, it's that I don't understand how the heater is 'fixed' by a resistance ?

    And why changing this resistance won't work ?  Why this don't work like a regular resitance ?

    Maybe something I didn't understand here...anyway forget it.

     

    still very cold I'll need to use a fuel heater even if this sound totally crazy.

     

    c ya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • redgreenblue
    0 redgreenblue over 8 years ago

    Alright,

     

    Now I understand probably why I coudn't find an easy solution on that... Like you expected, at 'high' level on the heater, the inverter shot down, I tried this option to see what it would do...also drain out the 30aH battery I had to test the whole thing.

     

    There just one thing that bother me, it's that I don't understand how the heater is 'fixed' by a resistance ?

    And why changing this resistance won't work ?  Why this don't work like a regular resitance ?

    Maybe something I didn't understand here...anyway forget it.

     

    still very cold I'll need to use a fuel heater even if this sound totally crazy.

     

    c ya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • the-dubster
    0 the-dubster over 8 years ago in reply to redgreenblue

    redgreenblue  wrote:

     

    . . . . still very cold I'll need to use a fuel heater even if this sound totally crazy.

     

     

     

    Not crazy at all! Eberspächer have been around for decades!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to redgreenblue

    Hi Andrew,

     

    The heater element itself is the resistance. If we could get inside and tap onto the resistance wire 1/10 of the way down then we would have the proper resistance for 12 volts which is 1/10th of 120 volts. The other option would be another ceramic heater that was built to have the proper resistance for 12 volts. Heat is a very difficult energy form to obtain from the electrical system in a car. The relatively low 12 volt system demands low resistance and high current in order to generate the sufficient amounts of heat needed for our comfort and to compensate for the relatively poor insulation afforded by the cars design and large glass surface area.

     

    I personally would drive cold and with lots of clothes or even not drive before I would drive with a fuel type heater in the enclosed space of a vehicle. Fuel heaters quickly consume the oxygen levels in an enclosed environment and then they produce carbon monoxide which will silently and odorlessly kill you over time. The effects can be accumulative if adequate time is not left between exposure. There has to be a better solution than using a fuel heater.

     

    Good luck

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • the-dubster
    0 the-dubster over 8 years ago in reply to jw0752

    Hi John,

    The linked heaters are mounted in the engine bay nowadays.

     

    I think the old units from the VW campers were cab mounted but - for your stated safety reasons - I guess that’s why they moved them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to the-dubster

    OK I feel better. Just didn't want to loose a friend to CO.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • the-dubster
    0 the-dubster over 8 years ago in reply to jw0752

    Amen to that, death by a shonky setup is never good! image