Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the correct replacement?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 8 answers
  • Subscribers 340 subscribers
  • Views 4413 views
  • Users 0 members are here
  • thermal switch
  • dehydrator
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the correct replacement?

hafcanadian
hafcanadian over 7 years ago

The thermal fuse on our old Magic Aire II dehydrator failed.  I ordered and installed what appeared to be a correct replacement, and did some soldering to reinforce and repair some connections on the heater board.  All original connections were rivets, so I don't know if solder will survive but am trying to save the device.

 

Everything seems to work except there's still no heat.  The one bad component yet seems to be a switch of some sort built into the heater circuit.  It is rectangular black, riveted to the board (asbestos(?) ring) with heat bands contacting the rivets, with brass connection arms in between, and a copper tongue inside that may have points on it, it's too hard to see very well inside.  Another dark blade is loose inside and I cannot tell how it fits, nor maneuver it very easily.  The switch is one and a quarter inch long overall and a quarter inch wide.

 

Is it a thermal switch of some sort, to keep the heater from getting too hot?  Perhaps it's failure caused the thermal fuse to fail?  After the time and effort so far, I'd like to see if I can get a replacement switch and probably a couple new rivets for it, since I'll try to drill out the old ones without destroying the fragile asbestos(?) board.  Or has my resurrection effort all been a waste of time?  There's a lot of extra trays and other accessories we've bought over the years for it... not crazy about tossing it all if I don't have to.  A new one is $120 and just the base unit is $90.

 

Thanks for any advice.

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • hafcanadian
    hafcanadian over 7 years ago in reply to jw0752 +4 suggested
    Note where I had to notch out the end so it straddled the rivet hole and screw, and add a wide washer for the lower screw to effectively clamp the cutout. This particular device was 2mm shorter than the…
  • jw0752
    jw0752 over 7 years ago +3 suggested
    Hi Joel, I could not get your pictures to load. Try replying to your own post and use the picture icon on the tool bar to insert your pictures into the text. In my experience the thermal fuses blow for…
  • jw0752
    jw0752 over 7 years ago in reply to hafcanadian +3 suggested
    Hi Joel, The pictured switch is the Auto Setting thermal cut out. It will open up if the element gets too hot due to lack of air flow and automatically close again when it cools down.. It should test with…
Parents
  • jw0752
    0 jw0752 over 7 years ago

    Hi Joel,

    I found this switch on ebay that cuts out at 105C. I do not know if this is going to work but it is the closest replacement that I have seen. If you have to replace rivets do it with screws, washers and nuts as this will make a good connection that is not susceptible to heat failure like solder is.

     

    https://www.ebay.com/itm/Bimetalic-Switch-Thermostat-Over-Temperature-Switch-221-Deg-F-in-USA/172517131295?hash=item282ad2841f:g:bkIAAOSwnHZYl5Px

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hafcanadian
    0 hafcanadian over 7 years ago in reply to jw0752

    I was considering getting a Klixon TH21 but now believe from its specs and description at carbonbrush.com that it doesn’t self-reset.  It’s dimensions are exactly the same as the old one’s, and it’s 20v, but each time it got hot enough to pop it’s points I’d have to shut the unit off and on to get them to close again and keep heat to the dehydrator.  When you let the unit run overnight that’s not going to be particularly convenient, and unless checked often you wouldn’t know when the heat was off because you hear the fan running regardless.  I’ve sent an email to carbonbrush.com inquiring as to a proper replacement “thermostat”.  No, I can see no identifying writing on the faulty cutout, but it may be on the underside, which cutting it off the board might reveal.

     

    John, re your comments on heat and solder, I didn’t think of using crimp connectors on the thermal fuse and power source repairs I made.  I’ve believed since my 30’s that solder joints are more complete contact-wise than manual crimping.  Before than I crimped most wiring, but they often loosened or corroded.  I originally tried prying open the eyelet-wire connectors on the mica board, but they didn’t cooperate and I only damaged the mica board in the process.  So I opted to solder wires to the crimps, kind of in iffy solution.  I may desolder them all and see if I can get crimp connectors to fit both over the crimp on one end and smaller wire on the other.  The crimps I have are different sizes of automotive-type;  hopefully they’d suffice, or are their some better suited for higher voltage alternating current?

     

    Rather than try drilling out the holddown/contact rivets and look for new ones, probably destroying the mica board in the process of replacing them, my thoughts go to cutting off the brass ends of the cutout with my Drexel to remove it, leaving the rivets and their crimps to the heater coil ends intact.  Then simply placing the replacement cutout’s holed ends over the rivets and bolting them down to the board with small brass nuts and screws through the rivet holes.  Is that a plausible idea?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hafcanadian
    0 hafcanadian over 7 years ago in reply to jw0752

    I was considering getting a Klixon TH21 but now believe from its specs and description at carbonbrush.com that it doesn’t self-reset.  It’s dimensions are exactly the same as the old one’s, and it’s 20v, but each time it got hot enough to pop it’s points I’d have to shut the unit off and on to get them to close again and keep heat to the dehydrator.  When you let the unit run overnight that’s not going to be particularly convenient, and unless checked often you wouldn’t know when the heat was off because you hear the fan running regardless.  I’ve sent an email to carbonbrush.com inquiring as to a proper replacement “thermostat”.  No, I can see no identifying writing on the faulty cutout, but it may be on the underside, which cutting it off the board might reveal.

     

    John, re your comments on heat and solder, I didn’t think of using crimp connectors on the thermal fuse and power source repairs I made.  I’ve believed since my 30’s that solder joints are more complete contact-wise than manual crimping.  Before than I crimped most wiring, but they often loosened or corroded.  I originally tried prying open the eyelet-wire connectors on the mica board, but they didn’t cooperate and I only damaged the mica board in the process.  So I opted to solder wires to the crimps, kind of in iffy solution.  I may desolder them all and see if I can get crimp connectors to fit both over the crimp on one end and smaller wire on the other.  The crimps I have are different sizes of automotive-type;  hopefully they’d suffice, or are their some better suited for higher voltage alternating current?

     

    Rather than try drilling out the holddown/contact rivets and look for new ones, probably destroying the mica board in the process of replacing them, my thoughts go to cutting off the brass ends of the cutout with my Drexel to remove it, leaving the rivets and their crimps to the heater coil ends intact.  Then simply placing the replacement cutout’s holed ends over the rivets and bolting them down to the board with small brass nuts and screws through the rivet holes.  Is that a plausible idea?