Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the correct replacement?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 8 answers
  • Subscribers 340 subscribers
  • Views 4398 views
  • Users 0 members are here
  • thermal switch
  • dehydrator
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the correct replacement?

hafcanadian
hafcanadian over 7 years ago

The thermal fuse on our old Magic Aire II dehydrator failed.  I ordered and installed what appeared to be a correct replacement, and did some soldering to reinforce and repair some connections on the heater board.  All original connections were rivets, so I don't know if solder will survive but am trying to save the device.

 

Everything seems to work except there's still no heat.  The one bad component yet seems to be a switch of some sort built into the heater circuit.  It is rectangular black, riveted to the board (asbestos(?) ring) with heat bands contacting the rivets, with brass connection arms in between, and a copper tongue inside that may have points on it, it's too hard to see very well inside.  Another dark blade is loose inside and I cannot tell how it fits, nor maneuver it very easily.  The switch is one and a quarter inch long overall and a quarter inch wide.

 

Is it a thermal switch of some sort, to keep the heater from getting too hot?  Perhaps it's failure caused the thermal fuse to fail?  After the time and effort so far, I'd like to see if I can get a replacement switch and probably a couple new rivets for it, since I'll try to drill out the old ones without destroying the fragile asbestos(?) board.  Or has my resurrection effort all been a waste of time?  There's a lot of extra trays and other accessories we've bought over the years for it... not crazy about tossing it all if I don't have to.  A new one is $120 and just the base unit is $90.

 

Thanks for any advice.

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • hafcanadian
    hafcanadian over 7 years ago in reply to jw0752 +4 suggested
    Note where I had to notch out the end so it straddled the rivet hole and screw, and add a wide washer for the lower screw to effectively clamp the cutout. This particular device was 2mm shorter than the…
  • jw0752
    jw0752 over 7 years ago +3 suggested
    Hi Joel, I could not get your pictures to load. Try replying to your own post and use the picture icon on the tool bar to insert your pictures into the text. In my experience the thermal fuses blow for…
  • jw0752
    jw0752 over 7 years ago in reply to hafcanadian +3 suggested
    Hi Joel, The pictured switch is the Auto Setting thermal cut out. It will open up if the element gets too hot due to lack of air flow and automatically close again when it cools down.. It should test with…
Parents
  • hafcanadian
    0 hafcanadian over 7 years ago

    Regarding John’s valid concern about the heat ultimately degrading the soldered source wire and thermal fuse connections I made, if that happens (if not before) I may just clockwise-loop the wire ends around screws through the rivet holes, imitating my cutout switch fix.  Now that I know what size screw (miniature stainless roundhead #1) to use it seems simpler or at least as easy as using crimp connectors.

     

    Now I’m off to post my next question for the Community re. where I can get an amber or yellow straw hat LED that’ll operate on a single 1.5v battery... 2v is all I’ve found, and it won’t light up on one AA battery.

     

    Thanks to John and those that found my question here worth following.

     

    Joel

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hafcanadian
    0 hafcanadian over 7 years ago

    Regarding John’s valid concern about the heat ultimately degrading the soldered source wire and thermal fuse connections I made, if that happens (if not before) I may just clockwise-loop the wire ends around screws through the rivet holes, imitating my cutout switch fix.  Now that I know what size screw (miniature stainless roundhead #1) to use it seems simpler or at least as easy as using crimp connectors.

     

    Now I’m off to post my next question for the Community re. where I can get an amber or yellow straw hat LED that’ll operate on a single 1.5v battery... 2v is all I’ve found, and it won’t light up on one AA battery.

     

    Thanks to John and those that found my question here worth following.

     

    Joel

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 7 years ago in reply to hafcanadian

    Hi Joel,

    I know there are white LEDs that will operate at or below 1.25 V as they are used in the sidewalk lights that work off of a single 1.25 V NiCad or Nimh battery. Perhaps you can get white ones and coat them the color that you want? The other option is to use a boost  DC to DC converter to get the voltage above the junction energy level for the regular LEDs.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer