Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Flexible PCBs; Any interest, and any tips? (NOT a discussion about specific PCB manufacturers, that will get reported, so no spam please : )
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 333 subscribers
  • Views 5495 views
  • Users 0 members are here
  • pcb manufacture
  • flexible pcb
  • pcb design
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Flexible PCBs; Any interest, and any tips? (NOT a discussion about specific PCB manufacturers, that will get reported, so no spam please : )

shabaz
shabaz over 2 years ago

The cost of prototype flex PCBs seems to have come down a _lot_ with some (not all) prototype PCB manufacturers.

Here's an example quote from a popular (3-letter name) prototype PCB manufacturer, for a 2-layer 160x100mm board with a lot of holes (I randomly chose Gerber files for a normal FR4 project, to generate this quote for now), and ENIG finish by default. $33 for 5 boards, so $6.60 per board basically,. This might actually be cheaper than an FR4 ENIG board!

image

These are the options (default settings); the board thickness is 0.11mm:

image

Another popular PCB manufacturer (one that is famous for a lot of spam) is currently quoting $158 for five boards of similar size, so that's quite a difference!

I had a variety of general questions since I've never done a flex PCB design.

Could these be useful for perhaps creating membrane-style keyboards? I'm thinking that perhaps the solder mask might be thick enough to create separation between the flex PCB and (say) an FR4 base, to create a PCB maybe. Alternatively, a laser-cut sheet could be placed in between for added separation. Has anyone tried such a thing? I'm considering it for a keypad with many dozens of keys for a variant of this project:  Triggered Sound FX: On-the-Fly Sound Mixing with Pi Pico  

Are there any tips/tricks for flex PCBs? For instance, are there particular components or connectors that lend themselves to such use, and are some components best avoided? Any checklist you use for flex PCB designs?

Would you rarely apply components to a flex PCB (using it as an interconnect), or are you comfortable with components on them? Both sides or one side? : )

Has anyone tried soldering flex PCB directly to a FR4 PCB? I have done this with the flex on some LCD displays, and it is great; they have tiny holes for allowing the flux or excess solder to pop out of, and it works very well. I was wondering if the prototype flex PCB would behave the same as the flex on typical LCD screens.

Any problems with warpage, etc., i.e., if the flex PCB outline is intricate, will it curl up while it is being manufactured, potentially getting damaged?

Are any particular copper features or trace thicknesses best avoided for portions of flex that may be bent a lot (or even repeatedly)?

What applications do you have for flex PCBs? Are you considering them for any prototype or product, perhaps where you would typically not consider them, now that they are lower cost?

I apologize for all the questions, but I figure someone must ask the basic questions!

All comments are welcome! (apart from spam!).

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +3
    Some research via Google images.. The style using metal springy domes is quite common, and the top surface can be plastic with raised bumps. I don't want a clicky tact-switch style keypad, but if that…
  • wolfgangfriedrich
    wolfgangfriedrich over 2 years ago +3
    Back in time, I did a collection of design and best practices articles. hackaday.io/.../164461-flex-pcb-design-information And probably the most impotant lesson I have learnt is, that a 2mil polyimide…
  • baldengineer
    baldengineer over 2 years ago in reply to shabaz +3
    Uneven heating is usually a different type of crack. It is possible that one side of the capacitor gets anchored, and then the other tries to move, creating a flex-like crack. Flex cracks start at the…
Parents
  • dougw
    dougw over 2 years ago

    We do a lot of rigid/flex where the component areas are FR4 and the flex allows the rigid sections to be at different angles.

    We have noticed a couple of manufacturers have dramatically reduced prices.

    Large components on flex, especially BGAs probably should have stiffeners glued under the components on the other side of the flex.

    Our flex PCBs usually have rigid frames to maintain dimensional accuracy during CCA component stuffing. (The frame adds to the cost)

    I think it is recommended to have copper on only one side of flex where it is repeatedly flexed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 2 years ago

    We do a lot of rigid/flex where the component areas are FR4 and the flex allows the rigid sections to be at different angles.

    We have noticed a couple of manufacturers have dramatically reduced prices.

    Large components on flex, especially BGAs probably should have stiffeners glued under the components on the other side of the flex.

    Our flex PCBs usually have rigid frames to maintain dimensional accuracy during CCA component stuffing. (The frame adds to the cost)

    I think it is recommended to have copper on only one side of flex where it is repeatedly flexed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 2 years ago in reply to dougw

    The manufacturer doesn't offer the rigid portion capability on that service, I suspect that would cost a lot more, but I guess there are DIY techniques that could be used, e.g. combine the flex PCB with a separate thin FR4 board for the portions where the large components need to go. I guess that's the best of both worlds, combine a flexible PCB design with normal FR4, using the flex for all the more interconnect areas and maybe smaller components if needed!